|
AM243x MCU+ SDK
11.01.00
|
|
Go to the documentation of this file.
54 #ifndef RM_TISCI_CORE_H
55 #define RM_TISCI_CORE_H
struct tisci_header hdr
Definition: tisci_rm_core.h:131
struct tisci_header hdr
Definition: tisci_rm_core.h:97
struct tisci_msg_rm_get_resource_range_req __attribute__((__packed__))
uint16_t range_start
Definition: tisci_rm_core.h:132
Get resource range response message.
Definition: tisci_rm_core.h:130
uint8_t secondary_host
Definition: tisci_rm_core.h:100
This file contains:
Definition: tisci_rm_core.h:96
uint16_t range_num
Definition: tisci_rm_core.h:133
uint8_t subtype
Definition: tisci_rm_core.h:99
uint16_t type
Definition: tisci_rm_core.h:98
uint16_t range_start_sec
Definition: tisci_rm_core.h:134
uint16_t range_num_sec
Definition: tisci_rm_core.h:135