|
AM243x MCU+ SDK
11.01.00
|
|
Go to the documentation of this file.
50 #ifndef REVISION_RD_WR_H
51 #define REVISION_RD_WR_H
66 #define JTAG_DISABLE_CHECK_SET_VAL 1U
67 #define JTAG_DISABLE_CHECK_CLEAR_VAL 0U
uint32_t value
Definition: tisci_otp_revision.h:155
struct tisci_header hdr
Definition: tisci_otp_revision.h:177
Response message after disabling jtag unlock.
Definition: tisci_otp_revision.h:113
Request message to disable jtag unlock.
Definition: tisci_otp_revision.h:104
struct tisci_header hdr
Definition: tisci_otp_revision.h:188
uint32_t value
Definition: tisci_otp_revision.h:84
tisci_jtag_disable_check_identifier
JTAG Disable check Identifiers.
Definition: tisci_otp_revision.h:229
@ JTAG_DISABLE_CHECK_SET
Definition: tisci_otp_revision.h:231
Request message to set swrev.
Definition: tisci_otp_revision.h:81
Request message to get keycnt, keyrev.
Definition: tisci_otp_revision.h:197
struct tisci_header hdr
Definition: tisci_otp_revision.h:166
uint32_t value
Definition: tisci_otp_revision.h:189
Request message to get swrev.
Definition: tisci_otp_revision.h:176
Response message to get swrev.
Definition: tisci_otp_revision.h:187
uint8_t identifier
Definition: tisci_otp_revision.h:83
@ JTAG_DISABLE_CHECK_CLEAR
Definition: tisci_otp_revision.h:233
struct tisci_header hdr
Definition: tisci_otp_revision.h:114
Request message for disabling jtag unlock check.
Definition: tisci_otp_revision.h:123
struct tisci_header hdr
Definition: tisci_otp_revision.h:93
Request message to set keyrev.
Definition: tisci_otp_revision.h:153
uint32_t keyrev
Definition: tisci_otp_revision.h:211
uint8_t identifier
Definition: tisci_otp_revision.h:125
struct tisci_header hdr
Definition: tisci_otp_revision.h:198
@ OTP_REV_ID_SBL
Definition: tisci_otp_revision.h:219
enum tisci_otp_revision_identifier __attribute__
tisci_otp_revision_identifier
OTP Revision Identifiers.
Definition: tisci_otp_revision.h:217
struct tisci_header hdr
Definition: tisci_otp_revision.h:154
@ OTP_REV_ID_SEC_BRDCFG
Definition: tisci_otp_revision.h:223
struct tisci_header hdr
Definition: tisci_otp_revision.h:209
Response message to get keycnt, keyrev.
Definition: tisci_otp_revision.h:208
struct tisci_header hdr
Definition: tisci_otp_revision.h:135
struct tisci_header hdr
Definition: tisci_otp_revision.h:82
uint32_t cert_addr_hi
Definition: tisci_otp_revision.h:157
@ OTP_REV_ID_SYSFW
Definition: tisci_otp_revision.h:221
struct tisci_header hdr
Definition: tisci_otp_revision.h:105
@ JTAG_DISABLE_CHECK_GET
Definition: tisci_otp_revision.h:235
Response message after seting swrev.
Definition: tisci_otp_revision.h:92
Response message after setting keyrev.
Definition: tisci_otp_revision.h:165
uint8_t value
Definition: tisci_otp_revision.h:136
Response message after disabling jtag unlock check.
Definition: tisci_otp_revision.h:134
uint8_t identifier
Definition: tisci_otp_revision.h:178
uint32_t keycnt
Definition: tisci_otp_revision.h:210
uint32_t cert_addr_lo
Definition: tisci_otp_revision.h:156
struct tisci_header hdr
Definition: tisci_otp_revision.h:124