|
AM243x MCU+ SDK
11.01.00
|
|
Go to the documentation of this file.
53 #ifndef TISCI_KEYSTORE_H_
54 #define TISCI_KEYSTORE_H_
64 #define KEYSTORE_ABI_MAJ_VALUE 0x00
66 #define KEYSTORE_ABI_MIN_VALUE 0x01
uint32_t keystore_lo
Definition: tisci_keystore.h:86
struct tisci_header hdr
Definition: tisci_keystore.h:162
Request for writing the entire keystore contents.
Definition: tisci_keystore.h:84
Request for exporting the entire keystore contents.
Definition: tisci_keystore.h:119
uint32_t keystore_hi
Definition: tisci_keystore.h:150
Response to the keystore import.
Definition: tisci_keystore.h:161
struct tisci_header hdr
Definition: tisci_keystore.h:100
uint32_t keystore_hi
Definition: tisci_keystore.h:87
uint32_t keystore_lo
Definition: tisci_keystore.h:149
struct tisci_header hdr
Definition: tisci_keystore.h:120
struct tisci_msg_keystore_write_req __attribute__((__packed__))
Response to the keystore export.
Definition: tisci_keystore.h:133
Request for importing a previously exported keystore.
Definition: tisci_keystore.h:147
struct tisci_header hdr
Definition: tisci_keystore.h:148
uint32_t keystore_lo
Definition: tisci_keystore.h:121
struct tisci_header hdr
Definition: tisci_keystore.h:85
Response to the keystore write.
Definition: tisci_keystore.h:99
uint32_t keystore_hi
Definition: tisci_keystore.h:122
struct tisci_header hdr
Definition: tisci_keystore.h:134