AM243x MCU+ SDK  11.01.00

Detailed Description

Determine the result of a hypothetical set frequency operation.

This allows the OS to determine what rate would be set given a set of parameters. A nack will be received if a frequency is not available in the given range.

Parameters
hdrTISCI header
deviceThe device ID that the clock is connected to.
min_freq_hzThe minimum allowable frequency in Hz. This is the minimum allowable programmed frequency and does not account for clock tolerances and jitter.
target_freq_hzThe target clock frequency. A frequency will be found as close to the target frequency as possible.
max_freq_hzThe maximum allowable frequency in Hz. This is the maximum allowable programmed frequency and does not account for clock tolerances and jitter. The firmware will actually accept any frequency up to but not including max + 1.
clkEach device has its own set of clock inputs. This indexes which clock input to query.

If the clock index is 255 or greater, this field should be set to 255 and the full value placed in the clk32 field. This is kept for backwards compatibility with older firmwares.

Parameters
clk32Stores the actual clock index if clk field is set to 255. This field is ignored otherwise. This field can hold the full range of possible clock indexes, but for compatibility with older firmwares should only be used when the index is 255 or greater.

Data Fields

struct tisci_header hdr
 
uint32_t device
 
uint64_t min_freq_hz
 
uint64_t target_freq_hz
 
uint64_t max_freq_hz
 
uint8_t clk
 
uint32_t clk32
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_query_freq_req::hdr

◆ device

uint32_t tisci_msg_query_freq_req::device

◆ min_freq_hz

uint64_t tisci_msg_query_freq_req::min_freq_hz

◆ target_freq_hz

uint64_t tisci_msg_query_freq_req::target_freq_hz

◆ max_freq_hz

uint64_t tisci_msg_query_freq_req::max_freq_hz

◆ clk

uint8_t tisci_msg_query_freq_req::clk

◆ clk32

uint32_t tisci_msg_query_freq_req::clk32