AM243x MCU+ SDK  11.01.00

Detailed Description

Processor Status Wait Response.

Although this message is essentially empty and contains only a header a full data structure is created for consistency in implementation.

Parameters
hdrGeneric TISCI message header.

ACK Response: The status requested was achieved within the constraints provided in request. NAK Response: The processor access is not permitted or operation failed or timedout.

Data Fields

struct tisci_header hdr
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_proc_status_wait_resp::hdr