AM243x MCU+ SDK  11.01.00

Detailed Description

Authenticate and start image.

Parameters
hdrMessage header
certificate_address_loLower 32bit (Little Endian) of certificate
certificate_address_hiHigher 32bit (Little Endian) of certificate

Data Fields

struct tisci_header hdr
 
uint32_t certificate_address_lo
 
uint32_t certificate_address_hi
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_proc_auth_boot_req::hdr

◆ certificate_address_lo

uint32_t tisci_msg_proc_auth_boot_req::certificate_address_lo

◆ certificate_address_hi

uint32_t tisci_msg_proc_auth_boot_req::certificate_address_hi