AM243x MCU+ SDK  11.01.00

Detailed Description

TISCI_MSG_DM_VERSION response struct to provide version info about currently running DM firmware.

Parameters
hdrTISCI header.
versionVersion number of the firmware.
sub_versionSub-version number of the firmware.
patch_versionPatch-version number of the firmware.
abi_majorMajor version number of ABI in use by firmware.
abi_minorMinor version number of ABI in use by firmware.
rm_pm_hal_versionHuman readable rm_pm_hal version string.
sciserver_versionHuman readable Sciserver version string.

Data Fields

struct tisci_header hdr
 
uint16_t version
 
uint8_t sub_version
 
uint8_t patch_version
 
uint8_t abi_major
 
uint8_t abi_minor
 
char rm_pm_hal_version [12]
 
char sciserver_version [26]
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_dm_version_resp::hdr

◆ version

uint16_t tisci_msg_dm_version_resp::version

◆ sub_version

uint8_t tisci_msg_dm_version_resp::sub_version

◆ patch_version

uint8_t tisci_msg_dm_version_resp::patch_version

◆ abi_major

uint8_t tisci_msg_dm_version_resp::abi_major

◆ abi_minor

uint8_t tisci_msg_dm_version_resp::abi_minor

◆ rm_pm_hal_version

char tisci_msg_dm_version_resp::rm_pm_hal_version[12]

◆ sciserver_version

char tisci_msg_dm_version_resp::sciserver_version[26]