AM243x MCU+ SDK  11.01.00
sdl_soc_rti.h
Go to the documentation of this file.
1 /* =============================================================================
2  * Copyright (c) Texas Instruments Incorporated 2023
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  *
32  */
33 
34 #ifndef SDL_SOC_RTI_H_
35 #define SDL_SOC_RTI_H_
36 
37 #include <sdl/include/am64x_am243x/sdlr_soc_baseaddress.h>
38 
39 #ifdef __cplusplus
40 extern "C" {
41 #endif
42 
54 /*======================================================================================================
55 * Required Macros for Instances config
56 ======================================================================================================*/
57 
58 #define SDL_RTI_MAX_INSTANCE (0x07U)
59 #define INSTANCE_INVALID (0x0U)
60 
67 /*************************************************************************************************************
68 * Enum for different RTI module instances
69 **************************************************************************************************************/
70 
71 typedef enum {
72 
74 
77 
80 
84 
86 
87 
88 /*======================================================================================================
89 * This is global array gives the BASE ADDRESS of RTI modules
90 ======================================================================================================*/
91 
92 static uint32_t SDL_RTI_baseAddress[SDL_RTI_MAX_INSTANCE+1U] = {SDL_MCU_RTI0_CFG_BASE, SDL_RTI0_CFG_BASE, \
93  SDL_RTI1_CFG_BASE, SDL_RTI8_CFG_BASE, SDL_RTI9_CFG_BASE, \
94  SDL_RTI10_CFG_BASE, SDL_RTI11_CFG_BASE, \
95  INSTANCE_INVALID};
96 
98  uint32_t *baseAddr);
99 
100 #ifdef __cplusplus
101 }
102 #endif
103 
104 #endif /* SDL_SOC_RTI_H_ */
SDL_INSTANCE_RTI9_CFG
@ SDL_INSTANCE_RTI9_CFG
Definition: sdl_soc_rti.h:79
SDL_INSTANCE_RTI10_CFG
@ SDL_INSTANCE_RTI10_CFG
Definition: sdl_soc_rti.h:81
SDL_INSTANCE_MCU_RTI0_CFG
@ SDL_INSTANCE_MCU_RTI0_CFG
Definition: sdl_soc_rti.h:73
instance
uint8_t instance
Definition: tisci_dkek.h:1
SDL_INSTANCE_RTI8_CFG
@ SDL_INSTANCE_RTI8_CFG
Definition: sdl_soc_rti.h:78
SDL_INSTANCE_INVALID
@ SDL_INSTANCE_INVALID
Definition: sdl_soc_rti.h:83
SDL_INSTANCE_RTI11_CFG
@ SDL_INSTANCE_RTI11_CFG
Definition: sdl_soc_rti.h:82
SDL_RTI_getBaseaddr
int32_t SDL_RTI_getBaseaddr(SDL_RTI_InstanceType instance, uint32_t *baseAddr)
SDL_RTI_MAX_INSTANCE
#define SDL_RTI_MAX_INSTANCE
Definition: sdl_soc_rti.h:58
SDL_INSTANCE_RTI0_CFG
@ SDL_INSTANCE_RTI0_CFG
Definition: sdl_soc_rti.h:75
SDL_INSTANCE_RTI1_CFG
@ SDL_INSTANCE_RTI1_CFG
Definition: sdl_soc_rti.h:76
SDL_RTI_baseAddress
static uint32_t SDL_RTI_baseAddress[SDL_RTI_MAX_INSTANCE+1U]
Definition: sdl_soc_rti.h:92
SDL_RTI_InstanceType
SDL_RTI_InstanceType
Definition: sdl_soc_rti.h:71