AM243x MCU+ SDK  11.01.00
Generic NOR Flash API for single pin mode

Introduction

These APIs try to communicate with whichever flash is connected the OSPI peripheral in 1-1-1 mode. This can be used in bringing up new flashes and mostly used for debug and diagnostic purposes

Functions

int32_t OSPI_lld_norFlashInit1s1s1s (OSPILLD_Handle handle)
 This function initializes the NOR flash to work in 1-1-1 mode. More...
 
void OSPI_lld_norFlashSetCmds (uint8_t rdCmd, uint8_t wrCmd, uint8_t eraseCmd)
 This function sets up internal bookkeeping variables for read, write and erase commands. This API has to be called immediately before OSPI_lld_norFlashInit1s1s1s. More...
 
int32_t OSPI_lld_norFlashReadId (OSPILLD_Handle handle, uint32_t *manufacturerId, uint32_t *deviceId)
 This function tries to read the JEDEC ID from the NOR flash connected to the OSPI peripheral. More...
 
int32_t OSPI_lld_norFlashWrite (OSPILLD_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 This function writes data to the flash at a specified offset. More...
 
int32_t OSPI_lld_norFlashRead (OSPILLD_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 This function reads data from the flash from a specified offset in DAC mode. More...
 
int32_t OSPI_lld_norFlashReadIndirect (OSPILLD_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 This function reads data from the flash from a specified offset in INDAC mode. More...
 
int32_t OSPI_lld_norFlashReadSfdp (OSPILLD_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 This function reads SFDP table from the flash from a specified offset. More...
 
int32_t OSPI_lld_norFlashErase (OSPILLD_Handle handle, uint32_t address)
 This function erases 1 block of data starting from a provided address. More...
 
int32_t OSPI_lld_configResetPin (OSPILLD_Handle handle, uint32_t config)
 This function configures reset functionality. More...
 
int32_t OSPI_lld_configBaudrate (OSPILLD_Handle handle, uint32_t baud)
 Configures baud divider. More...
 
int32_t OSPI_lld_readBaudRateDivFromReg (OSPILLD_Handle handle, uint32_t *baudDiv)
 Return value of baudrate that is programmed in IP register. More...
 
int32_t OSPI_lld_getBaudRateDivFromObj (OSPILLD_Handle handle, uint32_t *baudDiv)
 Return value of baudrate that is saved in OSPI Object. More...
 
int32_t OSPI_lld_setResetPinStatus (OSPILLD_Handle hOspi, uint32_t pinStatus)
 This function activates the RESET pin feature. More...
 

Function Documentation

◆ OSPI_lld_norFlashInit1s1s1s()

int32_t OSPI_lld_norFlashInit1s1s1s ( OSPILLD_Handle  handle)

This function initializes the NOR flash to work in 1-1-1 mode.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_norFlashSetCmds()

void OSPI_lld_norFlashSetCmds ( uint8_t  rdCmd,
uint8_t  wrCmd,
uint8_t  eraseCmd 
)

This function sets up internal bookkeeping variables for read, write and erase commands. This API has to be called immediately before OSPI_lld_norFlashInit1s1s1s.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
rdCmdCommand to be used in single mode read
wrCmdCommand to be used in single mode write/page program
eraseCmdCommand to be used to erase (block or sector)

◆ OSPI_lld_norFlashReadId()

int32_t OSPI_lld_norFlashReadId ( OSPILLD_Handle  handle,
uint32_t *  manufacturerId,
uint32_t *  deviceId 
)

This function tries to read the JEDEC ID from the NOR flash connected to the OSPI peripheral.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
manufacturerIdPointer to a uint32_t variable. This will be filled with the manufacturer ID on success
deviceIdPointer to a uint32_t variable. This will be filled with the device ID on success
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_norFlashWrite()

int32_t OSPI_lld_norFlashWrite ( OSPILLD_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

This function writes data to the flash at a specified offset.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
offsetOffset at which the data is to be written
bufBuffer which has the data to be written to the flash
lenNumber of bytes to be written to the flash
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_norFlashRead()

int32_t OSPI_lld_norFlashRead ( OSPILLD_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

This function reads data from the flash from a specified offset in DAC mode.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
offsetOffset at which the data is to be read from
bufBuffer to which data will be written into
lenNumber of bytes to be read from the flash
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_norFlashReadIndirect()

int32_t OSPI_lld_norFlashReadIndirect ( OSPILLD_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

This function reads data from the flash from a specified offset in INDAC mode.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
offsetOffset at which the data is to be read from
bufBuffer to which data will be written into
lenNumber of bytes to be read from the flash
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_norFlashReadSfdp()

int32_t OSPI_lld_norFlashReadSfdp ( OSPILLD_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

This function reads SFDP table from the flash from a specified offset.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
offsetOffset at which the data is to be read from
bufBuffer to which data will be written into
lenNumber of bytes to be read from the flash
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_norFlashErase()

int32_t OSPI_lld_norFlashErase ( OSPILLD_Handle  handle,
uint32_t  address 
)

This function erases 1 block of data starting from a provided address.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
addressAddress of the data block to be erased. This address should be block aligned.
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_configResetPin()

int32_t OSPI_lld_configResetPin ( OSPILLD_Handle  handle,
uint32_t  config 
)

This function configures reset functionality.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPI_Handle returned from an OSPI_open()
configreset config
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_configBaudrate()

int32_t OSPI_lld_configBaudrate ( OSPILLD_Handle  handle,
uint32_t  baud 
)

Configures baud divider.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPI_Handle returned from an OSPI_open()
baudbaudrate from 2 to 32 and divisible by 2
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_readBaudRateDivFromReg()

int32_t OSPI_lld_readBaudRateDivFromReg ( OSPILLD_Handle  handle,
uint32_t *  baudDiv 
)

Return value of baudrate that is programmed in IP register.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPI_Handle returned from an OSPI_open()
baudDivpointer to memory into which baudrate will be written
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_getBaudRateDivFromObj()

int32_t OSPI_lld_getBaudRateDivFromObj ( OSPILLD_Handle  handle,
uint32_t *  baudDiv 
)

Return value of baudrate that is saved in OSPI Object.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_init()
baudDivpointer to memory into which baudrate will be written
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_setResetPinStatus()

int32_t OSPI_lld_setResetPinStatus ( OSPILLD_Handle  hOspi,
uint32_t  pinStatus 
)

This function activates the RESET pin feature.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
hOspiAn OSPILLD_Handle returned from an OSPI_open()
pinStatuspinStatus - HIGH/LOW
Returns
SystemP_SUCCESS on success, SystemP_FAILURE otherwise