AM243x MCU+ SDK  11.01.00

Introduction

These APIs try are used for the phy tuning

Functions

uint32_t OSPI_lld_getInputClk (OSPILLD_Handle handle)
 This function returns the input clk frequency OSPI was programmed at. More...
 
uint32_t OSPI_lld_isDacEnable (OSPILLD_Handle handle)
 This function checks if the Direct Access Controller is enabled. More...
 
uint32_t OSPI_lld_isDmaEnable (OSPILLD_Handle handle)
 This function checks if DMA is enabled for reads. More...
 
uint32_t OSPI_lld_isIntrEnable (OSPILLD_Handle handle)
 This function checks if interrupts are enabled. More...
 
uint32_t OSPI_lld_isPhyEnable (OSPILLD_Handle handle)
 This function checks if the OSPI PHY controller is enabled. More...
 
int32_t OSPI_lld_enableDDR (OSPILLD_Handle handle)
 This function enables the Dual Data Rate (DDR) More...
 
int32_t OSPI_lld_enableSDR (OSPILLD_Handle handle)
 This function enables the Single Data Rate (SDR) More...
 
int32_t OSPI_lld_enableDdrRdCmds (OSPILLD_Handle handle)
 This function sets DDR bit in INSTR_RD register for RD commands. More...
 
int32_t OSPI_lld_setRdDataCaptureDelay (OSPILLD_Handle handle, uint32_t rdDataCapDelay)
 This function sets read data capture cycles in the OSPI controller. More...
 
void OSPI_lld_setNumAddrBytes (OSPILLD_Handle handle, uint32_t numAddrBytes)
 This function set the number of bytes used to send address while reading or writing to flash memory. More...
 
void OSPI_lld_setDeviceSize (OSPILLD_Handle handle, uint32_t pageSize, uint32_t blkSize)
 This function sets the block size and page size of the flash to the device size register in OSPI. More...
 
void OSPI_lld_setCmdDummyCycles (OSPILLD_Handle handle, uint32_t cmdDummyCycles)
 This function sets appropriate dummy cycles to be used while sending STIG commands to flash. More...
 
void OSPI_lld_setReadDummyCycles (OSPILLD_Handle handle, uint32_t dummyCycles)
 This function sets appropriate dummy cycles for flash read. More...
 
void OSPI_lld_setWriteDummyCycles (OSPILLD_Handle handle, uint32_t dummyCycles)
 This function sets appropriate dummy cycles for flash write. More...
 
void OSPI_lld_setPhyEnableSuccess (OSPILLD_Handle handle, uint32_t success)
 This function sets the phyEnableSuccess field in OSPILLD_Object. Has to be called from flash driver. More...
 
void OSPI_lld_setModeBits (OSPILLD_Handle handle, uint32_t modeBits)
 This function sets mode bits in the mode bit field of OSPI config register. More...
 
void OSPI_lld_enableModeBitsCmd (OSPILLD_Handle handle)
 This function enables mode bits transmission while sending CMDs. More...
 
void OSPI_lld_enableModeBitsRead (OSPILLD_Handle handle)
 This function enables mode bits transmission while reading. More...
 
uint32_t OSPI_lld_getPhyEnableSuccess (OSPILLD_Handle handle)
 This function fetches the phyEnableSuccess field in OSPILLD_Object. More...
 
uint32_t OSPI_lld_getProtocol (OSPILLD_Handle handle)
 This function returns the current protocol for which the transfer lines in OSPI driver is configured for. More...
 
void OSPI_lld_setProtocol (OSPILLD_Handle handle, uint32_t protocol)
 This function sets the number of transfer lines in the OSPI driver to set the requested protocol. More...
 
void OSPI_lld_setDualOpCodeMode (OSPILLD_Handle handle)
 This function sets OSPI controller to use dual byte opcodes. More...
 
void OSPI_lld_clearDualOpCodeMode (OSPILLD_Handle handle)
 This function sets OSPI controller to not use dual byte opcodes. More...
 
void OSPI_lld_setXferOpCodes (OSPILLD_Handle handle, uint8_t readCmd, uint8_t pageProgCmd)
 This function sets the opcodes for reading and page programming the flash. More...
 
void OSPI_lld_setCmdExtType (OSPILLD_Handle handle, uint32_t cmdExtType)
 This function sets the type of command extension used in dual byte opcode mode. More...
 
int32_t OSPI_lld_enableDacMode (OSPILLD_Handle handle)
 This function enables the Direct Access Mode. More...
 
int32_t OSPI_lld_disableDacMode (OSPILLD_Handle handle)
 This function disables the Direct Access Mode. More...
 
uint32_t OSPI_lld_getFlashDataBaseAddr (OSPILLD_Handle handle)
 This function gets the SOC mapped data base address of the flash. More...
 

Function Documentation

◆ OSPI_lld_getInputClk()

uint32_t OSPI_lld_getInputClk ( OSPILLD_Handle  handle)

This function returns the input clk frequency OSPI was programmed at.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
OSPI RCLK in Hertz

◆ OSPI_lld_isDacEnable()

uint32_t OSPI_lld_isDacEnable ( OSPILLD_Handle  handle)

This function checks if the Direct Access Controller is enabled.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
1 if DAC is enabled, 0 otherwise

◆ OSPI_lld_isDmaEnable()

uint32_t OSPI_lld_isDmaEnable ( OSPILLD_Handle  handle)

This function checks if DMA is enabled for reads.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
1 if DMA is enabled, 0 otherwise

◆ OSPI_lld_isIntrEnable()

uint32_t OSPI_lld_isIntrEnable ( OSPILLD_Handle  handle)

This function checks if interrupts are enabled.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
1 if interrupts are enabled, 0 otherwise

◆ OSPI_lld_isPhyEnable()

uint32_t OSPI_lld_isPhyEnable ( OSPILLD_Handle  handle)

This function checks if the OSPI PHY controller is enabled.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
1 if PHY is enabled, 0 otherwise

◆ OSPI_lld_enableDDR()

int32_t OSPI_lld_enableDDR ( OSPILLD_Handle  handle)

This function enables the Dual Data Rate (DDR)

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
OSPI_SYSTEM_SUCCESS if DDR successfully enabled, else error on failure

◆ OSPI_lld_enableSDR()

int32_t OSPI_lld_enableSDR ( OSPILLD_Handle  handle)

This function enables the Single Data Rate (SDR)

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
OSPI_SYSTEM_SUCCESS if SDR successfully enabled, else error on failure

◆ OSPI_lld_enableDdrRdCmds()

int32_t OSPI_lld_enableDdrRdCmds ( OSPILLD_Handle  handle)

This function sets DDR bit in INSTR_RD register for RD commands.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
OSPI_SYSTEM_SUCCESS if SDR successfully enabled, else error on failure

◆ OSPI_lld_setRdDataCaptureDelay()

int32_t OSPI_lld_setRdDataCaptureDelay ( OSPILLD_Handle  handle,
uint32_t  rdDataCapDelay 
)

This function sets read data capture cycles in the OSPI controller.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
rdDataCapDelayNumber of read data capture cycles to be programmed
Returns
OSPI_SYSTEM_SUCCESS if read data capture cycles successfully set, else error on failure

◆ OSPI_lld_setNumAddrBytes()

void OSPI_lld_setNumAddrBytes ( OSPILLD_Handle  handle,
uint32_t  numAddrBytes 
)

This function set the number of bytes used to send address while reading or writing to flash memory.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
numAddrBytesNumber of address bytes to be used while sending addresses.

◆ OSPI_lld_setDeviceSize()

void OSPI_lld_setDeviceSize ( OSPILLD_Handle  handle,
uint32_t  pageSize,
uint32_t  blkSize 
)

This function sets the block size and page size of the flash to the device size register in OSPI.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
pageSizePage size of the flash in bytes
blkSizeBlock size of the flash in bytes

◆ OSPI_lld_setCmdDummyCycles()

void OSPI_lld_setCmdDummyCycles ( OSPILLD_Handle  handle,
uint32_t  cmdDummyCycles 
)

This function sets appropriate dummy cycles to be used while sending STIG commands to flash.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
cmdDummyCyclesDummy cycles to be used for STIG cmd

◆ OSPI_lld_setReadDummyCycles()

void OSPI_lld_setReadDummyCycles ( OSPILLD_Handle  handle,
uint32_t  dummyCycles 
)

This function sets appropriate dummy cycles for flash read.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
dummyCyclesNumber of dummy cycles

◆ OSPI_lld_setWriteDummyCycles()

void OSPI_lld_setWriteDummyCycles ( OSPILLD_Handle  handle,
uint32_t  dummyCycles 
)

This function sets appropriate dummy cycles for flash write.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
dummyCyclesNumber of dummy cycles

◆ OSPI_lld_setPhyEnableSuccess()

void OSPI_lld_setPhyEnableSuccess ( OSPILLD_Handle  handle,
uint32_t  success 
)

This function sets the phyEnableSuccess field in OSPILLD_Object. Has to be called from flash driver.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
successSet this to 1 if phy enable was successful. 0 otherwise

◆ OSPI_lld_setModeBits()

void OSPI_lld_setModeBits ( OSPILLD_Handle  handle,
uint32_t  modeBits 
)

This function sets mode bits in the mode bit field of OSPI config register.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
modeBitsNumber of mode bits to be set

◆ OSPI_lld_enableModeBitsCmd()

void OSPI_lld_enableModeBitsCmd ( OSPILLD_Handle  handle)

This function enables mode bits transmission while sending CMDs.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()

◆ OSPI_lld_enableModeBitsRead()

void OSPI_lld_enableModeBitsRead ( OSPILLD_Handle  handle)

This function enables mode bits transmission while reading.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()

◆ OSPI_lld_getPhyEnableSuccess()

uint32_t OSPI_lld_getPhyEnableSuccess ( OSPILLD_Handle  handle)

This function fetches the phyEnableSuccess field in OSPILLD_Object.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
1 if phyEnable was successful, 0 otherwise.

◆ OSPI_lld_getProtocol()

uint32_t OSPI_lld_getProtocol ( OSPILLD_Handle  handle)

This function returns the current protocol for which the transfer lines in OSPI driver is configured for.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
protocol Protocol being used

◆ OSPI_lld_setProtocol()

void OSPI_lld_setProtocol ( OSPILLD_Handle  handle,
uint32_t  protocol 
)

This function sets the number of transfer lines in the OSPI driver to set the requested protocol.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
protocolProtocol to be used

◆ OSPI_lld_setDualOpCodeMode()

void OSPI_lld_setDualOpCodeMode ( OSPILLD_Handle  handle)

This function sets OSPI controller to use dual byte opcodes.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()

◆ OSPI_lld_clearDualOpCodeMode()

void OSPI_lld_clearDualOpCodeMode ( OSPILLD_Handle  handle)

This function sets OSPI controller to not use dual byte opcodes.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()

◆ OSPI_lld_setXferOpCodes()

void OSPI_lld_setXferOpCodes ( OSPILLD_Handle  handle,
uint8_t  readCmd,
uint8_t  pageProgCmd 
)

This function sets the opcodes for reading and page programming the flash.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
readCmdCommand opcode to be used for reading from the flash
pageProgCmdCommand opcode to be used for writing to / programming the flash

◆ OSPI_lld_setCmdExtType()

void OSPI_lld_setCmdExtType ( OSPILLD_Handle  handle,
uint32_t  cmdExtType 
)

This function sets the type of command extension used in dual byte opcode mode.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
cmdExtTypeType of command extension used. As of now only two types are supported - REPEAT and INVERSE

◆ OSPI_lld_enableDacMode()

int32_t OSPI_lld_enableDacMode ( OSPILLD_Handle  handle)

This function enables the Direct Access Mode.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_disableDacMode()

int32_t OSPI_lld_disableDacMode ( OSPILLD_Handle  handle)

This function disables the Direct Access Mode.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_getFlashDataBaseAddr()

uint32_t OSPI_lld_getFlashDataBaseAddr ( OSPILLD_Handle  handle)

This function gets the SOC mapped data base address of the flash.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
Data BaseAddress of the flash