AM243x MCU+ SDK  11.01.00
gp_timer/v0/gp_timer.h File Reference

Introduction

GPTIMER Driver API/interface file.

Go to the source code of this file.

Data Structures

struct  GPTIMER_HwAttrs
 GPTIMER Hardware attributes. More...
 
struct  GPTIMER_Params
 GPTIMER Parameters. More...
 
struct  GPTIMER_Compare_Config
 GPTIMER Compare Mode Configuration Parameters. More...
 
struct  GPTIMER_Capture_Config
 GPTIMER Capture Mode Configuration Parameters. More...
 
struct  GPTIMER_PWM_Config
 GPTIMER PWM Generation Mode Configuration Parameters. More...
 
struct  GPTIMER_Object
 GPTIMER driver object. More...
 
struct  GPTIMER_Config
 GPTIMER Global Configuration. More...
 

Macros

MACROS for the possible Configurations of GPTIMER.

#define GPTIMER_MODE_CONFIG_FREE_RUN   ((uint8_t) 0U)
 Free Running Mode. More...
 
#define GPTIMER_MODE_CONFIG_INPUT_CAPTURE   ((uint8_t) 1U)
 Input Capture Mode. More...
 
#define GPTIMER_MODE_CONFIG_OUTPUT_COMPARE   ((uint8_t) 2U)
 Output Compare Mode. More...
 
#define GPTIMER_MODE_CONFIG_PWM_GEN   ((uint8_t) 3U)
 PWM Generation Mode. More...
 
MACROS for the possible Configurations of GPTIMER input Capture Mode.

#define GPTIMER_INPUT_CAPTURE_MODE_SINGLE   ((uint32_t) 0U)
 Capture Single Event. More...
 
#define GPTIMER_INPUT_CAPTURE_MODE_SECOND   ((uint32_t) 1U)
 Capture Two Events. More...
 
MACROS for the possible Configurations of GPTIMER input Capture event.

#define GPTIMER_INPUT_CAPTURE_EVENT_NO_CAPTURE   ((uint32_t) 0U)
 No Event Capture. More...
 
#define GPTIMER_INPUT_CAPTURE_EVENT_RISING   ((uint32_t) 1U)
 Capture Event on Rising Edge. More...
 
#define GPTIMER_INPUT_CAPTURE_EVENT_FALLING   ((uint32_t) 2U)
 Capture Event on Falling Edge. More...
 
#define GPTIMER_INPUT_CAPTURE_EVENT_EDGE   ((uint32_t) 3U)
 Capture Event on both rising and falling edge. More...
 
MACROS for the possible Configurations of GPTIMER PWM output Trigger.

#define GPTIMER_PWM_OUT_NO_TRIGGER   ((uint32_t) 0U)
 PWM Uses No Trigger. More...
 
#define GPTIMER_PWM_OUT_OVERFLOW_TRIGGER   ((uint32_t) 1U)
 PWM uses overflow as a Trigger. More...
 
#define GPTIMER_PWM_OUT_OVERFLOW_MATCH_TRIGGER   ((uint32_t) 2U)
 PWM uses overflow and compare match as a trigger. More...
 
MACROS for the possible Configurations of PWM output Pin Default Val.

#define GPTIMER_PWM_OUT_PIN_DEFAULT_0   ((uint32_t) 0U)
 Pin Default value 0. More...
 
#define GPTIMER_PWM_OUT_PIN_DEFAULT_1   ((uint32_t) 1U)
 Pin Default value 0. More...
 
MACROS for the possible Configurations of PWM output Pin Modulation

Type.

#define GPTIMER_PWM_OUT_PIN_MODULATION_PULSE   ((uint32_t) 0U)
 Pin Modulation type Pulse. More...
 
#define GPTIMER_PWM_OUT_PIN_MODULATION_TOGGLE   ((uint32_t) 1U)
 Pin Modulation type Toggle. More...
 
MACROS for the possible IRQ Status Mask.

#define TIMER_IRQ_TCAR_IT_FLAG_MASK   (uint32_t)0x04U
 
#define TIMER_IRQ_OVF_IT_FLAG_MASK   (uint32_t)0x02U
 
#define TIMER_IRQ_MAT_IT_FLAG_MASK   (uint32_t)0x01U
 

Typedefs

typedef struct GPTIMER_Config_s * GPTIMER_Handle
 A handle that is returned from a GPTIMER_open() call. More...
 
typedef void(* GPTIMER_OverflowCallbackFxn) (GPTIMER_Handle handle)
 GPTIMER Overflow Callback Function. More...
 
typedef void(* GPTIMER_CompareMatchCallbackFxn) (GPTIMER_Handle handle)
 GPTIMER Compare Match Callback Function. More...
 
typedef void(* GPTIMER_CaptureCallbackFxn) (GPTIMER_Handle handle)
 GPTIMER Capture Callback Function. More...
 

Functions

void GPTIMER_init (void)
 Initialize the GPTIMER module. More...
 
void GPTIMER_deinit (void)
 De-initialize the GPTIMER module. More...
 
void GPTIMER_Params_init (GPTIMER_Params *params)
 Function to set default values of GPTIMER_Params in params. More...
 
GPTIMER_Handle GPTIMER_open (uint32_t idx, const GPTIMER_Params *params)
 Open the GPTIMER at index idx with parameters params. More...
 
void GPTIMER_close (GPTIMER_Handle handle)
 Function to close the GPTIMER Peripheral specified by the handle. More...
 
void GPTIMER_start (GPTIMER_Handle handle)
 Start the Timer. More...
 
void GPTIMER_stop (GPTIMER_Handle handle)
 Stop the TImer. More...
 
uint32_t GPTIMER_getCount (GPTIMER_Handle handle)
 Get timer counter value. More...
 
void GPTIMER_setCount (GPTIMER_Handle handle, uint32_t value)
 Set timer counter value. More...
 
void GPTIMER_setCompareVal (GPTIMER_Handle handle, uint32_t value)
 Set timer compare value. More...
 
uint32_t GPTIMER_getTimerCaptureVal1 (GPTIMER_Handle handle)
 Get Timer Capture Value 1. More...
 
uint32_t GPTIMER_getTimerCaptureVal2 (GPTIMER_Handle handle)
 Get Timer Capture Value 2. More...
 
int32_t GPTIMER_setFreeRunMode (GPTIMER_Handle handle)
 Change Timer Configuration to freerun mode. More...
 
int32_t GPTIMER_setIpCaptureMode (GPTIMER_Handle handle, GPTIMER_Capture_Config *config)
 Change Timer Configuration to Input capture mode. More...
 
int32_t GPTIMER_setOpCompareMode (GPTIMER_Handle handle, GPTIMER_Compare_Config *config)
 Change Timer Configuration to output compare mode. More...
 
int32_t GPTIMER_setPWMGenMode (GPTIMER_Handle handle, GPTIMER_PWM_Config *config)
 Change Timer Configuration to PWM generation mode. More...
 
void GPTIMER_setCallbackFxn (GPTIMER_Handle handle, GPTIMER_OverflowCallbackFxn overflowCbFxn, GPTIMER_CompareMatchCallbackFxn compMatchCbFxn, GPTIMER_CaptureCallbackFxn captureCbFxn)
 Update Callback Functions. More...
 
uint32_t GPTIMER_getIRQStatus (GPTIMER_Handle handle)
 Get IRQ status. More...
 
void GPTIMER_clearIRQStatus (GPTIMER_Handle handle, uint32_t irqMask)
 Clear IRQ status bit. More...
 
void GPTIMER_enableInterruptStatus (GPTIMER_Handle handle, uint32_t irqMask)
 Enable IRQ Status, Corresponding status bit will be set in case of an event. Interrupt and callback will be called if interrupt is registered. More...
 
void GPTIMER_disableInterruptStatus (GPTIMER_Handle handle, uint32_t irqMask)
 Disable IRQ Status. More...