AM243x MCU+ SDK  11.01.00
Release Notes 11.00.00

Attention
1. Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
2. A53 support is applicable for AM64x only. It is NOT applicable for AM243x.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless noted otherwise, the SW modules would work in both FreeRTOS and NORTOS environment.
Unless noted otherwise, the SW modules would work on any of the R5F's present on the SOC.
Unless noted otherwise, the SW modules would work on all supported EVMs
M4F drivers support only MCU domain peripheral and peripheral instance while R5/A53 supports MAIN domain peripheral and peripheral instance.
Attention
Klockwork Static Analysis report is not updated for this release

New in this Release

Feature Module
LLD drivers for FSI Drivers
ECC example for R5F cache SDL

Device and Validation Information

SOC Supported CPUs Boards Host PC
AM243x R5F, M4F AM243x GP EVM (referred to as am243x-evm in code),
AM243x LAUNCHPAD (referred to as am243x-lp in code)
Windows 10 64b or Ubuntu 18.04 64b

Tools, Compiler and Other Open Source SW Module Information

Tools / SW module Supported CPUs Version
Code Composer Studio R5F, M4F, A53 12.8.1
SysConfig R5F, M4F, A53 1.22.0, build 3893
TI ARM CLANG R5F, M4F 4.0.1.LTS
GCC AARCH64 A53 9.2-2019.12
GCC ARM R5F 7-2017-q4-major (AM64x only)
FreeRTOS Kernel R5F, M4F, A53 11.1.0
FreeRTOS SMP Kernel A53 202110.00-SMP
Tiny USB R5F 0.14.0
LwIP R5F STABLE-2_2_0_RELEASE
Mbed-TLS R5F mbedtls-2.13.1

SDK Components

SYSFW / DMSC

Version 11.00.07
Release Notes LINK
User Guide LINK

Key Features

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
GUI for UART Uniflash Tool (No support for EMMC flashing) Bootloader

Features not supported in release

AM243X LAUNCHPAD not tested/not supported features

Below features are not support on AM243X LAUNCHPAD due to SOC or board constraints,

  • DDR is not supported on the AM243X 11x11 SOC used in AM243X LAUNCHPAD.
  • I2C temperature sensor example not validated, due to board limitation.
  • M4F examples for UART, MCSPI and GPIO not validated, due to board limitation.

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F, M4F, A53 NA Task, Task notification, interrupts, semaphores, mutexes, timers, event groups. ROV views in CCS IDE, Task load measurement using FreeRTOS run time statistics APIs. Only single core A53 FreeRTOS is supported. Second core is NOT used.
FreeRTOS SMP Kernel A53 NA Task, Task notification, interrupts, semaphores, mutexes, timers, event groups. ROV views in CCS IDE, Task load measurement using FreeRTOS run time statistics APIs. -
FreeRTOS POSIX R5F, M4F, A53 NA pthread, mqueue, semaphore, clock -
NO RTOS R5F, M4F, A53 NA See Driver Porting Layer (DPL) below Only single core A53 NORTOS is supported. Second core is NOT used.

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Address Translate M4F YES FreeRTOS, NORTOS Use RAT to allow M4F access to peripheral address space -
Cache R5F, A53 YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F, M4F, A53 YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CpuId R5F NA FreeRTOS, NORTOS Verify Core ID and Cluster ID that application is running -
CycleCounter R5F, M4F, A53 NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F, M4F, A53 YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F, M4F, A53 NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F, M4F, A53 YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore -
MPU R5F, M4F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
MMU A53 YES NORTOS Setup MMU and control access to address space -
Semaphore R5F, M4F, A53 NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F, M4F, A53 NA FreeRTOS Create, delete tasks -
Timer R5F, M4F, A53 YES FreeRTOS, NORTOS Configure arbitrary timers -
Event R5F, M4F YES FreeRTOS Setting, getting, clearing, and waiting of Event bits -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Bootloader R5FSS0-0 YES NORTOS Boot modes: OSPI, OSPI XIP, UART, SD. All R5F's, M4F, A53 NORTOS/FreeRTOS/Linux boot. RPRC, multi-core image format, DDR init SBL OSPI XIP for A53

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
ADC R5F, A53 YES Yes Single conversion (one-shot mode), interrupt mode, DMA mode Continuous conversion not tested
CRC R5F YES No CRC in full CPU mode -
DDR R5F YES No Tested LPDDR4 at 400MHz frequency. -
ECAP R5F, A53 YES No Frequency, Duty cycle, interrupt mode -
EPWM R5F, A53 YES No Different Frequency, Duty cycle, interrupt mode, Deadband and chopper module Tripzone module not tested
EQEP R5F, A53 YES No Signal Frequency and Direction, interrupt mode -
FSI (RX/TX) R5F YES No RX, TX, polling, interrupt mode, single/dual lanes -
GPIO R5F, M4F, A53 YES No Basic input/output, GPIO as interrupt -
GTC R5F, A53 NA No Enable GTC, setting FID (Frequency indicator) -
I2C R5F, M4F, A53 YES No Controller mode, basic read/write, polling and interrupt mode Target mode not supported. M4F not tested due to EVM limitation
IPC Notify R5F, M4F, A53 YES No Low latency IPC between RTOS/NORTOS CPUs -
IPC Rpmsg R5F, M4F, A53 YES No RPMessage protocol based IPC for all R5F, M4F, A53 running NORTOS/FreeRTOS/Linux -
MCAN R5F, A53 YES No RX, TX, interrupt and polling mode -
MCSPI R5F, M4F, A53 YES Yes Controller/Peripheral mode, basic read/write, polling, interrupt and DMA mode -
MDIO R5F NA No Register read/write, link status and link interrupt enable API -
MMCSD R5F, A53 YES Yes Raw read/write and file I/O on MMCSD0 eMMC, and MMCSD1 SD. eMMC tested till HS SDR mode (8-bit data, 52 MHz), SD tested till SD HS mode (4-bit, 25 MHz) Interrupt mode not tested
OSPI R5F, A53 YES Yes Read direct, Write indirect, Read/Write commands, DMA for read, PHY Mode Interrupt mode not supported
PCIe R5F YES No Buffer Transfer between EP and RC modes. Legacy interrupt MSI and MSIx capability
Pinmux R5F, M4F, A53 YES No Tested with multiple peripheral pinmuxes -
PRUICSS R5F YES No Tested with Ethercat, EtherNet/IP, IO-Link, ICSS-EMAC, HDSL, EnDat -
SOC R5F, M4F, A53 YES No lock/unlock MMRs, get CPU clock, CPU name, clock enable, set frequency, SW Warm/POR Reset, Address Translation -
Sciclient R5F, M4F, A53 YES No Tested with clock setup, module on/off -
SPINLOCK R5F, M4F, A53 NA No Lock, unlock HW spinlocks -
UART R5F, M4F, A53 YES Yes Basic read/write, polling, interrupt mode, HW flow control not tested. DMA mode not supported
UDMA R5F, A53 YES Yes Basic memory copy, SW trigger, Chaining -
WDT R5F, A53 YES No Interrupt after watchdog expiry Reset not supported

Software Diagnostic Library (SDL)

SDL Module Supported CPUs SysConfig Support
ESM M4F, R5F NO
MCRC M4F, R5F NO
RTI M4F, R5F NO
DCC M4F, R5F NO
VTM M4F, R5F NO
STOG M4F, R5F NO
PBIST M4F, R5F NO
MTOG M4F NO
POK M4F, R5F NO
ECC M4F, R5F NO
ROM Checksum R5F NO

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES I2C based EEPROM -
ETHPHY R5F YES Ethernet Phy configuration for EtherCAT SubDevice example -
Flash R5F YES XSPI, OSPI, QSPI based flash, Octal, Quad mode, DDR mode All vendor flash types not tested
LED R5F, A53 YES GPIO , I2C IO expander based LED control, I2C based industrial LEDs(TPIC2810) -

File System

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
FreeRTOS+FAT R5F YES FreeRTOS, NORTOS File read, write, create. FAT partition and mounting File I/O with FreeRTOS

CMSIS

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
CMSIS DSP R5F NA FreeRTOS, NORTOS Basic math, complex math, controller, fast math, filtering, Matrix, statistics, transform -

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
TSN R5F NO FreeRTOS gPTP IEEE 802.1 AS-2020 compliant gPTP stack, End Nodes and Bridge mode support, YANG data model configuration Multi-Clock Domain
A53 NO FreeRTOS
LwIP R5F YES FreeRTOS, NORTOS TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, TCP iperf, scatter-gather, DSCP priority mapping, LwIP bridge, shared memory driver Other LwIP features
A53 YES FreeRTOS
Ethernet driver (ENET) R5F YES FreeRTOS, NORTOS Ethernet as port using CPSW, MAC loopback and PHY loopback, Layer 2 MAC, Packet Timestamping, CPSW Switch, Policer and Classifier, MDIO Manual Mode, CBS (IEEE 802.1Qav) on CPSW, IET (IEEE 802.1Qbu) on CPSW, Strapped PHY (Early Ethernet), cut through switch on CPSW RMII mode
A53 YES FreeRTOS
Mbed-TLS R5F NO FreeRTOS Tested software cryptography after porting, used mbedTLS with LwIP to implement HTTPS server Hardware offloaded cryptography

USB

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
USB SoC Porting Layer R5F YES FreeRTOS, NORTOS USB 2.0 device mode USB 3.0
USB Device Driver R5F NO FreeRTOS, NORTOS USB 2.0 device mode USB Host driver
TinyUSB Core and CDC Driver R5F NO FreeRTOS, NORTOS USB device with CDC class USB Host, other USB device class drivers
TinyUSB Core and DFU Driver R5F NO FreeRTOS, NORTOS USB device with DFU class USB Host, other USB device class drivers

SECURITY

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
SA2UL AES R5F YES NORTOS AES CBC-128 encryption and decryption, AES CBC-256 encryption and decryption, AES ECB-128 encryption and decryption, AES ECB-256 encryption and decryption, AES CMAC-128, AES CMAC-256 -
SA2UL SHA R5F YES NORTOS SHA 512 single shot and multi-shot, SHA 256 single shot and multi-shot, HMAC SHA-256, HMAC SHA-512, HMAC SHA-1 -
SA2UL RNG R5F YES NORTOS RNG generate random number with size of 4 words(128 bit) -
SA2UL PKA R5F YES NORTOS RSA Encryption and Decryption support upto 4k bit, RSA Signing and Verification support upto 4k bit, ECDSA Signing and Verification support with P-256 and P-384 curves -

Demos

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
Benchmark demo 4xR5F's YES NORTOS CFFT, FIR and FOC benchmarks ADC/PWM benchmark

Fixed Issues

ID Head Line Module Applicable Releases Applicable Devices
EXT_SITMPUSW-61 UART DMA LLD SysConfig generates incorrect files UART 10.01.00 onwards AM64x, AM243x
EXT_SITMPUSW-62 SPI0_CS1 pin can't be added Pinmux 10.01.00 onwards AM64x, AM243x
EXT_SITMPUSW-63 Undeclared Identifier for MCU GPIO interrupt router GPIO 10.01.00 onwards AM64x, AM243x
EXT_SITMPUSW-64 AM64x: a53 core: Unable to flash Examples >1.2MB size using UART boot mode Uniflash 10.01.00 onwards AM64x
EXT_SITMPUSW-65 At some random timing Pinmux registers (PADCFG) are not updated properly Pinmux 10.01.00 onwards AM64x, AM243x
EXT_SITMPUSW-66 Dhrystone benchmark example has CPU clock hard code Benchmark 10.00.00 onwards AM64x, AM243x
EXT_SITMPUSW-67 Comparing unsigned integer value with signed integer Sysconfig 10.00.00 onwards AM64x, AM243x
EXT_SITMPUSW-68 Load from JSON button fails to load the JSON flash config file Flash 10.00.00 onwards AM64x, AM243x
EXT_SITMPUSW-69 MMCSD_RAW_IO example does not boot with SBL_EMMC Flash 10.00.00 onwards AM64x, AM243x
EXT_SITMPUSW-70 SBL_DFU booting but not initializing DFU interface to receive the application image USB DFU 10.00.00 onwards AM64x, AM243x
EXT_EP-12290 SysConfig 1.21 creates incorrect MCSPI structs in ti_drivers_config.c Sysconfig 10.00.00 onwards AM64x, AM243x
EXT_SITMPUSW-71 Not able to open drivers for MCU_I2C1 I2C 10.01.00 onwards AM64x, AM243x
EXT_SITMPUSW-72 Inline ECC init sequence not matching the steps mentioned in TRM for AM243/AM64x DDR 10.01.00 onwards AM64x, AM243x
EXT_EP-12324 gSDL_pvt_poly_golden has to be used in SDL_vtmPrepLookupTable API instead of gSDL_pvt_poly SDL 11.00.00 AM64x, AM243x
EXT_EP-12319 ScrambleValue for the MCU PBIST instance has to updated for AM64x/AM243x SDL 11.00.00 AM64x, AM243x
EXT_EP-12318 SDL_ECC_aggrTransBaseAddressTable declared without extern keyword SDL 11.00.00 AM64x, AM243x
PROC_SDL-8891 AM243x: POK: Example is stuck on M4F core SDL 11.00.00 AM243x
EXT_SITMPUSW-55 AM64x: ENET : A53 : TCP Throughput drop in iperf application running on FreeRTOS A53 core Ethernet 11.00.00 AM64x

Issue is seen only with 1Gbps Full Duplex link speed. Any other link speed such as 100 Mbps link speed shall work seemlessly

EXT_SITMPUSW-56 AM64X: ENET: Data inconsitency with MAC loopback application with FreeRTOS running on A53 core Ethernet 11.00.00 AM64x Issue is seen in release mode. In debug mode it works fine.
EXT_EP-12337 ICSSG: TAPRIO - Firmware can’t handle base-time which is not a multiple of cycle-time. Ethernet (ICSSG) 10.00.00 onwards AM64x, AM243x
EXT_EP-12338 ICSSG: PA_STATS are not sequenced properly Ethernet (ICSSG) 09.02.00 onwards AM64x, AM243x
EXT_EP-12339 Switch/MAC/HSR firmware does not drop corrupted packets Ethernet (ICSSG) 10.01.00 onwards

AM64x, AM243x

Known Issues

ID Head Line Module Applicable Releases Applicable Devices Workaround
EXT_SITMPUSW-22 Pcie_benchmark, Pcie_buf_transfer, Pcie_legacy_irq, Pcie_msi_irq, Pcie_msix_irq and sbl_pcie are broken on 9.2.1 release PCIE 9.2.1 onwards AM64x, AM243x None.
EXT_SITMPUSW-21 DMA not working with ADC FIFO 1 ADC 7.3.0 onwards AM64x, AM243x

Use ADC FIFO 0

EXT_SITMPUSW-23 [Docs] Sysfw RM/PM documentation doesn't specify AM243x Docs 8.0.0 onwards AM243x -
EXT_SITMPUSW-24 PKA ECDSA sign verify is not working for P-521 and BrainPool P-512R1 curves SECURITY 8.2.0 onwards AM64x, AM243x -
EXT_SITMPUSW-25 Last 512KB of memory is not accessible in dev boot mode flow SBL 8.4.0 AM64x, AM243x Use other boot modes
EXT_SITMPUSW-26 PCIe MSI error when connected to Linux Root Complex PCIe 8.6.0 AM64x, AM243x -
EXT_SITMPUSW-73 OSPI_readDirect and OSPI_isPhyEnable do not correctly check if the PHY is enabled OSPI 10.1.0 onwards AM64x, AM243x None.
EXT_SITMPUSW-77 Modify Read capture delay logic for Tap Mode SDL 10.1.0 onwards AM64x, AM243x None
EXT_SITMPUSW-81 MCU+ SDK: EPWM_tbTimebaseClkCfg does not choose the optimal pre-scaler combination EPWM 7.3.0 onwards AM64x, AM243x None
EXT_SITMPUSW-82 AM64/AM243: M4F core getting hangs when doing IPC with Linux IPC 7.3.0 onwards AM64x, AM243x None
EXT_SITMPUSW-83 DPL - configure HwiP_MAX_INTERRUPTS based on SOC supported values DPL 7.3.0 onwards AM64x, AM243x None
EXT_SITMPUSW-86 The configurations of GPIO interrupt routers are based on banks rather than individual pins. GPIO 7.3.0 onwards AM64x, AM243x None
EXT_EP-12271 AM64x: AM243x: ECC: SDL_PCIE0_PCIE_G2X1_64_CORE_CORE_ECC_AGGR aggregator is failing SDL 10.1.0 onwards AM64x, AM243x No known workaround
EXT_EP-12336 Last 1B of payload missing in forwarding scenario Ethernet (ICSSG) 10.1.0 onwards AM64x, AM243x No known workaround

Errata

ID Head Line Module SDK Status
i2278 MCAN: Message Transmit order not guaranteed from dedicated Tx Buffers configured with same Message ID MCAN Open
i2279 MCAN: Specification Update for dedicated Tx Buffers and Tx Queues configured with same Message ID MCAN Open
i2310 USART: Erroneous clear/trigger of timeout interrupt UART Implemented
i2311 USART: Spurious DMA Interrupts UART Implemented
i2312 MMCSD: HS200 and SDR104 Command Timeout Window Too Small MMCSD Open
i2313 GPMC: Sub-32-bit read issue with NAND and FPGA/FIFO GPMC Implemented
i2326 PCIe: MAIN_PLLx operating in fractional mode, which is required for enabling SSC, is not compliant with PCIe Refclk jitter limits PCIe Open
i2329 MDIO interface corruption, CPSW, ICSSG Open
i2331 CPSW: Device lockup when reading CPSW registers CPSW, SBL Implemented
i2345 CPSW: Ethernet Packet corruption occurs if CPDMA fetches a packet which spans across memory banks CPSW Implemented
i2401 CPSW: Host Timestamps Cause CPSW Port to Lock up CPSW Open
i2402 CPSW: Ethernet to Host Checksum Offload does not work CPSW Open

Limitations

ID Head Line Module Reported in Release Applicable Devices Workaround
EXT_SITMPUSW-27 gmake with -j can sometimes lock up Windows command prompt Build 7.3.0 AM64x, AM243x Use bash for windows as part of git for windows or don't use -j option

Upgrade and Compatibility Information

Attention
When migrating from Processor SDK RTOS, see Migration Guides for more details

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.

Compiler Options

Module Affected API Change Additional Remarks

Examples

Module Affected API Change Additional Remarks
Ethernet - Path for Ethernet examples has been changed from ${MCU_PLUS_SDK_PATH}/examples/networking to ${MCU_PLUS_SDK_PATH}/source/networking/enet/core/examples Refer Version Updates from earlier SDKs to Latest

OS Kernel

Module Affected API Change Additional Remarks

SOC Device Drivers

Module Affected API Change Additional Remarks

Networking

Module Affected API Change Additional Remarks