Below features are not support on AM243X LAUNCHPAD due to SOC or board constraints,
| OS | Supported CPUs | SysConfig Support | Key features tested | Key features not tested / NOT supported |
| FreeRTOS Kernel | R5F, M4F, A53 | NA | Task, Task notification, interrupts, semaphores, mutexs, timers, event groups. ROV views in CCS IDE, Task load measurement using FreeRTOS run time statistics APIs. | Only single core A53 FreeRTOS is supported. Second core is NOT used. |
| FreeRTOS SMP Kernel | A53 | NA | Task, Task notification, interrupts, semaphores, mutexs, timers, event groups. ROV views in CCS IDE, Task load measurement using FreeRTOS run time statistics APIs. | - |
| FreeRTOS POSIX | R5F, M4F, A53 | NA | pthread, mqueue, semaphore, clock | - |
| NO RTOS | R5F, M4F, A53 | NA | See Driver Porting Layer (DPL) below | Only single core A53 NORTOS is supported. Second core is NOT used. |
| Module | Supported CPUs | SysConfig Support | OS support | Key features tested | Key features not tested / NOT supported |
| Address Translate | M4F | YES | FreeRTOS, NORTOS | Use RAT to allow M4F access to peripheral address space | - |
| Cache | R5F, A53 | YES | FreeRTOS, NORTOS | Cache write back, invalidate, enable/disable | - |
| Clock | R5F, M4F, A53 | YES | FreeRTOS, NORTOS | Tick timer at user specified resolution, timeouts and delays | - |
| CycleCounter | R5F, M4F, A53 | NA | FreeRTOS, NORTOS | Measure CPU cycles using CPU specific internal counters | - |
| Debug | R5F, M4F, A53 | YES | FreeRTOS, NORTOS | Logging and assert to any combo of: UART, CCS, shared memory | - |
| Heap | R5F, M4F, A53 | NA | FreeRTOS, NORTOS | Create arbitrary heaps in user defined memory segments | - |
| Hwi | R5F, M4F, A53 | YES | FreeRTOS, NORTOS | Interrupt register, enable/disable/restore | - |
| MPU | R5F, M4F | YES | FreeRTOS, NORTOS | Setup MPU and control access to address space | - |
| MMU | A53 | YES | NORTOS | Setup MMU and control access to address space | - |
| Semaphore | R5F, M4F, A53 | NA | FreeRTOS, NORTOS | Binary, Counting Semaphore, recursive mutexs with timeout | - |
| Task | R5F, M4F, A53 | NA | FreeRTOS | Create, delete tasks | - |
| Timer | R5F, M4F, A53 | YES | FreeRTOS, NORTOS | Configure arbitrary timers | - |
| Event | R5F, M4F | YES | FreeRTOS | Setting, getting, clearing, and waiting of Event bits | - |
| Peripheral | Supported CPUs | SysConfig Support | Key features tested | Key features not tested / NOT supported |
| ADC | R5F | YES | Single conversion (one-shot mode), interrupt mode, DMA mode | Continuous conversion not tested |
| CRC | R5F | YES | CRC in full CPU mode | - |
| DDR | R5F | YES | Tested LPDDR4 at 400MHz frequency. | - |
| ECAP | R5F | YES | Frequency, Duty cycle, interrupt mode | PWM mode not tested |
| EPWM | R5F | YES | Different Frequency, Duty cycle, interrupt mode, Deadband and chopper module | Tripzone module not tested |
| EQEP | R5F | YES | Signal Frequency and Direction, interrupt mode | - |
| FSI (RX/TX) | R5F | YES | RX, TX, polling, interrupt mode, single/dual lanes | - |
| GPIO | R5F, M4F, A53 | YES | Basic input/output, GPIO as interrupt | GPIO as interrupt is not tested for A53. |
| GTC | R5F, A53 | NA | Enable GTC, setting FID (Frequency indicator) | - |
| I2C | R5F, M4F, A53 | YES | Controller mode, basic read/write, polling and interrupt mode | Target mode not supported. M4F not tested due to EVM limitation |
| IPC Notify | R5F, M4F, A53 | YES | Low latency IPC between RTOS/NORTOS CPUs | - |
| IPC Rpmsg | R5F, M4F, A53 | YES | RPMessage protocol based IPC for all R5F, M4F, A53 running NORTOS/FreeRTOS/Linux | - |
| MCAN | R5F | YES | RX, TX, interrupt and polling mode | - |
| MCSPI | R5F, M4F | YES | Controller/Peripheral mode, basic read/write, polling, interrupt and DMA mode | - |
| MDIO | R5F | NA | Register read/write, link status and link interrupt enable API | - |
| MMCSD | R5F | YES | Raw read/write and file I/O on MMCSD0 eMMC, and MMCSD1 SD. eMMC tested till HS SDR mode (8-bit data, 52 MHz), SD tested till SD HS mode (4-bit, 25 MHz) | Interrupt mode not tested |
| OSPI | R5F | YES | Read direct, Write indirect, Read/Write commands, DMA for read, PHY Mode | Interrupt mode not supported |
| Pinmux | R5F, M4F, A53 | YES | Tested with multiple peripheral pinmuxes | - |
| PRUICSS | R5F | YES | Tested with Ethercat, EtherNet/IP, IO-Link, ICSS-EMAC, HDSL, EnDat | - |
| SOC | R5F, M4F, A53 | YES | lock/unlock MMRs, get CPU clock, CPU name, clock enable, set frequency | - |
| Sciclient | R5F, M4F, A53 | YES | Tested with clock setup, module on/off | - |
| SPINLOCK | R5F, M4F, A53 | NA | Lock, unlock HW spinlocks | - |
| UART | R5F, M4F, A53 | YES | Basic read/write, polling, interrupt mode, | HW flow control not tested. DMA mode not supported |
| UDMA | R5F, A53 | YES | Basic memory copy, SW trigger, Chaining | - |
| WDT | R5F, A53 | YES | Interrupt after watchdog expiry | Reset not supported |
| Module | Supported CPUs | SysConfig Support | OS Support | Key features tested | Key features not tested |
| EtherCAT SubDevice FWHAL | R5F | NO | FreeRTOS | Tested with ethercat_slave_beckhoff_ssc_demo example | Reset isolation |
| EtherCAT SubDevice Evaluation Stack | R5F | NO | FreeRTOS | Tested with ethercat_slave_demo examples | - |
| EtherNet/IP Adapter FWHAL | R5F | NO | FreeRTOS | Tested with ethernetip_adapter_demo examples | Multicast Filtering |
| EtherNet/IP Adapter Evaluation Stack | R5F | NO | FreeRTOS | Tested with ethernetip_adapter_demo examples | - |
| IO-Link Controller Evaluation Stack | R5F | NO | FreeRTOS | Tested with iolink_master_demo example | - |
| Profinet Device FWHAL | R5F | NO | FreeRTOS | Tested with profinet_device_demo examples | IRT, MRP |
| Profinet Device Evaluation Stack | R5F | NO | FreeRTOS | Tested with profinet_device_demo examples | - |
| Module | Supported CPUs | SysConfig Support | OS Support | Key features tested | Key features not tested |
| LwIP | R5F | YES | FreeRTOS | TCP/UDP IP networking stack, DHCP, ping, TCP iperf, TCP/UDP IP | Other LwIP features, performance and memory optimizations pending, more robustness tests pending |
| Ethernet driver (ENET) | R5F | YES | FreeRTOS | Ethernet as port using CPSW and ICSS, Layer 2 MAC, Layer 2 PTP Timestamping, CPSW Switch | - |
| ICSS-EMAC | R5F | YES | FreeRTOS | Tested switch mode with ethernetip_adapter_demo and profinet_device_demo examples | EMAC mode, VLAN/Multicast Filtering |
| ICSS TimeSync | R5F | NO | FreeRTOS | Tested E2E mode with ethernetip_adapter_demo examples | P2P mode, Transparent Clock mode |
| ID | Head Line | Module | Applicable Releases | Applicable Devices | Resolution/Comments |
| MCUSDK-2131 | EtherCAT SubDevice increments long frame errors for frames with size less than 2000 bytes | EtherCAT SubDevice FWHAL | 7.3.0 onwards | AM64x, AM243x | Fixed |
| MCUSDK-2202 | DDR: High bandwidth data traffic at certain burst patterns causes faiures. | High bandwidth data traffic at certain burst patterns on the DDR bus cause resonance frequencies on the DDR IO voltage rail. This in turn affects the DDR address bus and causes the failures. The main fix in the updated configurations is enabling write DBI on LPDDR4, and read DBI on DDR4. This helps to quite the data transitions on the DDR bus and greatly reduces the impact on the DDR IO voltage rail. | 8.1.0 onwards | AM64x, AM243x | Fixed. |
| MCUSDK-2261 | CCS Target Configuration from SDK examples does not work | CCS | 8.1.0 | AM64x, AM243x | Added 1-click debug in the documentation which uses default target config itself. Updated documentation to use either target configuration for SBL, but for CCS load, you need to use "AM64x_GP_EVM/AM24x_GP_EVM" |
| MCUSDK-2301 | Correct main task name from frertos_main to freertos_main | FREERTOS EXAMPLES | 7.3.0 onwards | AM64x, AM243x | Fixed |
| MCUSDK-2338 | LwIP fails to build with <sys/select.h> header | LWIP | 8.1.0 onwards | AM64x | Fixed |
| MCUSDK-2344 | MCU+ SDK: Removing mmcsd driver in sysconfig file leads to linker error | MMCSD | 8.1.0 onwards | AM64x, AM243x | Fixed. MMCSD Sysconfig provides an option of choosing 'NO DEVICE' if there is no device connected. |
| MCUSDK-2347 | Enet: PORT_MODE_SEL in CTRLMMR_ENET1_CTRL can't be changed | ENET | 8.1.0 onwards | AM64x, AM243x | Incorrect offset for kick0 and kick1 registers. |
| MCUSDK-2413 | Enet - build failure when LwIP stats is disabled | Enet | 8.1.0 onwards | AM64x, AM243x | Fixed |
| MCUSDK-2416 | AM64X: Writing images to flash larger than 1024 KByte, uniflash finishes with errors | UART, SBL | 8.1.0 onwards | AM64x, AM243x | Fixed |
| MCUSDK-2458 | AM243x EVM: the SBL_NULL does not initialize DDR | SBL | 8.1.0 onwards | AM243x | Fixed |
| MCUSDK-2469 | AM243x: EPWM example for AM243x LP is using the wrong pin | EPWM | 8.1.0 onwards | AM64x, AM243x | Fixed |
| MCUSDK-2510 | Enet - Loopback example not supported but packaged | Enet | 8.1.0 onwards | AM64x, AM243x | Fixed |
| MCUSDK-2528 | EtherCAT : Latch pins are not working | EtherCAT SubDevice Beckhoff SSC Demo | 7.3.0 onwards | AM64x, AM243x | Timesync router configuration was required for these pins. |
| MCUSDK-2531 | I2C module should be disabled before doing softreset in I2C_ctrlInit | I2C | 8.1.0 onwards | AM64x | Fixed |
| MCUSDK-3275 | Enet - build error on Dev assert enable | Enet | 8.1.0 onwards | AM243x | Fixed |
| MCUSDK-3276 | Enet - Missing extern "C" statement when using enet.h with C++ | Enet | 8.1.0 onwards | AM243x | Fixed |
| MCUSDK-3616 | CPSW: packet drops seen in ping and low iperf performance numbers on am64x-evm and am243x-evm | Enet | 8.1.0 onwards | AM64x, AM243x | Fixed |
| ID | Head Line | Module | Applicable Releases | Applicable Devices | Workaround |
| MCUSDK-626 | DMA not working with ADC FIFO 1 | ADC | 7.3.0 onwards | AM64x, AM243x | Use ADC FIFO 0 |
| MCUSDK-1016 | Semaphore does not function as expected when "post" call is present in multiple ISRs at different priorities | DPL | 7.3.0 onwards | AM64x, AM243x | Interrupt nesting should be disabled. SDK disables interrupt nesting by default. |
| MCUSDK-1922 | SBL UART appimage size limitation of less then 384 KB | SBL | 7.3.0 onwards | AM64x, AM243x | -
|
| MCUSDK-2113 | [Docs] Sysfw RM/PM documentation doesn't specify AM243x | Docs | 8.0.0 onwards | AM243x | - |
| MCUSDK-2135 | Insufficient UDMA TX channels allocated for Dual-mac mode | Enet | 8.1.0 onwards | AM64x, AM243x | Allocate minimum of 2 TX channels(ENET_CFG_TX_CHANNELS_NUM macro) in enet_cfg.h file |
| MCUSDK-2319 | 2 PRU(ICSS) driver instances are added while changing Enet ICSSG instance to ICSSG0 in SysConfig | SYSCFG | 8.1.0 onwards | AM64x, AM243x | Please remove the extra one manually |
| MCUSDK-3453 | UDMA unable to process icssg rx timestamp and some bytes of packet content after Allocated Packets(Wraparound) | Enet | 8.1.0 onwards | AM64x, AM243x | - |
| MCUSDK-2419 | MCSPI TX Only mode is not functional in DMA mode | MCSPI, UDMA | 8.2.0 onwards | AM64x, AM243x | Use TX/RX mode and ignore RX. |
| MCUSDK-3424 | SBL OSPI fails to load image using OSPI DMA in HS device | SBL, OSPI, UDMA | 8.2.0 onwards | AM64x, AM243x | Use non DMA mode |
| MCUSDK-2715 | PKA ECDSA sign verify is not working for P-521 and BrainPool P-512R1 curves | SECURITY | 8.2.0 onwards | AM64x, AM243x | - |
| MCUSDK-2753 | SOC_controlModuleLockMMR() API doesn't lockCTRLMMR registers | SDK | 8.1.0 onwards | AM243x | - |
| MCUSDK-3513 | SBL JTAG Example flash write fails if the file size is not aligned to multiple of flash page size | SBL JTAG | 8.2.0 onwards | AM64x, AM243x | Aligned file size to page size by padding 0's at the end |
| MCUSDK-3626 | Enet: Phy tuning is not done correctly on AM64x/AM243x and AM263x platforms | Enet | 8.1.0 onwards | AM64x, AM243x | PHY delay is not tuned but set to value based on limited testing on a small set of boards.If packet drops are still seen, we can force the phy to set to 100mbps.Make below change in application code: linkCfg->speed = ENET_SPEED_100MBIT; linkCfg->duplexity = ENET_DUPLEX_FULL; |
This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.