AM243x MCU+ SDK  11.01.00
Release Notes 07.03.01

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.
Unless explicitly noted otherwise, the SW modules would work on any of the R5F's present on the SOC.
All SW modules will not work on M4F. M4F support for a module will be explicitly called out.

New in this Release

Feature Module
SBL with OSPI XIP boot OSPI, Bootloader
OSPI Phy mode and DMA mode OSPI, Bootloader
ROV views in CCS IDE CCS, FreeRTOS, No-RTOS
FreeRTOS IRQ handler to save/restore FPU registers FreeRTOS
MCAN Polled mode transfer MCAN

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM243x R5F, M4F AM243x GP EVM (referred to as am243x-evm in code) Windows 10 64b or Ubuntu 18.04 64b

Dependent Tools and Compiler Information

Tools Supported CPUs Version
Code Composer Studio R5F, M4F 10.3.1
SysConfig R5F, M4F 1.8.1, build 1900
TI ARM CLANG R5F, M4F 1.3.0.LTS
FreeRTOS Kernel R5F, M4F 10.4.3

Key Features

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F, M4F NA Task, Task notification, interrupts, semaphores, mutexs, timers. ROV views in CCS IDE Task load measurement using FreeRTOS run time statistics APIs.
FreeRTOS POSIX R5F, M4F NA pthread, mqueue, semaphore, clock -
NO RTOS R5F, M4F NA See Driver Porting Layer (DPL) below -

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Address Translate M4F YES FreeRTOS, NORTOS Use RAT to allow M4F access to peripheral address space -
Cache R5F YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F, M4F YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CycleCounter R5F, M4F NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F, M4F YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F, M4F NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F, M4F YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore -
MPU R5F, M4F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
Semaphore R5F, M4F NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F, M4F NA FreeRTOS Create, delete tasks -
Timer R5F, M4F YES FreeRTOS, NORTOS Configure arbitrary timers -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Bootloader R5FSS0-0 YES NORTOS Boot modes: OSPI, OSPI XIP, UART. All R5F's, M4F boot. RPRC, multi-core image format DDR init during SBL. SBL booting Linux. SBL booting A53.

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
ADC R5F YES Single conversion (one-shot mode), interrupt mode, DMA mode Continuous conversions
CRC R5F NO Only compiled Not tested
ECAP R5F NO Only compiled Not tested
EPWM R5F YES Different Frequency, Duty cycle, interrupt mode, Deadband and chopper module Tripzone module not tested
EQEP R5F NO Only compiled Not tested
FSI (RX/TX) R5F YES RX, TX, polling, interrupt mode, single/dual lanes -
GPIO R5F, M4F YES Basic input/output, GPIO as interrupt -
I2C R5F, M4F YES Controller mode, basic read/write, polling and interrupt mode Target mode. M4F not tested due to EVM limitation
IPC Notify R5F, M4F YES Low latency IPC between RTOS/NORTOS CPUs -
IPC Rpmsg R5F YES RPMessage protocol based IPC, All R5F and Linux A53 cores M4F core
MCAN R5F YES RX, TX, interrupt and polling mode -
MCSPI R5F, M4F YES Controller/Peripheral mode, basic read/write, polling, interrupt mode DMA mode
MDIO R5F NA Register read/write, link status and link interrupt enable API -
OSPI R5F YES Read direct, Write indirect, Read/Write commands, DMA for read Interrupt mode
Pinmux R5F, M4F YES Tested with multiple peripheral pinmuxes -
PRUICSS R5F YES Tested with Ethercat FW HAL, HDSL, EnDat More protocols integration tests pending
SOC R5F, M4F YES lock/unlock MMRs, get CPU clock, CPU name, clock enable, set frequency -
Sciclient R5F, M4F YES Tested with clock setup, module on/off -
SPINLOCK R5F, M4F NA Lock, unlock HW spinlocks -
UART R5F, M4F YES Basic read/write, polling, interrupt mode, HW flow control not tested, DMA mode not supported
UDMA R5F YES Basic memory copy, SW trigger, Chaining -

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES I2C based EEPROM -
ETHPHY R5F YES Ethernet Phy configuration for EtherCAT SubDevice example -
Flash R5F YES XSPI based flash, Octal mode, DDR mode Other flash types
LED R5F YES GPIO and I2C IO expander based LED control -

CMSIS

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
CMSIS DSP R5F NA FreeRTOS, NORTOS Basic math, complex math, controller, fast math, filtering, Matrix, statistics, transform -

Motor Control

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
Position Sense HDSL R5F YES FreeRTOS, NORTOS Freerun mode, Sync mode -
Position Sense EnDAT R5F YES FreeRTOS, NORTOS Single channel, Multi channel, Continuous mode -

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
EtherCAT SubDevice FW HAL R5F YES FreeRTOS Tested with Beckhoff's EtherCAT stack based example Online firmware update, reset isolation
EtherCAT SubDevice ETG Stack R5F NO FreeRTOS Standard stack (NOT BUNDLED in SDK) -
EtherNet/IP Adapter FW HAL R5F NO FreeRTOS Only compiled Not tested
Profinet Device FW HAL R5F NO FreeRTOS Only compiled Not tested
ICSS-EMAC R5F YES FreeRTOS Only compiled Not tested
ICSS TimeSync R5F NO FreeRTOS Only compiled Not tested. "Event" construct related code is not compiled.

Fixed Issues

ID Head Line Module Applicable Releases Applicable Devices Resolution/Comments
MCUSDK-635 HwiP_construct when compiled in release mode would reorder instruction such interrupt can get enabled before ISR is setup DPL (No-RTOS and FreeRTOS) 7.3.0 AM64x Fixed
MCUSDK-180 Bootloader: Flash_Open and other APIs in SBL fail when the bootmode is OSPI Bootloader 7.3.0 AM64x Fixed
MCUSDK-636 Incorrect Input FCLK leading to wrong SPI CLK output McSPI 7.3.0 AM64x Fixed. Input clock fixed to right frequency of 50 MHz from 48 MHz assumed earlier
MCUSDK-353 ENDAT: EnDAT diagnostic does not support multi channel. ENDAT 7.3.0 AM64x Rejected. Setup issue.
MCUSDK-397 Incorrect values for SYNC_PERMISSION_UPDATE_*_SIZE macros in EtherCAT FW HAL EtherCAT SubDevice FW HAL 7.3.0 AM64x Fixed the macro definitions.
MCUSDK-398 HwiP_restore not called after HwiP_disable in bsp_send_command_to_firmware of EtherCAT EtherCAT SubDevice FW HAL 7.3.0 AM64x Fixed. This was applicable only if SUPPORT_CMDACK_POLL_MODE macro was enabled and ENABLE_PDI_TASK macro was disabled.
MCUSDK-399 ICSS_EMAC_updatePhyStatus function fails if auto-negotiation is disabled ICSS-EMAC 7.3.0 AM64x Fixed by use of PHY Status register instead of auto-negotiation specific registers for checking speed and duplex configuration.
MCUSDK-633 Statistics structure is needed for all ports in ICSS-EMAC ICSS-EMAC 7.3.0 AM64x Fixed by allocating the structure per port inside the ICSS-EMAC driver object.

Known Issues

ID Head Line Module Applicable Releases Applicable Devices Workaround
MCUSDK-177 DMTimer on M4F results in 2 interrupts instead of 1 for every DM timer expiry in release mode DPL 7.3.0 AM64x, AM243x Use ClockP module which uses SysTick M4 timer and this does not have any issues.
MCUSDK-316 ROV does not work with DDR being used in application FreeRTOS 7.3.0 AM64x, AM243x ROV cannot be used when operating from DDR
MCUSDK-596 Zero init of globals and static does not happen with current compiler and linker option Common 7.3.0, 7.3.1 AM64x, AM243x Explicitly initialize the required variables
MCUSDK-317 OSPI: DMA reads fails after a flash write which was not block aligned OSPI 7.3.0 AM64x, AM243x Use non-DMA read mode or use DMA mode but always write from start of a erased block
MCUSDK-627 R5FSS0_0 ATCM is not enabled after NULL SBL boot Bootloader 7.3.0, 7.3.1 AM64x, AM243x Enable ATCM in application
MCUSDK-626 DMA not working with ADC FIFO 1 ADC 7.3.0, 7.3.1 AM64x, AM243x Use ADC FIFO 0
MCUSDK-354 EtherCAT State Machine from EtherCAT Conformance Test fails intermittently EtherCAT 7.3.0 AM64x, AM243x Use debug mode library for FreeRTOS. The makefile and projectspec for this example use debug mode library by default for all configurations

Limitations

ID Head Line Module Reported in Release Applicable Devices Workaround
MCUSDK-208 gmake with -j can sometimes lock up Windows command prompt Build 7.3.0 AM64x, AM243x Use bash for windows as part of git for windows or don't use -j option

Upgrade and Compatibility Information

Attention
When migrating from Processor SDK RTOS, see Migration Guides for more details

Driver Porting Layer (DPL)

Module Affected API Change Additional Remarks
ClockP ClockP_Params Added a new parameter name to specify a user defined name for a clock object No change needed in application as long as ClockP_Params_init is used to init the parameters to default

SOC Device Drivers

Module Affected API Change Additional Remarks
BOOTLOADER Bootloader_loadSelfCpu Takes argument as Bootloader_CpuInfo, instead of Bootloader_BootImageInfo Bootloader_loadSelfCpu should be called each time for each CPU vs calling it once for all "self" CPUs earlier.

Networking

Module Affected API Change Additional Remarks
EtherCAT SubDevice FW HAL bsp_init Added new parameters in bsp_params for PDI and SYNC ISR functions to be called when interrupt is received from PRU, if ENABLE_PDI_TASK or ENABLE_SYNC_TASK macros are disabled. No change needed if ENABLE_PDI_TASK or ENABLE_SYNC_TASK are enabled. They are enabled by default.
ICSS-EMAC ICSS_EMAC_open ETHPHY_Handle is an addition in ICSS_EMAC_Params structure ETHPHY_Handle should be passed in the ICSS_EMAC_Params structure while making the ICSS_EMAC_open function call.
ICSS-EMAC ICSS_EMAC_Params_init ICSS_EMAC_params_init is renamed to ICSS_EMAC_Params_init NA