AM243x MCU+ SDK  11.01.00
Migrating examples to 11.01.00 from older versions

Note
Images are shown for AM64x. It is application for AM243X as well.

Makefile Changes

Library Name change on makefile and CCS projects

From 11.01.00 SDK all the libraries are built seperately for OS. There are seperate libraries available for NoRTOS and FreeROTS. So the makefiles needs to be updated accordingly. Please refer the sample changes on the makefile below. These changes are not applicbale for the librarries which were already built seperately for NoRTOS/FreeRTOS like kernel libraries.

For NoRTOS/baremetal,

Library name change for NoRTOS example

For FreeRTOS,

Library name change for FreeRTOS example

similar change can be done on the CCS project as well

OS define on makefile and CCS projects

Addtional macro OS_NORTOS or OS_FREERTOS should be deined on the makefile or CC project based on the OS of the project.

For NoRTOS/baremetal,

OS Macro addition for NoRTOS example

For FreeRTOS,

OS Macro addition for FreeRTOS example