AM243x MCU+ SDK  11.01.00
SA2UL HMAC SHA-512 Test

Introduction

This example demonstrates the how to generate HMAC-SHA 512 hash using SA2UL module.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am243x-evm, am243x-lp
Example folder examples/security/crypto/sa2ul_hmac_sha/crypto_hmac_sha512/crypto_hmac_sha512.c

Steps to Run the Example

See Also

SA2UL

Sample Output

Shown below is a sample output when the application is run.

CCS Console:

[CRYPTO] HMAC SHA-512 example started ...
[CRYPTO] HMAC SHA-512 example completed!!
All tests have passed!!