This example uses the LLD driver to demonstrates basic read write operations to the eMMC device in interrupt mode. The MMC instance and the media connected to it are selectable via Sysconfig.
The example writes known data to a particular offset in the media and then reads it back. The read data is then compared with the written known data. When both the comparisons match, test result is passed otherwise failed.
| Parameter | Value |
|---|---|
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Boards | am243x-evm |
| Example folder | examples/drivers/mmcsd/mmcsd_raw_io_emmc_intr_lld |