This example demonstrates setting of multiple LED at the same time connected to the same I2C controller. The application will blink all the I2C controlled LED in the EVM.
Application blinks leds for 3 loops in interrupt mode and 3 loops in polling mode. Application exits after 6 iterations.
| Parameter | Value |
|---|---|
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Boards | am243x-evm, am243x-lp |
| Example folder | examples/drivers/i2c/i2c_led_blink_polling_lld |
Shown below is a sample output when the application is run,