AM243x MCU+ SDK  11.01.00
ECAP APWM mode

Introduction

This example uses the ECAP in APWM mode to generate a PWM signal.

The example does the below

  • Configures ECAP in APWM mode and configures values in period and compare registers.
  • Waits for the specified time using the ECAP ISR.

External Connections

AM243X-EVM

  • The signal can be probed on Pin 1 of the J12 header on the base board.

AM243X-LP

  • The signal can be probed on Pin 1 of the J21 header on the base board.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
r5fss0-0 freertos
Toolchain ti-arm-clang
Board am243x-evm, am243x-lp
Example folder examples/drivers/ecap/ecap_apwm_mode/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run

See Also

ECAP

Sample Output

Shown below is a sample output when the application is run,

ECAP APWM Mode Test Started ...
ECAP APWM Test Passed!!
All tests have passed!!