AM243x MCU+ SDK  11.01.00
CRC FULL CPU

Introduction

This example demonstrates Cyclic Redundancy Check (CRC) in full CPU mode for Channel number 1. CRC signature is calculated on a frame that is stored in memory and compared against pre-calculated CRC signature value.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
m4fss0-0 nortos
Toolchain ti-arm-clang
Boards am243x-evm, am243x-lp
Example folder examples/drivers/crc/crc_full_cpu/

Steps to Run the Example

See Also

CRC

Sample Output

Shown below is a sample output when the application is run,

CRC Full CPU Test Started ...
Full CPU mode CRC Test Passed!!
All tests have passed!!