SimpleLink™ CC3501 LaunchPad™ Settings & Resources

The SimpleLink™ CC3501 LaunchPad™ contains a CC3501ENJARSHR device.

Jumper Settings

SysConfig Board File

The LP_EM_CC35X1.syscfg.json is a handcrafted file used by SysConfig. It describes the physical pin-out and components on the LaunchPad.

Driver Examples Resources

Examples utilize SysConfig to generate software configurations into the ti_drivers_config.c and ti_drivers_config.h files. The SysConfig user interface can be utilized to determine pins and resources used. Information on pins and resources used is also present in both generated files.

TI BoosterPacks™

The following BoosterPack is used with some driver examples.

CC3200 Audio BoosterPack

The BoosterPack’s DIN, DOUT, BCLK and FSYNC/WCLK signal pins are not compatible with this LaunchPad. Use the following modifications to enable the CC3200 Audio BoosterPack’s usage with the i2secho example.

On the LP_EM_CC35X1 board, bend down the following BoosterPack header pins:

Be sure that the bent pins do not make contact with the IC or any other component, bend them enough to make sure they don’t connect to the CC3200 Audio BoosterPack.

Attach the CC3200 Audio BoosterPack to the LP_EM_CC35X1 and run jumper wires between the following pins on the CC3200 Audio BoosterPack:

See Audio BP User Guide (Figure 2-1), or the diagram below, for information on where these pins are located.

CC3200 Audio BoosterPack Jumper Wire Diagram