WiFi F3 SimpleLink Core SDK 9.20.00.23 Release Notes
Table of Contents
Introduction
This is a Production (GA) release of the Core SDK 9.20.00.23 for WiFi F3 devices.
Documentation
Open the Documentation Overview file in the docs/ folder for a full list of documentation.
What’s New
- A summary of changes made in the current release of this product can be found in the product Change Log.
Upgrade and Compatibility Information
Host Support
See the SDK release notes for a description of which host operating systems are supported in this release.
Dependencies
See the SDK release notes for a description of which components and tools are required to work with this product.
Device Support
See the SDK release notes for a list of TI devices that are supported in this product.
Validation Information
The Core SDK was validated with the following components:
- Code Composer Studio™ 20.1.0
- TI Clang Code Generation Tools
- ARM ti-cgt-armllvm_4.0.4.LTS
- FreeRTOS 10.5.1-1
- SysConfig 1.26.0
- Python 3.10.12
- Toolbox 4.0.2
New Features
| ID | Summary |
|---|---|
| LPRFSEC-256 | Enable usage of hash length > curve length in ECDSA Driver |
Fixed Issues
| ID | Summary |
|---|---|
| TIDRIVERS-7639 | Fixed bit Misalignment in ExceptionArmV8M.c within the Exception module |
| LPRFSEC-253 | Fixed an issue where psa_mac_abort() would return an error instead of invoking mbedtls when using SW crypto |
Known Issues
| ID | Summary |
|---|---|
| TIDRIVERS-7249 | [CC35XX] ROV is not functional |
Customer Support
- Use the E2E support forums for customer support.
- Use the External Bug and Enhancement System to track issues.
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
Prior Release Changes
A summary of changes made in previous releases of this product can be found in the product Change Log.