Overview & Features

Introduction

CC35xx Simplelink Wi-Fi family of devices is a full SoC, enabling connectivity through Wi-Fi and BLE. In this section, the focus would be on Wi-Fi and to demonstrates its capabilities, the Network Terminal example in the SimpleLink Wi-Fi Software Development Kit would be used. The purpose is to familiarize users with Wi-Fi in general and with the set of APIs available to the application. To simplify the experience, the network terminal is used to translate these APIs into a readable terminal interactive commands that would be covered in this section.

Note

Follow the Quick Start Guide under the SDK documentation folder to install the SDK, build the setup, activate the device (which is locked initially) and program the device for the first time. Upon successful procedure, the Network Terminal menu should appear on the Terminal emulation.

Wi-Fi Features

  • 2.4GHz and 5GHz bands
  • Station role (STA)
  • Access Point role (AP) - up to 4 connections, Wi-Fi4 only
  • IEEE 802.11 b/g/n/a/(ax only for STA)
  • Multirole - STA role and AP role running in parallel
  • Channel Switch Announcement support in Station role
  • P2P Client and Go
  • Support Security types - Personal - WPA3 (STA role only), WPA2 (STA and AP), WPA/WPA2 (mixed mode, STA role only), WPS, OPEN
    • Enterprise - WPA3, WPA2 (TLS,TTLS, PEAP0)
  • Date and time module
  • Agile Multiband
  • DFS support and channel switch