ALL VERSIONS

For each SDK release, do the following steps to update SDK version on existing projects

Attention

If you have an already activated device, you will need to perform “Factory Programming” with the toolbox provided in the sdk before being flashing via CCS.

  1. Open CCS and verify that the latest versions of SimpleLink Wifi Toolbox, SimpleLink Wi-Fi SDK, and SysConfig are detected as a product

    This can be done by going to FilePreferencesCode Composer Studio Settings

    ../_images/Theia_CCSSettings.png

    Fig. 32 Code Composer Settings

    Next go into GeneralProducts

    ../_images/Theia_Products.png

    Fig. 33 Products

  2. Import Project from the new SDK by going to FileImport Projects

    ../_images/Theia_Import1.png

    Fig. 34 Import Project

    Browse for the example

    ../_images/Theia_Browse1.png

    Fig. 35 Browse Examples

  3. Verify SimpleLink Wifi Toolbox, SimpleLink Wi-Fi SDK, and SysConfig is in the product dependencies. Right click on the Project and navigate to Properties

    ../_images/Theia_Properties1.png

    Fig. 36 Project Properties

    In the Project Properties go to GeneralDependenciesProduct Dependencies

    ../_images/Theia_Dependencies1.png

    Fig. 37 Product Dependencies

    If the SimpleLink Wifi Toolbox is not in the list. Click on the Plus icon and select the SimpleLink Wifi Toolbox and latest version.

    ../_images/Theia_AddProduct.png

    Fig. 38 Add Product Reference

  1. Open CCS and verify that the latest versions of SimpleLink Wifi Toolbox, SimpleLink Wi-Fi SDK, and SysConfig are detected as a product

    This can be done by going to FilePreferencesCode Composer Studio Settings

    ../_images/import-1.png

    Fig. 39 Click on Preferences

    ../_images/import-2.png

    Fig. 40 Refresh Products

  2. Import Project from the new SDK by going to FileImport Projects

    ../_images/import-3.png

    Fig. 41 Import projects

    • On pop up dialog select “Code Composer Studio” and then “CCS Project” and “Next”.
    ../_images/import-4.png

    Fig. 42 CCS Project

    • Click on “Browse …” and navigate into examples.
      • SDK_INSTALL_DIR/examples
        1. /rtos/CC35X1_LAUNCHXL for driver examples
        2. /CC35xx_network_terminal for the WiFi network terminal example
    • Click “Select Folder” and selected projects should appear in “Discovered projects”. Make sure “Copy projects into workspace” is checked before clicking “Finish”.
    ../_images/import-5.png

    Fig. 43 Select Project

  3. Verify SimpleLink Wifi Toolbox, SimpleLink Wi-Fi SDK, and SysConfig is in the product dependencies.

Right click on the Project and navigate to Properties

If the SimpleLink Wifi Toolbox is not in the list. Click on the Plus icon and select the SimpleLink Wifi Toolbox and latest version.