Radio Configuration¶
The CC35xx allows the configuration of radio parameters this can be done using Sysconfig or INI Composer.
The CC35xx_conf.bin can be created with the Simplelink Wifi Toolbox, using the INI Composer.
Note
Reference the Wifi Toolbox User Guide for more information on how to generate the conf files and detailed information on parameters
Inside the RF Stacks section of the project.syscfg file There are 3 sets of settings, BLE, Co-Ex, and Wi-Fi
Note
Reference the Wifi Toolbox User Guide INI Composer for more information on parameters
Once all parameters have been chosen build the sysconfig file, this will generate a file called cc35xx_conf.ini that holds the chosen parameters.
This file will be used when creating a CC35xx_conf.bin
The CC35xx_conf.bin generated is the file that will be flashed in the vendor TLV section of the vendor container slot
Note
For more information on container slots please refer to Flash Mapping under Memory Overview
If using personal makefiles to flash the CC35xx device please refer to the makefile located in the Wifi Toolbox
<SimpleLink_WiFi_Toolbox_DIR>/scripts/makefile