HCI Extension Commands
In addition to the BLE HCI commands, the following HCI Extension vendor specific commands are also available.
HCI_EXT_SetTxPowerCmd
| Opcode: | 0xFC01 |
| Command Description: |
| | This command is used to set the RF transmitter output power. |
Command Parameters
| TX Power: | Tx power to use.
| Size: | 1 byte(s)
|
| Default: | 2
|
| Range: |
| Value |
Description |
| 0 |
: 0 dBm |
| 1 |
: 5 dBm |
| 2 |
: 10 dBm |
| 3 |
: 20 dBm |
|
|
Events Generated
When this command has completed, an HCI_EXT_SetTxPowerDone event shall be generated.
HCI_EXT_OnePktPerEvtCmd
| Opcode: | 0xFC02 |
| Command Description: |
| | This command is used to configure the Link Layer to only allow one packet per connection event. This command can be used to trade^off throughput and power consumption during a connection. When enabled, power can be conserved during a connection by limiting the number of packets per connection event to one, at the expense of more limited throughput. When disabled, the number of packets transferred during a connection event is not limited, at the expense of higher power consumption. Note that when set, all connections will be restricted to one packet per event. |
Command Parameters
| Control: | Enable or disable allowing only one packet per event.
| Size: | 1 byte(s)
|
| Default: | 0
|
| Range: |
| Value |
Description |
| 0 |
Disable |
| 1 |
Enable |
|
|
Events Generated
When this command has completed, an HCI_EXT_OnePacketPerEventDone event shall be generated only if the state has changed.
HCI_EXT_DecryptCmd
| Opcode: | 0xFC05 |
| Command Description: |
| | This command is used to decrypt encrypted text using AES128. |
Command Parameters
| Key: | 128 bit key for the decryption of the data given in the command. The most significant octet of the data corresponds to key[0] using the notation specified in FIPS 197.
| Size: | 16 byte(s) |
| Default: | “BF:01:FB:9D:4E:F3:BC:36:D8:74:F5:39:41:38:68:4C” |
| Range: | Any 16 byte value |
|
| Data: | 128 bit encrypted data to be decrypted. The most significant octet of the key corresponds to key[0] using the notation specified in FIPS 197.
| Size: | 16 byte(s) |
| Default: | “66:C6:C2:27:8E:3B:8E:05:3E:7E:A3:26:52:1B:AD:99” |
| Range: | Any 16 byte value |
|
Events Generated
When this command has completed, an HCI_EXT_DecryptCommandDone event shall be generated.
HCI_EXT_SetLocalSupportedFeaturesCmd
| Opcode: | 0xFC06 |
| Command Description: |
| | This command is used to set the Controllers Local Supported Features. For a complete list of supported LE features, please see [1], Part B, Section 4.6. Note: This command can be issued either before or after one or more connections are formed. However, the local features set in this manner are only effective if performed before a Feature Exchange Procedure has been initiated by the Master. Once this control procedure has been completed for a particular connection, only the exchanged feature set for that connection will be used. Since the Link Layer may initiate the feature exchange procedure autonomously, it is best to use this command before the connection is formed. |
Command Parameters
| FeatureSet: | Write LL local supported features.
| Size: | 8 byte(s)
|
| Default: | 0x0000000000000001
|
| Range: |
| Value |
Description |
| 0x0000000000000000 |
No Events Specified |
| 0x0000000000000001 |
Encryption |
| 0x0000000000000002 |
Connection Parameters Request |
| 0x0000000000000004 |
Reject Extended Indication |
| 0x0000000000000008 |
Slave Features Exchange |
| 0x0000000000000010 |
Ping |
| 0x0000000000000020 |
Data Packet Length Extension |
| 0x0000000000000040 |
Privacy |
| 0x0000000000000080 |
Extended Scanner Filter Policies |
| 0x0000000000000100 |
2M PHY |
| 0x0000000000000200 |
Stable Modulation Index Tx |
| 0x0000000000000400 |
Stable Modulation Index Rx |
| 0x0000000000000800 |
Coded PHY |
| 0x0000000000001000 |
Extended Advertising |
| 0x0000000000002000 |
Periodic Advertising |
| 0x0000000000004000 |
Channel Selection Algorithm #2 |
| 0x0000000000008000 |
LE Power Class 1 |
| 0x0000000000010000 |
Minimum Number of Used Channels |
|
|
Events Generated
When this command has completed, an HCI_EXT_WriteLocalFeatureSupportDone event shall be generated.
HCI_EXT_SetFastTxRespTime
| Opcode: | 0xFC07 |
| Command Description: |
| | This command is used to set whether transmit data is sent as soon as possible even when peripheral latency is used. |
Command Parameters
| Control: | Enable or disable allowing only one packet per event.
| Size: | 1 byte(s)
|
| Default: | 0
|
| Range: |
| Value |
Description |
| 0 |
Disable |
| 1 |
Enable |
|
|
Events Generated
When this command has completed, an HCI_EXT_SetFastTxRespTimeDone event shall be generated.
HCI_EXT_SetBDADDRCmd
| Opcode: | 0xFC0C |
| Command Description: |
| | This command is used to set this devices BLE address (BDADDR). This address will override the devices address determined when the device is reset (i.e. a hardware reset, not an HCI Controller Reset). To restore the devices initialized address, issue this command with an invalid address. Note: This command is only allowed when the Controller is in the Standby state. Note: This command is intended to only be used during initialization. Changing the devices BDADDR after various BLE operations have already taken place may cause unexpected problems. |
Command Parameters
| BDADDR: | BLE Public Address (MSB..LSB). Use “FF:FF:FF:FF:FF:FF” to restore the device address to that which was determined at initialization.
| Size: | 6 byte(s) |
| Default: | “00:00:00:00:00:00” |
| Range: | Any 6 byte value |
|
Events Generated
When this command has completed, an HCI_EXT_SetBDADDRDone event shall be generated.
HCI_EXT_SetSCACmd
| Opcode: | 0xFC0D |
| Command Description: |
| | This command is used to set this devices Sleep Clock Accuracy (SCA) value, in parts per million (PPM), from 0 to 500. For a Master device, the value is converted to one of eight ordinal values representing a SCA range (per [1], Volume 6, Part B, Section 2.3.3.1, Table 2.2), which will be used when a connection is created. For a Slave device, the value is directly used. The system default value for a Master and Slave device is 50ppm and 40ppm, respectively. Note: This command is only allowed when the device is not in a connection. Note: The devices SCA value remains unaffected by an HCI Reset. |
Command Parameters
| SCA: | BLE Device Sleep Clock Accuracy (PPM).
| Size: | 2 byte(s) |
| Default: | “40” |
| Range: | (0..500) |
|
Events Generated
When this command has completed, an HCI_EXT_SetSCADone event shall be generated.
HCI_EXT_SetMaxDtmTxPowerCmd
| Opcode: | 0xFC11 |
| Command Description: |
| | This command is used to set the RF transmitter output power when doing RF testing in PLT mode. |
Command Parameters
| TX Power: | Tx power to use.
| Size: | 1 byte(s)
|
| Default: | 2
|
| Range: |
| Value |
Description |
| 0 |
: 0 dBm |
| 1 |
: 5 dBm |
| 2 |
: 10 dBm |
| 3 |
: 20 dBm |
|
|
Events Generated
When this command has completed, an HCI_EXT_SetTxPowerDone event shall be generated.
HCI_EXT_DisconnectImmedCmd
| Opcode: | 0xFC13 |
| Command Description: |
| | This command is used to disconnect a connection immediately. This command can be useful for when a connection needs to be ended without the latency associated with the normal BLE Controller Terminate control procedure. Note that the Host issuing the command will still receive the HCI Disconnection Complete event with a Reason status of 0x16 (i.e. Connection Terminated by Local Host), followed by an HCI Vendor Specific Event. |
Command Parameters
| Connection Handle: |
| | Handle used to identify a connection
| Size: | 2 byte(s) |
| Default: | 0x0000 |
| Range: | 0x0000 to 0x0EFF |
|
Events Generated
When this command has completed, an HCI_EXT_DisconnectImmedDone event shall be generated.
HCI_EXT_PacketErrorRateCmd
| Opcode: | 0xFC14 |
| Command Description: |
| | This command is used to Reset or Read the Packet Error Rate counters for a connection. When Reset, the counters are cleared; when Read, the total number of packets received, the number of packets received with a CRC error, the number of events, and the number of missed events are returned. The system default value upon hardware reset is Reset. Note: The counters are only 16 bits. At the shortest connection interval, this provides a little over 8 minutes of data. Note: This command is only valid for a valid connection handle (i.e. for an active connection). It is therefore not possible to read the packet error rate data once the connection has ended. |
Command Parameters
| Connection Handle: |
| | Handle used to identify a connection
| Size: | 2 byte(s) |
| Default: | 0x0000 |
| Range: | 0x0000 to 0x0EFF |
|
| PER Test Command: |
| | Reset or Read the PER counters.
| Size: | 1 byte(s)
|
| Default: | 0
|
| Range: |
| Value |
Description |
| 0 |
Reset PER Counters |
| 1 |
Read PER Counters |
|
|
Events Generated
When this command has completed, an HCI_EXT_PER event shall be generated.
HCI_EXT_ResetSystemCmd
| Opcode: | 0xFC1D |
| Command Description: |
| | This command is used to issue a hard or soft system reset. A hard reset is caused by setting the SYSRESET bit in the System Controller Reset Control register. The soft reset is currently not supported on the CC264x. |
Command Parameters
| Type: | Reset Type
| Size: | 1 byte(s)
|
| Default: | 0
|
| Range: |
| Value |
Description |
| 0x00 |
Chip Reset |
| 0x01 |
Soft Reset |
|
|
Events Generated
When this command has completed, an HCI_EXT_ResetSystemDone event shall be generated.
HCI_EXT_NumComplPktsLimitCmd
| Opcode: | 0xFC1F |
| Command Description: |
| | This command is used to set the limit on the minimum number of complete packets before a Number of Completed Packets event is returned by the Controller. If the limit is not reached by the end of a connection event, then the Number of Completed Packets event will be returned (if non^zero) based on the flushOnEvt flag. The limit can be set from one to the maximum number of HCI buffers (please see the LE Read Buffer Size command in the Bluetooth Core specification). The default limit is one; the default flushOnEvt flag is FALSE. |
Command Parameters
| Limit: | Set Number of Completed Packets Limit.
| Size: | 1 byte(s) |
| Default: | 1 |
| Range: | 0x01 to the value returned from HCI_LE_ReadBufSizeCmd |
|
| flushOnEvt: | Enable or disable flush of Number of Completed Packets at end of Event.
| Size: | 1 byte(s)
|
| Default: | 0
|
| Range: |
| Value |
Description |
| 0 |
Disable |
| 1 |
Enable |
|
|
Events Generated
When this command has completed, an HCI_EXT_NumComplPktsLimitDone event shall be generated.
HCI_EXT_GetConnInfoCmd
| Opcode: | 0xFC20 |
| Command Description: |
| | This command (which replaces Get Number Connections) is used to get the number of allocated connections, the number of active connections, and for each active connection, the connection handle, the connection role, the peer device address and peer device address type. The number of allocated connections is based on a default build value that can be changed in the project using MAX_NUM_BLE_CONNS (please see the software users guide for additional details). The number of active connections refers to active BLE connections. The information per connection is based on the structure hciConnInfo_t provided in hci.h. If all parameters are NULL, then the call to this command is considered a network processor call via a transport layer, and the results will be provided via a vendor specific command complete event.If any parameter is not NULL, then the call to this command is considered a direct function call and the valid pointers will be used to store the result. In this case, it is the users responsibility to ensure there is sufficient memory allocated! Note that partial results can be obtained by selective use of the pointers. For example, if only the number of active connections is desired, this can be obtained as follows: |
Events Generated
When this command has completed, an HCI_EXT_GetConnInfoDone event shall be generated.
HCI_EXT_SetMaxDataLenCmd
| Opcode: | 0xFC21 |
| Command Description: |
| | This command is used to set the Data Length Extension internal variables supportedMaxTxOctets, supportedMaxTxTime, supportedMaxRxOctets and supportedMaxRxTime that are normally set exclusively by the Controller to the maximum data length and duration allowed by this device (default Tx and Rx Octets is 251; default Tx and Rx Time is 2120 us [but note that any future change to support PHYs could alter the default values of Time]). |
Command Parameters
| Tx Octets: | Maximum number of payload octets that the local Controller supports for transmission of a single Link Layer Data Channel PDU.
| Size: | 2 byte(s) |
| Default: | 0 |
| Range: | 0x001B to 0x00FB |
|
| Tx Time: | Maximum time, in microseconds, that the local Controller supports for transmission of a single Link Layer Data Channel PDU.
| Size: | 2 byte(s) |
| Default: | 0 |
| Range: | 0x0148 to 0x0848 |
|
| Rx Octets: | Maximum number of payload octets that the local Controller supports for reception of a single Link Layer Data Channel PDU.
| Size: | 2 byte(s) |
| Default: | 0 |
| Range: | 0x001B to 0x00FB |
|
| Rx Time: | Maximum time, in microseconds, that the local Controller supports for reception of a single Link Layer Data Channel PDU.
| Size: | 2 byte(s) |
| Default: | 0 |
| Range: | 0x0148 to 0x0848 |
|
Events Generated
When this command has completed, an HCI_EXT_SetMaxDataLengthDone event shall be generated.
HCI_EXT_ReadRandomAddressCmd
| Opcode: | 0xFC25 |
| Command Description: |
| | This command is used to Read the controller’s own random device address |
Command Parameters
None
Events Generated
When this command has completed, an HCI_EXT_ReadRandomAddressDone event shall be generated.
HCI_EXT_GetActiveConnectionInfoCmd
| Opcode: | 0xFC2C |
| Command Description: |
| | This command is used to get connection information needed to track an active BLE connection. |
Command Parameters
| connID: | Connection ID
| Size: | 1 byte(s) |
| Default: | 0 |
| Range: | 0x0000 to 0x0EFF |
|
Events Generated
When this command has completed, an HCI_EXT_GetActiveConnInfoDone shall be generated.
HCI_EXT_GetRxStatisticsCmd
| Opcode: | 0xFC31 |
| Command Description: |
| | This command is used to get RX statistics. |
Command Parameters
| Connection Handle: |
| | Handle used to identify a connection
| Size: | 2 byte(s) |
| Default: | 0x0000 |
| Range: | 0x0000 to 0x0EFF |
|
| Command: | Resets or Reads Statistic Counters
| Size: | 1 byte(s)
|
| Default: | 0
|
| Range: |
| Value |
Description |
| 0 |
Reset (Clears all Statistic Counters) |
| 1 |
Read (Reads Statistic Counters) |
|
|
Events Generated
When this command has completed, an HCI_EXT_GetRxStatsDone event shall be generated.
HCI_EXT_GetTxStatisticsCmd
| Opcode: | 0xFC32 |
| Command Description: |
| | This command is used to get TX statistics. |
Command Parameters
| Connection Handle: |
| | Handle used to identify a connection
| Size: | 2 byte(s) |
| Default: | 0x0000 |
| Range: | 0x0000 to 0x0EFF |
|
| Command: | Resets or Reads Statistc Counters
| Size: | 1 byte(s)
|
| Default: | 0
|
| Range: |
| Value |
Description |
| 0 |
Reset (Clears all Statistic Counters) |
| 1 |
Read (Reads Statisc Counters) |
|
|
Events Generated
When this command has completed, an HCI_EXT_GetTxStatsDone event shall be generated.
HCI_EXT_GetCoexStatisticsCmd
| Opcode: | 0xFC33 |
| Command Description: |
| | This command is used to get Coexistence statistics. |
Command Parameters
| Command: | Resets or Reads Statistic Counters
| Size: | 1 byte(s)
|
| Default: | 0
|
| Range: |
| Value |
Description |
| 0 |
Reset (Clears all Statistic Counters) |
| 1 |
Read (Reads Statistic Counters) |
|
|
Events Generated
When this command has completed, an HCI_EXT_GetCoexStatsDone event shall be generated.
HCI_EXT_LESetExtendedAdvertisingDataCmd
| Opcode: | 0xFC71 |
| Command Description: |
| | This command is used to set extended ADV data. |
Command Parameters
| Connection Handle: |
| | Handle used to identify a connection
| Size: | 1 byte(s) |
| Default: | 0x00 |
| Range: | 0x00 to 0xEF |
|
| Fragment: | Allows the fragmentation of data
| Size: | 1 byte(s)
|
| Default: | 0
|
| Range: |
| Value |
Description |
| 0 |
The Controller may fragment all data |
| 1 |
The Controller should not fragment data |
|
|
| Data Length: | The number of bytes in the Advertising Data parameter
:Size: 1 byte(s)
:Range: 0 to 251
|
| Advertsing Data: |
| | Data that will be set while Advertising
:Size: N/A
|
Events Generated
When this command has completed, an HCI_EXT_LESetExtendedAdvertisingDataDone event shall be generated.
HCI_EXT_LESetExtendedScanResponseDataCmd
| Opcode: | 0xFC72 |
| Command Description: |
| | This command is used to set extended Scan Response. |
Command Parameters
| Connection Handle: |
| | Handle used to identify a connection
| Size: | 1 byte(s) |
| Default: | 0x00 |
| Range: | 0x00 to 0xEF |
|
| Fragment: | Allows the fragmentation of data
| Size: | 1 byte(s)
|
| Default: | 0
|
| Range: |
| Value |
Description |
| 0 |
The Controller may fragment all data |
| 1 |
The Controller should not fragment data |
|
|
| Data Length: | The number of bytes in the Advertising Data parameter
:Size: 1 byte(s)
:Range: 0 to 251
|
| Advertising Data: |
| | Data that will be set while Advertising
:Size: N/A
|
Events Generated
When this command has completed, an HCI_EXT_LESetExtendedScanResponseDataDone event shall be generated.
HCI Extension Events
The HCI Extension vendor specific commands generate the following vendor specific events.
HCI_EXT_SetRxGainDone
| Opcode: | 0x0400 |
| Event Description: |
| | This event is sent to indicate the RF receiver gain has been set, or that there was an error. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
HCI_EXT_SetTxPowerDone
| Opcode: | 0x0401 |
| Event Description: |
| | This event is sent to indicate the RF transmitter power has been set, or that there was an error. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
HCI_EXT_OnePacketPerEventDone
| Opcode: | 0x0402 |
| Event Description: |
| | This event is sent to indicate the One Packet Per Event feature has been enabled or disabled, or that there was an error. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
HCI_EXT_DecryptCommandDone
| Opcode: | 0x0405 |
| Event Description: |
| | This event is sent to indicate Decryption has completed. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
| Decrypted Data: | 128 bit decrypted data block. The most significant octet of plainTextData corresponds to plainTextData using the notation specified in FIPS 197.
| Size: | 16 byte(s) |
| Range: | Any 16 byte value |
|
HCI_EXT_WriteLocalFeatureSupportDone
| Opcode: | 0x0406 |
| Event Description: |
| | This event is sent to indicate the Set Local Supported Features command has completed. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
HCI_EXT_SetFastTxResponseTimeDone
| Opcode: | 0x0407 |
| Event Description: |
| | This event is sent to indicate the Set Fast Transmit Response Time feature has been enabled or disabled, or that there was an error. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
HCI_EXT_SetBDADDRDone
| Opcode: | 0x040C |
| Event Description: |
| | This event is sent to indicate the devices BLE address has been set, or that there was an error. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
HCI_EXT_SetSCADone
| Opcode: | 0x040D |
| Event Description: |
| | This event is sent to indicate the devices SCA has been set, or that there was an error. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
HCI_EXT_DisconnectImmedDone
| Opcode: | 0x0413 |
| Event Description: |
| | This event is sent to indicate the Disconnect Immediate command has completed, or that there was an error. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
HCI_EXT_PER
| Opcode: | 0x0414 |
| Event Description: |
| | This event is sent to indicate the Packet Error Rate Reset or Read command has completed, or that there was an error. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
| PER Command Type: |
| | Read or Reset
| Size: | 1 byte(s)
|
| Range: |
| Value |
Description |
| 0 |
Reset PER Counters |
| 1 |
Read PER Counters |
|
|
| RX Pkts: | Number of received packets.
| Condition: | ( cmdVal!=0x00 && cmdStat==0x00) |
| Size: | 2 byte(s) |
| Range: | Any 2 byte value |
|
| RX CRC Fails: | Number of received packets with CRC error.
| Condition: | ( cmdVal!=0x00 && cmdStat==0x00) |
| Size: | 2 byte(s) |
| Range: | Any 2 byte value |
|
| Events: | Number of connection events.
| Condition: | ( cmdVal!=0x00 && cmdStat==0x00) |
| Size: | 2 byte(s) |
| Range: | Any 2 byte value |
|
| Missed Events: | Number of missed connection events.
| Condition: | ( cmdVal!=0x00 && cmdStat==0x00) |
| Size: | 2 byte(s) |
| Range: | Any 2 byte value |
|
HCI_EXT_ResetSystemDone
| Opcode: | 0x041D |
| Event Description: |
| | This event is sent to indicate the Reset System command has completed, or that there was an error. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
HCI_EXT_NumComplPktsLimitDone
| Opcode: | 0x041F |
| Event Description: |
| | This event is sent to indicate the Number Completed Packets Limit command has completed, or that there was an error. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
HCI_EXT_GetConnInfoDone
| Opcode: | 0x0420 |
| Event Description: |
| | This event is sent to indicate the Get Connection Information command has completed. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
| Alloc Conns: | Total number of allocated connections
|
| Active Conns: | Number of currently active connections
|
An array of size “numConn” will be returned containing the parameters starting here:
| Conn Handle: | Connection Handle
|
| Conn Role: |
| Size: | 1 byte(s)
|
| Range: |
| Value |
Description |
| 0x22 |
LMP/LL Response Timeout |
| 0x23 |
LMP Error Transaction Collision |
| 0x24 |
LMP PDU Not Allowed |
| 0x25 |
Encryption Mode Not Acceptable |
| 0x26 |
Link Key Can Not be Changed |
| 0x27 |
Requested QoS Not Supported |
| 0x28 |
Instant Passed |
| 0x29 |
Pairing With Unit Key Not Supported |
| 0x2A |
Different Transaction Collision |
| 0x2B |
Reserved |
| 0x2C |
QoS Unacceptable Parameter |
| 0x2D |
QoS Rejected |
| 0x2E |
Channel Assessment Not Supported |
| 0x2F |
Insufficient Security |
| 0x30 |
Parameter Out Of Mandatory Range |
| 0x31 |
Reserved |
| 0x32 |
Role Switch Pending |
| 0x33 |
Reserved |
| 0x34 |
Reserved Slot Violation |
| 0x35 |
Role Switch Failed |
| 0x36 |
Extended Inquiry Response Too Large |
| 0x37 |
Simple Pairing Not Supported By Host |
| 0x38 |
Host Busy ^ Pairing |
| 0x39 |
Connection Rejected Due To No Suitable Channel Found |
| 0x3A |
Controller Busy |
| 0x3B |
Unacceptable Connection Interval |
| 0x3C |
Directed Advertising Timeout |
| 0x3D |
Connection Terminated Due To MIC Failure |
| 0x3E |
Connection Failed To Be Established |
| 0x3F |
MAC Connection Failed |
| 0x40 |
Coarse Clock Adjust Rejected |
| 0x41 |
Type0 Submap Not Defined |
| 0x42 |
Unknown Advertising Identifier |
| 0x43 |
Limit Reached |
| 0x44 |
Operation Cancelled by Host |
|
|
| Peer Addr: |
|
| Peer Addr Type: |
| Size: | 1 byte(s)
|
| Range: |
| Value |
Description |
| 0x00 |
Public |
| 0x01 |
Random |
| 0x02 |
Public Identity |
| 0x03 |
Random Identity |
|
|
The array of parameters ends here.
HCI_EXT_SetMaxDataLengthDone
| Opcode: | 0x0421 |
| Event Description: |
| | This event is sent to indicate the Set Max Data Length command has completed. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|
HCI_EXT_LLTestModeDone
| Opcode: | 0x0470 |
| Event Description: |
| | LL Test Mode event. |
Event Parameters
| Status: |
| Size: | 1 byte(s) |
| Range: | See Status Table |
|
| Command Opcode: |
| Size: | 2 byte(s) |
| Range: | See Command Table |
|