.. _sec-cc35xx-getting-started:

Getting Started with the SimpleLink |DEVICE|
********************************************

The |SDK| delivers components that enable engineers to develop applications on
the Texas Instruments SimpleLink |DEVICE| family of wireless microcontroller
(MCUs). This powerful software toolkit provides a cohesive and consistent
software experience for all SimpleLink |DEVICE| wireless MCU users by packaging
essential software components, such as a Bluetooth\ |reg| Low Energy (Bluetooth 
LE) protocol stack supporting Bluetooth 5.4, and Wi-Fi 6 networking stack based on
LwIP (https://savannah.nongnu.org/projects/lwip/), as well as the FreeRTOS kernel and TI
Drivers in one easy-to-use software package along with example applications and
exhaustive documentation.

Prerequisites
=============

The user is expected to have the following:

* |LP|
* XDS110 Debugger `LP-XDS110ET`_
* |SDK|
* CCS 20.4.0
* Sysconfig 1.26.0
* Putty or any other Serial Terminal Application

.. attention::
       Please note that CCS must be installed prior to moving on to the next steps. CCS is available here: `Code Composer Studio`_ .

SDK - Download and Installation
===============================

Installing the SDK
------------------
This section covers the required settings for a |SDK| installation. The |SDK|
contains all of the Documentation, Example, Kernel, Driver Sources, and tools 
required to get up and running with the SimpleLink |DEVICE| family of devices.

1.  Download the |SDK| from the `SDK Product Page <https://www.ti.com/tool/SIMPLELINK-WIFI-SDK>`_.

2.  Install to the default installation directory.


Activation and Initial Programming
==================================

This section will cover the activation and initial programming of the
SimpleLink |DEVICE|. 

.. attention::
    Please note that throughout the activation and initial programming the window should **NOT be refreshed at any
    point**. Additionally, the activation and initial programming process **should only be done ONCE** for each new |DEVICE|.

Activation
----------

When the device is first received it will be in an 'OPEN' security state , which
will not allow you to do much with until it has gone through the activation
process. The activation process will change the device ownership by flipping 
the security state to 'deployed', and add customer credentials.

For the following steps you will need to have the |LP| connected to the
|LP-XDS110| and to the PC.

.. attention::
        Make sure that both |LP-XDS110| and |LP| are connected to the same PC through two different USB-C ports. 


1. Start the Toolbox application that is downloaded along the |SDK| by navigating to the root of the `simplelink_wifi_toolbox_"platform"_x_x_x` and run the "simplelink-wifi-toolbox.exe". 
    Executing the Toolbox application will open the default browser at the Toolbox home page. Once in the home page click on the **Programmer** tool.

    .. _fig_activation-1:

    .. figure:: resources/activation-1.png
        :align: center
        :scale: 50

        Toolbox Application Home Page

2. This will open a windows that will allow you to see any XDS connected device and select onbnoard flash.
    Select the connected XDS110 device from a drop-down list of XDS-devices
    connected to the PC.

    .. _fig_activation-2:

    .. figure:: resources/activation-2.png
        :align: center
        :scale: 50

        XDS110 Select Page

    .. note::
        
        If you are using a Revision A Launchpad, select IS25WJ064F. For Launchpads Revision E4 or earlier revisions, select IS25WJ032F

    .. _fig_activation-2-1:

    .. figure:: resources/flash-options.png
        :align: center
        :scale: 50

        Flash Device Select Page

3. The following step will require you to select the activation method. 
    There are 3 options for activating the device: 

    a. **Vendor Key** - Use custom Vendor keys

    b. **SDK Example Key** - Emulate the full vendor operation using an emulation key (TI-provided 'debug' key).

    c. **Authentication Bypass** - Enable the vendor to load and execute 
    unauthenticated images.

    However for the purposes of this Quickstart User's Guide please **select the SDK example key** (if wanting to use a Vendor Key please refer to the programmer guide in the Wifi Toolbox User guide)

    .. _fig_activation-3:

    .. figure:: resources/activation-3.png
        :align: center
        :scale: 50

        Activation Type Page

4. Since the SDK example key was selected the "Root of Trust" key will be pre-selected. 
    The key is not pre-selected if the Authentication Bypass activation method is chosen. Confirm
    the "Root of Trust" key is present as show in the image below. In the drop-down box for 'Flash Reset Type',
    select 'Do not use in band' and activate the |DEVICE|.
    
    The difference between using in band and not in band flash reset types are dependent on the flash used.
    Some flashes will have the ability to reset over a hardware line (like a reset pin) or can use an inband
    command over the data lines for reset operation (as in a software reset). Ensure that the type of flash on
    the target board supports the corresponding flash reset type. Users may have to check the flash's datasheet.
    
    .. _fig_activation-4:

    .. figure:: resources/activation-4.png
        :align: center
        :scale: 50

        Activation Page

5. At the end of the activation process the tool will report a summary for review. 
    In case of failed RoT fuse-programming, the activation/programming process 
    will be halted.

    .. _fig_activation-5:

    .. figure:: resources/activation-5.png
        :align: center
        :scale: 50

        Review Page

Initial Programming
-------------------

Once the activation process has concluded, the Initial Programming process will start 
automatically in the next window. During this process you will download 
an example image and :ref:`sec-cc35xx-connectivity-core` image to the |DEVICE| 
in addition to flash configuration. As a reminder, please be sure **not to refresh the page** during this process.

    * **Image selectionBoot Sector** - Flash partition, calibration, and flash 
      high-speed configuration.
    * **TI Bootloader** - RAM-bootloader (2nd stage BL provided by TI).
    * **TI Wifi Firmware** - WiFi Servicepack
    * **Vendor Demo Image** - for FCS versions the image will program Network Terminal.

    .. _fig_programming-1:

    .. figure:: resources/programming-1.png
        :align: center

        Initial Programming Page

Press the program button to begin Initial Programming. Once programmed you will be met with the following screen.

    .. figure:: resources/programming-2.png
        :align: center

        Initial Programming Page


Example Application (Network Terminal)
--------------------------------------

As part of the initial programming process above a precompiled network terminal
example has been programmed as the vendor image. In order to use the device and 
evaluate using the demo, follow the steps below:

    1. Determine which COM port the LP-XDS110ET is connected to. On Windows this can be done by referencing Ports section in Device Manager. Two XDS devices will show, for a serial connection the COM port that is relevant belongs to the device that is labeled "Application/User UART".
    2. Open a serial terminal application such as 'Putty' or 'Tera Term'.
    3. Configure the connection as Serial with BAUD of 115200 and the COM port found in step 1.
    4. Reset the |LP| and |LP-XDS110|.
    5. The **Network Terminal** example screen should show up, providing you with
       a command-line interface that enables running basic operations. The initial bringup and/or typing ``help`` 
       will show this menu:

    .. figure:: resources/tera-term.png
        :align: center
        :scale: 150

        Network Terminal Help Screen


This allows for verification that the device has been flashed and is working. For further development please refer
to the SimpleLink Wireless MCU CC35xx Overview section.