Migration from 9.10.00.01 |rarr| 9.13.00.13
===========================================

This page will go over the main changes between SDK version 9.10.00.01 and 9.13.00.13

WLAN Driver
-----------

Wlan_RoleUp
^^^^^^^^^^^

- Added RoleUpStaCmd_t type, API will now use this type instead RoleUpApCmd_t type.
- Added new WPS params to RoleUpStaCmd_t and RoleUpApCmd_t

Cryptography Driverlibs
-----------------------

All the cryptographic drivers have changed naming convention

For example the HSM driver changed from HSMLPF3 to HSMXXF3 all APIs and functions have similarly changed names

.. figure:: resources/HSM_driver_changes.png
    :align: center
    :width: 45%

Please update accordingly to your project

Build System
------------

CCS_projects directory was removed and with it replaced by cmake configuration to now build all libraries.