.. _Memory Overview: ../memory/memory.html
.. _here: ../memory/cc35xx-nvs.html

Over the Air Update (OTA)
=========================

The CC35xx device leverages ARM PSA (Platform Security Architecture) libraries to perform OTA updates. PSA is the new standard for
OTA security in ARM devices, read more about it at https://www.psacertified.org/ 
The CC35xx follows the Firmware Update (FWU) specifications and APIs created by ARM. https://arm-software.github.io/psa-api/fwu/
The following is the flow of an Over the Air Update.

OTA Container States
--------------------
To support OTA updates, two slots are allocated for most entities stored on the flash (e.g. TI bootloader, application, TI wireless firmware, etc). The primary slot will contain the active version of the entity and the secondary slot is reserved for storing new copies that are loaded during the OTA process (for validating and testing). This enables a reliable OTA solution where the device is always able to return to the current working version if the OTA is interrupted or fails.
You can choose to only update one entity or multiple at the same time via OTA.

The picture below depicts the format of the image and servicepack containers.  
The image container holds the application code and the servicepack container holds the TI wireless firmware. Each will have a primary and 
secondary slot (4 total).

Note that the image container addresses are shown in `Memory Overview`_

.. figure:: resources/GPE-slot.png
   :align: center
   :scale: 100 

* Additional Details: 

  - Container Manifest: Has metadata about a GPE image and includes header and version
  - Vendor TLVs: Type-Length-Value but we do not support this yet
  - Container Trailer: Records update progress, swap status, and slot status


+--------------------------+-------------------------------------------------------------+
| OTA Container State      | Description                                                 |
+==========================+=============================================================+
| Ready                    | The second container slot is ready for a new Firmware       |
|                          | update to be started                                        |
+--------------------------+-------------------------------------------------------------+
| Writing                  | When writing is complete, the image becomes a Candidate for |
|                          | installation                                                |
+--------------------------+-------------------------------------------------------------+
| Candidate                | Container slot has been filled, it can now be set to be the |
|                          | next active image                                           |
+--------------------------+-------------------------------------------------------------+
| Staged                   | Container Slot has been set to be the active image,         |
|                          | next time the device reboots                                |
+--------------------------+-------------------------------------------------------------+
| Trial                    | The Update is now the active image running in trial mode.   |
|                          | It requires the trial to be explicitly accepted to make the |
|                          | update permanent. If rejected the container is marked       |
|                          | and image is reverted to previous container                 |
+--------------------------+-------------------------------------------------------------+
| Failed/Rejected          | An update to a new image has been attempted, but has failed,|
|                          | or been cancelled for some reason                           |
+--------------------------+-------------------------------------------------------------+
| Updated                  | New image has passed trial and container slot becomes the   | 
|                          | new valid image while the previous is cleaned               |
+--------------------------+-------------------------------------------------------------+

OTA Process
-----------

.. figure:: resources/OTA-flow.png
   :align: center
   :scale: 100 

The graphic above shows a state machine of the OTA process.

* First a call to the function `psa_fwu_init(void)` must be done to set the secondary slot to the `Ready` state. 
* If there is an update available and the slot is `Ready` (can be checked with `psa_fwu_query`), `psa_fwu_start(component, *manifest, manifest_size)` will begin the OTA process and validate the Container Manifest
.. note:: 

  Call `psa_fwu_clean(component)` before any `psa_fwu_start` call

* If the start command passes, we can then move onto `psa_fwu_write(component, image_offset, *block, size_t block_size)` which writes a firmware image (or part of a firmware image) to the slot. This will move the container to the `Writing stage`. Once writing is complete,
  calling the function `psa_fwu_finish(component)` will move the Container onto the `Candidate` stage and mark the firmware image in the GPE slot as ready for installation.
* In the `Candidate` stage can now choose to stage this container to be used as the next active image by calling `psa_fwu_install(void)`. This will move
  the Container to the `Staged` state
* Once `Staged` the CC35xx device will require a reboot to load the newly updated container. This is done by calling `fwu_request_reboot()`. Rebooting
  will move the Container to the `Trial` stage.
* In the `Trial` stage the device is tested by the vendor. If rejected, the Container slot will become invalid and a reboot will revert to the previous Container
  slot and image. If accepted, the Container slot will be set to be the new primary slot and move to the `Updated` stage on the next reboot by calling `fwu_request_reboot(void)`.
  The previous container slot becomes the secondary slot and needs to be cleaned with `psa_fwu_clean(component)`.

To see what state of the OTA process the container is at anytime call the `psa_fwu_query(component, *info)` command. The OTA process can be rejected at any stage with
`psa_fwu_cancel(component)` once the update has begun till the time it is `Updated`, in which the GPE firmware image update status will be marked as `FAILED`. When you are in the trial stage,
you cannot cancel the "update" unless you trigger self reboot, in which you would then call `psa_fwu_cancel(component)`.

Important Arguments Explained
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^

  - `psa_fwu_component_t component`: 

    - either the primary or secondary vendor slot 
  - `psa_fwu_component_info_t *info`: 
  
    - the output value that gives you information about the component ie. state, whether it is primary or secondary slot etc.
  - `const void *manifest`: 
  
    - contains GPE header, version etc.
  - `size_t image_offset`: 
  
    - the offset of the data block in the whole image (see `XMEMWFF3_write` in `psa_fwu.c`)
  - `const void *block`: 
  
    - data block
  - `size_t manifest_size`:
    
    - Size of the manifest defined by `TI_FWU_MANIFEST_SIZE` which refers to the size of the `PSA_FWU_GPESlot_t` struct declared in `psa_fwu.h`

Enabling OTA
------------

To enable OTA in your project you must change the following setting in the `Memory Map` section of the sysconfig file.

.. figure:: resources/ota_syscfg.png
    :align: center
    :scale: 60

For a 4MB Flash, enabling this checkbox will create space for a second container, however, it will configure each container image size to 1078KB from the original 2752KB.
This will also automatically update the slots addresses in the `ti_flash_map_config.c`. You can find more information in the Memory section of the user guide.

.. note::
    When using a 8MB, 16MB, or 32MB Flash, OTA is automatically enabled and the setting in SYSCFG will be locked.

    .. figure:: resources/ota_setting_syscfg.png
        :align: center

OTA & NVS Region 
----------------
Content stored in the NVS region may be modified during an OTA, but the NVS region is not designed to be updated as a complete unit. Therefore, only a single region in the flash is allocated for the NVS and the application is responsible for managing it (i.e. performing create, read, write, delete operations). For more information on updating the NVS region via the NVOCMP driver, please see `here`_.

OTA Limitations 
---------------------

* You cannot redefine flash sizes or PSRAM presence ie. cannot start with "no PSRAM" configured on a stacked device and then OTA to "enable PSRAM", nor can you indicate a larger or smaller flash chip size 
* You cannot OTA different interface settings between the CC35xx and flash chip 
* You cannot OTA a different OTFDE to redefine what is and isn't encrypted in the flash region 
* You cannot redefine if code is allocated to secure or non-secure calable region 
* You cannot change flash partitions via OTA (i.e. flash map and entity sizes are fixed forever)
* You cannot OTA the boot sector 
* If a device currently does not support factory image restoration, you cannot OTA this capability when it is supported afterwards because you are OTA-ing a functionality that was previously programmed based on an SDK that could not handle factory image restoration 

.. Rollback Protection 
.. -------------------

.. * Rollback protection is to ensure you can NOT go back to a firmware of an older version 

..   - Use Case: If your firmware had vulnerabilities and a newer version addresses these, we do not want malicious people to try to revert the device back to a "vulnerable" state