.. _sec-cc35xx-hw-overview:

Hardware Overview
=================

.. important::

    The main source of information for |DEVICE| hardware is the Technical 
    Reference Manual:

System Core
-----------

The system core is designed to run the wireless protocol stack from the
network layer up to the user application.

- For CC35xx devices the system core is ARM Cortex M33

You can read more about ARM Cortex in the `ARM Cortex-M33 documentation`_.

The network layer interfaces to the radio core through a software module called the
Net driver. The RF driver runs on the system core and acts as an interface to the 
radio on the |DEVICE|, and also manages the power domains of the radio hardware 
and radio core. Documentation for the Net driver can be found at the |TI_DRIVERS_API|.

.. _sec-cc35xx-connectivity-core:

Connectivity Core
-----------------

The Connectivity Core  within the |DEVICE| is a Cortex M3 processor responsible for both interfacing
to the radio hardware, and translating complex instructions from the system core
into bits that are sent over the air using the radio. The Connectivity Core
implements the PHY and DATA Link layers of the protocol stack and is able to operate
autonomously, this frees up the system core for higher-level protocol and
application-layer processing.

The system core communicates with the Connectivity Core through a direct memory hardware 
interface, which is documented in the |TRM|. The connectivity core firmware is not
intended to be used or modified by the application developer.




Flash, RAM, and Peripherals
---------------------------

The following in-system programmable SRAM options are available
for the |DEVICE|. For a full memory of your device, please refer to the |DEVICE|
datasheet.

+------------------------+------------+-----------+
| Device                 | Flash (kB) | SRAM (kB) |
+========================+============+===========+
| CC35xx                 | External   | 1200      |
+------------------------+------------+-----------+

Supported Flashes
^^^^^^^^^^^^^^^^^

The |DEVICE| currently supports the following flash devices

+---------------+---------------------+-----------+
|Vendor         | Name                |  Size(MB) |
+===============+=====================+===========+
|ISSI           | IS25WJ032F          | 4         |
+---------------+---------------------+-----------+
|ISSI           | IS25WJ064F          | 8         |
+---------------+---------------------+-----------+
|Winbond*       | W25Q32JW            | 4         |
+---------------+---------------------+-----------+
|Winbond*       | W25Q64JW            | 8         |
+---------------+---------------------+-----------+
|Winbond*       | W25Q128JW           | 16        |
+---------------+---------------------+-----------+
|Gigadevice     | GD25LF32E           | 4         |
+---------------+---------------------+-----------+
|Gigadevice     | GD25LF64E           | 8         |
+---------------+---------------------+-----------+
|Puya           | PY25Q32LB           | 4         |
+---------------+---------------------+-----------+
|Puya           | PY25Q64LB           | 8         |
+---------------+---------------------+-----------+
|Puya           | PY25Q128LA          | 16        |
+---------------+---------------------+-----------+
|Puya           | PY25Q256LC          | 32        |
+---------------+---------------------+-----------+

.. Warning::

    *The Winbond devices are not recommended for new designs due to performance limitations

Note that there is no DRR support or OSPI support (QSPI only)

The following list are experimental flashes are supported but not yet system tested

+---------------+---------------------+-----------+
|Vendor         | Name                |  Size(MB) |
+===============+=====================+===========+
|ISSI           | IS25WJ128F          | 16        |
+---------------+---------------------+-----------+
|Macronix       | MX25U3235F          | 4         |
+---------------+---------------------+-----------+
|Macronix       | MX25U6435F          | 8         |
+-------------------------------------------------+


The |DEVICE| also hosts a full range of peripherals
including UART, I2C, I2S, AES, TRNG, temperature and battery monitors, 4x 32-bit
timers, 2x SSI, and an integrated Hardware Security Module (HSM).

Below is a sample device block diagram. Please check the datasheet for an
accurate block diagram of your device.

.. figure:: ../resources/fig-cc355x-block-diagram.png
    :name: fig-cc355x-block-diagram
    :align: center

    SimpleLink™ CC355x Block Diagram

Startup Sequence
----------------

For a complete description of the |DEVICE| reset sequence, see the |TRM|.

.. important::

    The main source of information for |DEVICE| hardware is the Technical 
    Reference Manual:

.. _sec-resets: