.. _gap:

Generic Access Profile (GAP)
============================

The GAP layer is responsible for connection functionality. This layer handles the
access modes and procedures of the device including device
discovery, link establishment, link termination, initiation of
security features, and device configuration. See :ref:`gap_state_diagram` for
more details.

.. _gap_state_diagram:
.. figure:: resources/image72.jpeg
    :align: center

    GAP State Diagram.

Based on the role for which the device is configured, :ref:`gap_state_diagram`
shows the states of the device. The following describes these states.

-  **Standby**: The device is in the initial idle state upon reset.

-  **Advertiser**: The device is advertising with specific data letting
   any initiating devices know that it is a connectable device (this
   advertisement contains the device address and can contain some
   additional data such as the device name).

-  **Scanner**: When receiving the advertisement, the scanning device
   sends a scan request to the advertiser. The advertiser responds
   with a scan response. This process is called device discovery.
   The scanning device is aware of the advertising device and can
   initiate a connection with it.

-  **Initiator**: When initiating, the initiator must specify a peer
   device address to which to connect. If an advertisement is
   received matching that address of the peer device, the initiating
   device then sends out a request to establish a connection (link) with the
   advertising device with the connection parameters described in
   :ref:`connection_parameters`.

-  **Peripheral/Central**: When a connection is formed, the device functions
   as a Peripheral if it is the advertiser and a Central if it is the initiator.

Bluetooth devices operate in one or more GAP roles based on the application use
case. The GAP roles utilize one or more of the GAP states.
Based on this configuration, many Bluetooth Low Energy protocol stack events
are handled directly by the main application task and sometimes routed from the
GAP Bond Manager. The application can register with the stack to be notified of
certain events.

.. _gap_roles:

GAP Roles
^^^^^^^^^

Based on the configuration of the device, the GAP layer always operates in one
of four (4) roles as defined by the specification:

-  **Broadcaster** - The device is an advertiser that is non connectable.

-  **Observer** - The device scans for advertisements but cannot initiate
   connections.

-  **Peripheral** - The device is an advertiser that is connectable and operates as
   Peripheral in a single link-layer connection.

-  **Central** - The device scans for advertisements and initiates
   connections and operates as a Central in a single or multiple
   link-layer connections.

The Bluetooth Core Specifications allows for certain combinations of multiple roles

GAP Advertiser
^^^^^^^^^^^^^^

The following list describes how to configure the GAP for
advertising. The **network terminal** example project will be used as an example.

.. _sbp_gap_configuration_example:

**Configure Advertisement instance with** `ble_gap_ext_adv_configure()`

    .. code-block:: c 

        int ble_gap_ext_adv_configure(uint8_t instance,
                              const struct ble_gap_ext_adv_params *params,
                              int8_t *selected_tx_power,
                              ble_gap_event_fn *cb, void *cb_arg);

   The function takes the advertisement parameters which need to be filled out from the following struct

    .. code-block:: c
     :caption: **nimble_host.c::nimble_host_ext_adv_cfg()** - Network Terminal advertising default parameters 
         
        struct ble_gap_ext_adv_params params;

        params.legacy_pdu = 1;
            if (params.legacy_pdu) {
                params.connectable = 1;
                params.scannable = 1;
                params.include_tx_power = 0;
            }
            else
            {
                params.connectable = 1;
                params.scannable = 0;
                params.include_tx_power = 0;
            }
            params.directed = 0;
            params.high_duty_directed = 0;
            params.anonymous = 0;
            params.scan_req_notif = 0;
            if (params.directed && params.legacy_pdu) {
                params.scannable = 0;
            }

            /* Other adv parameters */
            params.itvl_min = 100;
            params.itvl_max = 100;
            params.channel_map = 0x7;
            params.peer.type = BLE_OWN_ADDR_PUBLIC;
            os_memset(params.peer.val,0x00,BLE_DEV_ADDR_LEN);
            params.own_addr_type = own_addr_type;
            params.filter_policy = 0x0;
            params.tx_power = 127;
            params.primary_phy = 1;
            params.secondary_phy = 1;
            params.sid = 0;

           

**Set Advertisers virtual address** 
    The application can set a predefined public address or
    choose to generate a random address to advertise (for added security).

    .. code-block:: c
     :caption: **nimble_host.c::nimble_host_ext_adv_cfg()** - Network Terminal advertising address 
    
        /* Set adv Address */
        if (own_addr_type == BLE_OWN_ADDR_PUBLIC) {
            rc = ble_hs_id_copy_addr(BLE_ADDR_PUBLIC, addr.val, NULL);
            if ( rc != 0 )
            {
                console_printf("\n\rERROR: fail to retrieves one of the device's identity addresses, with error code: %d\n\r",rc);
                return (rc);
            }
        } else {
            rc = ble_hs_id_gen_rnd(1, &addr);
            if ( rc != 0 )
            {
                console_printf("\n\rERROR: fail to generates a new random address, with error code: %d\n\r",rc);
                return (rc);
            }
            /* Set random address for advertising instance */
            rc = ble_gap_ext_adv_set_addr(pAdvCfg->instance, &addr);
            if ( rc != 0 )
            {
                console_printf("\n\rERROR: fail to set random address for configured advertising instance, with error code: %d\n\r",rc);
                return (rc);
            }
        }

**Load Advertisement and Scan Response data**
   Advertising and scan response data is decoupled from the advertising set. That is, it is possible for multiple
   advertising instances to use the same memory for advertising\/scan response data. An
   advertising set could also use the same memory for its advertising and scan
   response data. (Note that this requires diligence as there are some data types
   that are only allowed once in the advertisement and scan response data.)

    Advertisement data is set with `ble_gap_ext_adv_set_data()`
    
    .. code-block:: c 
        
        int ble_gap_ext_adv_set_data(uint8_t instance, struct os_mbuf *data);

    The function needs the instance of the adv set this data will populate as well as the data.

    Using the function `ble_hs_adv_set_fields_mbuf()` you can get a buffer of data from setting the 
    `ble_hs_adv_fields` struct.

    .. code-block:: c
     :caption: **nimble_host.c::nimble_host_ext_adv_cfg()** - Network Terminal advertising data
    
        struct ble_hs_adv_fields adv_fields;
        struct os_mbuf *adv_data;

         /* Set ADV fields */
        memset(&adv_fields, 0, sizeof(adv_fields));
        /* General Discoverable and BrEdrNotSupported */
        adv_fields.flags = BLE_HS_ADV_F_DISC_GEN | BLE_HS_ADV_F_BREDR_UNSUP;
        adv_fields.tx_pwr_lvl_is_present = 0;
        adv_fields.tx_pwr_lvl = BLE_HS_ADV_TX_PWR_LVL_AUTO;
        /* Set device name as instance name */
        adv_fields.name = (uint8_t *) device_name;
        adv_fields.name_len = strlen(device_name);
        adv_fields.name_is_complete = 1;
        /* Manufacturer specific data */
        adv_fields.mfg_data = (uint8_t*)mgf_data;
        adv_fields.mfg_data_len = BLE_MGF_DATA_LEN;
        /* Get Packet Header */
        /* Default to legacy PDUs size, mbuf chain will be increased if needed */
        adv_data = os_msys_get_pkthdr(BLE_HCI_MAX_ADV_DATA_LEN, 0);
        if ( adv_data == NULL )
        {
            console_printf("\n\rERROR: failed to allocate memory for adv data\n\r");
            return (-1);
        }
        /* Set ADV fields */
        rc = ble_hs_adv_set_fields_mbuf(&adv_fields, adv_data);
        if ( rc != 0 )
        {
            console_printf("\n\rERROR: failed to set adv set fields, with error code: %d\n\r", rc);
            os_mbuf_free_chain(adv_data);
            return (rc);
        }
        /* Set ADV Data */
        rc = ble_gap_ext_adv_set_data(pAdvCfg->instance, adv_data);

.. note::
  There are more fields that can be set for advertisement data such as service UUIDs, however, this is what is used
  in the network terminal example

**Enable / Disable advertising.** 
    Calling `ble_gap_ext_adv_start` will start advertising.

    .. code-block:: c
     :caption: **nimble_host.c::nimble_host_ext_adv_enable()** - Start advertising
        
        int ble_gap_ext_adv_start(uint8_t instance, int duration, int max_events);

The above steps can be repeated to create multiple advertising sets. There is an
upper limit of six advertising sets (defined in the controller). The heap may
also restrict the number of advertising sets you can create in one application.

**Changing advertising parameters**

In order to change an individual parameter after advertising has been enabled,
advertising must first be disabled. Re-enable advertising after the parameter is modified.

.. _gapscanner:

GAP Scanner
^^^^^^^^^^^

The GAP Scanner performs Extended Scanning and Legacy Scanning.

**Set scan parameters.**
First we must set the set the `ble_gap_ext_disc_params` struct for each PHY

    .. note::
        Make sure the scanning window is at least twice the length of the expected advertising interval to ensure at least 1 advertising event 
        is captured in each scanning window. Otherwise, the scanning device may not find the advertising device.

    .. code-block:: c
     :caption: **nimble_host.c::nimble_host_ext_scan_enable()** - Set Scanning Parameter

            struct ble_gap_ext_disc_params uncoded_params;

            uncoded_params.itvl = BLE_GAP_SCAN_ITVL_MS(100);
            uncoded_params.window = BLE_GAP_SCAN_ITVL_MS(50);
            uncoded_params.passive = 1;

**Start scanning**
The function `ble_gap_ext_disc()` will initiate the discovery procedures
    .. note::
     Remember to reset scan results every time you start scanning.

    .. code-block:: c

        int ble_gap_ext_disc(uint8_t own_addr_type, uint16_t duration, uint16_t period,
                     uint8_t filter_duplicates, uint8_t filter_policy,
                     uint8_t limited,
                     const struct ble_gap_ext_disc_params *uncoded_params,
                     const struct ble_gap_ext_disc_params *coded_params,
                     ble_gap_event_fn *cb, void *cb_arg);

    You will need to also choose the duration, period, filter_duplicate, filter policy

    .. code-block:: c
        :caption: **nimble_host.c::nimble_host_ext_scan_enable()** - Scanning Network Terminal Defaults

            ble_gap_ext_disc(own_addr_type, 300, 1, 1, 0, 0, pUncodedParams, pCodedParams, gap_event_cb, NULL);


#. Advertisement Reports
Note that during scanning, individual advertisements and scan responses are
returned as `BLE_GAP_EVENT_EXT_DISC` in the GAP callback function.  
By default, duplicate reports are filtered such that only one event is returned to
the application per peer device address.

The maximum amount of scan responses that can be discovered during one scan can
be set with the `BLE_MAX_SCAN_RESULTS`

**Obtain Advertising Fields from Advertising Report**

The application can extract the advertising fields from the advertising report received in the callback function `gap_event_cb`

    .. code-block:: c
        :caption: **nimble_host.c::gap_event_cb()** - BLE_GAP_EVENT_EXT_DISC

             case BLE_GAP_EVENT_EXT_DISC:
                if (extScanCB.extScanResultsCount < BLE_MAX_SCAN_RESULTS)
                {
                    rc = ble_hs_adv_parse_fields(&adv_fields, event->ext_disc.data, event->ext_disc.length_data);

                    if( rc != 0 )
                    {
                        console_printf("ERROR: failed to parse adv fields with error code: %d\n\r",rc);
                        return  rc;
                    }

                    // Store partial adv report data
                    os_memcpy(&extScanCB.extScanResults[extScanCB.extScanResultsCount].addr,&event->ext_disc.addr,sizeof(ble_addr_t));
                    extScanCB.extScanResults[extScanCB.extScanResultsCount].prim_phy = event->ext_disc.prim_phy;
                    extScanCB.extScanResults[extScanCB.extScanResultsCount].rssi = event->ext_disc.rssi;
                    os_memcpy(extScanCB.extScanResults[extScanCB.extScanResultsCount].local_name,no_local_name,7);

                    if (adv_fields.name != NULL) {
                        if (adv_fields.name_len < (BLE_DEVICE_LOCAL_NAME_LEN-1)) {
                            os_memcpy(extScanCB.extScanResults[extScanCB.extScanResultsCount].local_name, adv_fields.name, adv_fields.name_len);
                            extScanCB.extScanResults[extScanCB.extScanResultsCount].local_name[adv_fields.name_len] = '\0';
                        }
                    }

                    extScanCB.extScanResultsCount++;
                }
                extScanCB.extScanResultsTotal++;
                break;


**Filtering**

The GAP Scanner module provides 5 different types of filter to reduce the amount of advertising
report notifications to the application and eventually save memory and power consumption.
The result of the filtering affects both advertising reports and advertising report recording.
The packets filtered out by the filter configurations are discarded and will
neither be reported nor recorded. 

    .. code-block:: c
        :caption: **nimble_host.c::gap_event_cb()** - BLE_GAP_EVENT_EXT_DISC
        
        * Scanning filter policy
        *  NO_WL:
        *      Scanner processes all advertising packets (white list not used) except
        *      directed, connectable advertising packets not sent to the scanner.
        *  USE_WL:
        *      Scanner processes advertisements from white list only. A connectable,
        *      directed advertisment is ignored unless it contains scanners address.
        *  NO_WL_INITA:
        *      Scanner process all advertising packets (white list not used). A
        *      connectable, directed advertisement shall not be ignored if the InitA
        *      is a resolvable private address.
        *  USE_WL_INITA:
        *      Scanner process advertisements from white list only. A connectable,
        *      directed advertisement shall not be ignored if the InitA is a
        *      resolvable private address.
        
        #define BLE_HCI_SCAN_FILT_NO_WL             (0)
        #define BLE_HCI_SCAN_FILT_USE_WL            (1)
        #define BLE_HCI_SCAN_FILT_NO_WL_INITA       (2)
        #define BLE_HCI_SCAN_FILT_USE_WL_INITA      (3)
        #define BLE_HCI_SCAN_FILT_MAX               (3)

GAP Initiator
^^^^^^^^^^^^^

The initiator module is used to initiate the connection to a peripheral device.
An initiator generally scans for advertisements then connects to a specific
device. The initiator is a short lived state that transitions to the Central
Role after a connection is established.

To begin a connection the following function must be called

    .. code-block:: c
        :caption: **ble_gap.h::ble_gap_ext_connect()** - Connect function

        int ble_gap_ext_connect(uint8_t own_addr_type, const ble_addr_t *peer_addr,
                        int32_t duration_ms, uint8_t phy_mask,
                        const struct ble_gap_conn_params *phy_1m_conn_params,
                        const struct ble_gap_conn_params *phy_2m_conn_params,
                        const struct ble_gap_conn_params *phy_coded_conn_params,
                        ble_gap_event_fn *cb, void *cb_arg);
        
**Connection Parameters**

This section describes the connection parameters which are sent by
the initiating device with the connection request

-  **Connection Interval** - In Bluetooth Low Energy connections, a
   frequency-hopping scheme is used. The two devices each send and
   receive data from one another only on a specific channel at a
   specific time. These devices meet a specific amount of time later
   at a new channel (the link layer of the Bluetooth Low Energy
   protocol stack handles the channel switching). This meeting
   where the two devices send and receive data is known as a
   ``connection event``. If there is no application data to be sent or
   received, the two devices exchange link layer data with empty 
   application payload to maintain the connection. 
   The connection interval is the amount of time
   between two connection events in units of 1.25 ms. The connection
   interval can range from a minimum value of 6 (7.5 ms) to a
   maximum of 3200 (4.0 s). See :ref:`gap_connection_event` for more details.

.. _gap_connection_event:
.. figure:: resources/image73.jpeg
    :align: center

    Connection Event and Interval


-  **Peripheral Latency** - Formerly known as 'Slave Latency'.
   This parameter gives the Peripheral 
   device the option of skipping a number of connection events. This
   ability gives the peripheral device some flexibility. If the
   peripheral does not have any data to send, it can skip connection
   events, stay asleep, and save power. The peripheral device
   selects whether to wake or not on a per connection event basis.
   The peripheral can skip connection events but must not skip more
   than allowed by the Peripheral latency parameter or the connection
   fails. See picture below for more details.

.. ditaa::
   :--no-separation:
   :--no-shadows:

     Peripheral Latency 0

       +----+ +----+          +----+ +----+          +----+ +----+          +----+ +----+          +----+ +----+            
       | C  | | P  |          | C  | | P  |          | C  | | P  |          | C  | | P  |          | C  | | P  |            
       |cGRE| |cAAA|          |cGRE| |cAAA|          |cGRE| |cAAA|          |cGRE| |cAAA|          |cGRE| |cAAA|
       +----+-+----+----------+----+-+----+----------+----+-+----+----------+----+-+----+----------+----+-+----+
       <---------------------->                                                                       
         Connection Interval             

     Peripheral Latency 3

       +----+ +----+          +----+                 +----+                 +----+                 +----+ +----+
       | C  | | P  |          | C  |                 | C  |                 | C  |                 | C  | | P  |
       |cGRE| |cAAA|          |cGRE|                 |cGRE|                 |cGRE|                 |cGRE| |cAAA|
       +----+-+----+----------+----+-----------------+----+-----------------+----+-----------------+----+-+----+
       <---------------------->
         Connection Interval                                                                       

-  **Supervision Time-out** - This time-out is the maximum amount of
   time between two successful connection events. If this time
   passes without a successful connection event, the device
   terminates the connection and returns to an unconnected state.
   This parameter value is represented in units of 10 ms. The
   supervision time-out value can range from a minimum of 10 (100
   ms) to 3200 (32.0 s). The time-out must be larger than the
   effective connection interval (see :ref:`effective_connection_interval` for
   more details).

.. _effective_connection_interval:

**Effective Connection Interval**

The effective connection interval is equal to the amount of time
between two connection events, assuming that the Peripheral skips the
maximum number of possible events if Peripheral latency is allowed (the
effective connection interval is equal to the actual connection
interval if Peripheral latency is set to 0).

The Peripheral Latency value represents the maximum number of events that
can be skipped. This number can range from a minimum value of 0
(meaning that no connection events can be skipped) to a maximum of
499. The maximum value must not make the effective connection
interval (see the following formula) greater than 16 s. The interval
can be calculated using the following formula:

 ``Effective Connection Interval = (Connection Interval) * (1 + [Peripheral Latency])``

Consider the following example:

-  Connection Interval: 80 (100 ms)

-  Peripheral Latency: 4

-  Effective Connection Interval: (100 ms) * (1 + 4) = 500 ms

When no data is being sent from the Peripheral to the Central, the Peripheral
transmits during a connection event once every 500 ms.

.. _connection_parameter_considerations:

**Connection Parameter Considerations**

In many applications, the Peripheral skips the maximum number of
connection events. Consider the effective connection interval when
selecting or requesting connection parameters. Selecting the correct
group of connection parameters plays an important role in power
optimization of the Bluetooth Low Energy device. The following list
gives a general summary of the trade-offs in connection parameter
settings.

Reducing the connection interval does as follows:

-  Increases the power consumption for both devices
-  Increases the throughput in both directions
-  Reduces the time for sending data in either direction

Increasing the connection interval does as follows:

-  Reduces the power consumption for both devices
-  Reduces the throughput in both directions
-  Increases the time for sending data in either direction

Reducing the Peripheral latency (or setting it to zero) does as follows:

-  Increases the power consumption for the peripheral device
-  Reduces the time for the peripheral device to receive the data sent
   from a central device

Increasing the Peripheral latency does as follows:

-  Reduces power consumption for the peripheral during periods when the
   peripheral has no data to send to the central device
-  Increases the time for the peripheral device to receive the data sent
   from the central device

**Connection Parameter Update**

In some cases, the central device requests a connection with a
peripheral device containing connection parameters that are
unfavorable to the peripheral device. In other cases, a peripheral
device might have the desire to change connection parameters in the middle of a
connection, based on the peripheral application.

This can be done with `ble_gap_update_params()`

    .. code-block:: c
        :caption: **ble_gap.h::le_gap_update_params()** - Update Connection Parameters

        int ble_gap_update_params(uint16_t conn_handle,
                          const struct ble_gap_upd_params *params);    

The `le_gap_upd_params` contains six parameters:

.. code-block:: c
        :caption: **ble_gap.h::le_gap_update_params()** - Update Connection Parameters

        struct ble_gap_upd_params {
            /** Minimum value for connection interval in 1.25ms units */
            uint16_t itvl_min;

            /** Maximum value for connection interval in 1.25ms units */
            uint16_t itvl_max;

            /** Connection latency */
            uint16_t latency;

            /** Supervision timeout in 10ms units */
            uint16_t supervision_timeout;

            /** Minimum length of connection event in 0.625ms units */
            uint16_t min_ce_len;

            /** Maximum length of connection event in 0.625ms units */
            uint16_t max_ce_len;
        };

Sending a Connection Parameter Update Request is optional and it is not
required for the central device to accept or apply the requested
parameters. Some applications try to establish a connection at a
faster connection interval to allow for a faster service discovery
and initial setup. These applications later request a longer
(slower) connection interval for optimal power usage.

**Connection Event Callback**

    +-------------------------+--------------------------------------------------------------------+
    |     **eventType**       |     **Description**                                                |
    +=========================+====================================================================+
    |BLE_GAP_EVENT_CONNECT    | This event is returned when connection is established. When this   |
    |                         | returns, the eventCount will be 0.                                 |
    +-------------------------+--------------------------------------------------------------------+
    |BLE_GAP_EVENT_CONN_UPDATE| This event is returned when connection parameters are updated      |
    |                         |                                                                    |
    +-------------------------+--------------------------------------------------------------------+
    |BLE_GAP_EVENT_DISCONNECT | This event occurs on disconnections from either side               |
    +-------------------------+--------------------------------------------------------------------+

**Connection Termination**

Either the Central or the Peripheral can terminate a connection for any
reason. One side initiates termination and the other side must
respond before both devices exit the connected state. 

To disconnect call `ble_gap_terminate`

.. code-block:: c
        :caption: **ble_gap.h:: ble_gap_terminate()** - Terminate connection
        
        int ble_gap_terminate(uint16_t conn_handle, uint8_t hci_reason);