Data Fields
ECC_NISTP521_Param Union Reference

Union to access ECC_NISTP521 curve params in bytes or words. More...

#include <ECCParamsXXF3HSM.h>

Data Fields

uint8_t byte [(66+2)]
 
uint32_t word [(66+2)/sizeof(uint32_t)]
 

Detailed Description

Union to access ECC_NISTP521 curve params in bytes or words.

Field Documentation

§ byte

uint8_t ECC_NISTP521_Param::byte[(66+ 2)]

§ word

uint32_t ECC_NISTP521_Param::word[(66+ 2)/sizeof(uint32_t)]

The documentation for this union was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale