Data Fields
ECC_NISTP192_Param Union Reference

Union to access ECC_NISTP192 curve params in bytes or words. More...

#include <ECCParamsXXF3HSM.h>

Data Fields

uint8_t byte [24]
 
uint32_t word [24/sizeof(uint32_t)]
 

Detailed Description

Union to access ECC_NISTP192 curve params in bytes or words.

Field Documentation

§ byte

uint8_t ECC_NISTP192_Param::byte[24]

§ word

uint32_t ECC_NISTP192_Param::word[24/sizeof(uint32_t)]

The documentation for this union was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale