Data Fields
ECDSAXXF3HSM_HWAttrs Struct Reference

ECDSAXXF3HSM Hardware Attributes. More...

#include <ECDSAXXF3HSM.h>

Data Fields

uint8_t dummy
 

Detailed Description

ECDSAXXF3HSM Hardware Attributes.

ECDSAXXF3HSM hardware attributes should be included in the board file and pointed to by the ECDSA_config struct.

Field Documentation

§ dummy

uint8_t ECDSAXXF3HSM_HWAttrs::dummy

The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale