RNGXXF3HSM.h File Reference

Detailed Description

RNG driver implementation for the F3 family.

============================================================================

This file should only be included in the board file to fill the RNG_config structure.

This is a temporary RNG implementation that uses a constant seed to derive random numbers. This implementation will be updated to HSM's TRNG to seed the RNG driver.

Note
This implementation does not support the RNG_RETURN_BEHAVIOR_CALLBACK return mode.
This implementation treats RNG_RETURN_BEHAVIOR_POLLING as RNG_RETURN_BEHAVIOR_BLOCKING.
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/RNG.h>
Include dependency graph for RNGXXF3HSM.h:

Go to the source code of this file.

© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale