Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
ECCParams.h File Reference

Detailed Description

============================================================================

This file contains a common definition for elliptic curve structures used throughout the ECC based drivers. Not all devices support every curve.

#include <stdint.h>
#include <stddef.h>
#include <stdbool.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
#include <ti/devices/DeviceFamily.h>
#include <ti/drivers/cryptoutils/ecc/ECCParamsXXF3HSM.h>
Include dependency graph for ECCParams.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  ECCParams_CurveParams
 A structure containing the parameters of an elliptic curve. More...
 
union  ECC_NISTP256_Param
 Union to access ECC_NISTP256 curve params in bytes or words. More...
 
union  ECC_NISTP224_Param
 Union to access ECC_NISTP256 curve params in bytes or words. More...
 
union  ECC_Param
 Union to format inputs to ECC library. More...
 
union  ECC_Curve25519_Param
 Union to access ECC_Curve25519 curve params in bytes or words. More...
 

Macros

#define ECCParams_STATUS_SUCCESS   (0)
 Successful status code. More...
 
#define ECCParams_STATUS_ERROR   (-1)
 Generic error status code. More...
 
#define ECCParams_CURVE_TYPE_NONE   0U
 
#define ECCParams_CURVE_TYPE_SHORT_WEIERSTRASS_AN3   1U
 
#define ECCParams_CURVE_TYPE_SHORT_WEIERSTRASS_GEN   2U
 
#define ECCParams_CURVE_TYPE_MONTGOMERY   3U
 
#define ECCParams_CURVE_TYPE_EDWARDS   4U
 
#define ECC_LENGTH_PREFIX_BYTES   4
 Number of bytes for the length word prepended before all parameters passed into the ECC SW library functions. More...
 
#define ECCParams_NISTP256_LENGTH   32
 Length of NIST P256 curve parameters in bytes. More...
 
#define ECC_NISTP256_PARAM_LENGTH_WITH_PREFIX_BYTES   (ECCParams_NISTP256_LENGTH + ECC_LENGTH_PREFIX_BYTES)
 Length in bytes of NISTP256 curve parameters including the prepended length word. More...
 
#define ECCParams_NISTP224_LENGTH   28
 Length of NIST P224 curve parameters in bytes. More...
 
#define ECC_NISTP224_PARAM_LENGTH_WITH_PREFIX_BYTES   (ECCParams_NISTP224_LENGTH + ECC_LENGTH_PREFIX_BYTES)
 Length in bytes of NISTP256 curve parameters including the prepended length word. More...
 
#define OCTET_STRING_OFFSET   1
 
#define OCTET_STRING_PREFIX   0x04
 
#define ECC_LENGTH_OFFSET_BYTES   4
 
#define ECC_PARAM_LENGTH_WITH_OFFSET_BYTES   (ECCParams_NISTP256_LENGTH + ECC_LENGTH_OFFSET_BYTES)
 
#define ECCParams_CURVE25519_LENGTH   32
 Length of Curve25519 curve parameters in bytes. More...
 
#define ECC_CURVE25519_LENGTH_WITH_PREFIX_BYTES   (ECCParams_CURVE25519_LENGTH + ECC_LENGTH_PREFIX_BYTES)
 Length in bytes of Curve25519 curve parameters including the prepended length word. More...
 
#define ECCParams_FormatCurve25519PrivateKey   ECCParams_formatCurve25519PrivateKey
 

Typedefs

typedef uint32_t ECCParams_CurveType
 Enumeration of curve equations supported. More...
 
typedef struct ECCParams_CurveParams ECCParams_CurveParams
 A structure containing the parameters of an elliptic curve. More...
 

Enumerations

enum  ECCParams_SecureCurve {
  ECCParams_SecureCurve_NISTP224 = 0, ECCParams_SecureCurve_NISTP256, ECCParams_SecureCurve_NISTP384, ECCParams_SecureCurve_NISTP521,
  ECCParams_SecureCurve_BrainpoolP256R1, ECCParams_SecureCurve_BrainpoolP384R1, ECCParams_SecureCurve_BrainpoolP512R1, ECCParams_SecureCurve_Curve25519,
  ECCParams_SecureCurve_Ed25519, ECCParams_SecureCurve_Wei25519, ECCParams_SecureCurve_COUNT
}
 Enumeration of ECC curve names supported by TF-M. More...
 

Functions

int_fast16_t ECCParams_formatCurve25519PrivateKey (CryptoKey *myPrivateKey)
 Formats a CryptoKey to conform to Curve25519 private key requirements. More...
 
int_fast16_t ECCParams_getUncompressedGeneratorPoint (const ECCParams_CurveParams *curveParams, uint8_t *buffer, size_t length)
 Extracts the curve generator point from an ecliptic curve description. More...
 

Variables

const ECCParams_CurveParams ECCParams_NISTP192
 The NISTP192 curve in short Weierstrass form. More...
 
const ECCParams_CurveParams ECCParams_NISTP224
 The NISTP224 curve in short Weierstrass form. More...
 
const ECCParams_CurveParams ECCParams_NISTP256
 The NISTP256 curve in short Weierstrass form. More...
 
const ECCParams_CurveParams ECCParams_NISTP384
 The NISTP384 curve in short Weierstrass form. More...
 
const ECCParams_CurveParams ECCParams_NISTP521
 The NISTP521 curve in short Weierstrass form. More...
 
const ECCParams_CurveParams ECCParams_BrainpoolP256R1
 The BrainpoolP256R1 curve in short Weierstrass form. More...
 
const ECCParams_CurveParams ECCParams_BrainpoolP384R1
 The BrainpoolP384R1 curve in short Weierstrass form. More...
 
const ECCParams_CurveParams ECCParams_BrainpoolP512R1
 The BrainpoolP512R1 curve in short Weierstrass form. More...
 
const ECCParams_CurveParams ECCParams_Wei25519
 A short Weierstrass equivalent representation of Ed25519. More...
 
const ECCParams_CurveParams ECCParams_Curve25519
 The Curve25519 curve in Montgomery form. More...
 
const ECCParams_CurveParams ECCParams_Ed25519
 The Ed25519 curve in Edwards form. More...
 
const ECC_NISTP256_Param ECC_NISTP256_generatorX
 X coordinate of the generator point of the ECC_NISTP256 curve. More...
 
const ECC_NISTP256_Param ECC_NISTP256_generatorY
 Y coordinate of the generator point of the ECC_NISTP256 curve. More...
 
const ECC_NISTP256_Param ECC_NISTP256_prime
 Prime of the generator point of the ECC_NISTP256 curve. More...
 
const ECC_NISTP256_Param ECC_NISTP256_a
 'a' constant of the ECC_NISTP256 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b). More...
 
const ECC_NISTP256_Param ECC_NISTP256_b
 'b' constant of the ECC_NISTP256 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b). More...
 
const ECC_NISTP256_Param ECC_NISTP256_order
 Order of the generator point of the ECC_NISTP256 curve. More...
 
const ECC_NISTP256_Param ECC_NISTP256_k_mont
 'k' in Montgomery domain of the ECC_NISTP256 curve. More...
 
const ECC_NISTP256_Param ECC_NISTP256_a_mont
 'a' in Montgomery domain of the ECC_NISTP256 curve. More...
 
const ECC_NISTP256_Param ECC_NISTP256_b_mont
 'b' in Montgomery domain of the ECC_NISTP256 curve. More...
 
const ECC_NISTP224_Param ECC_NISTP224_generatorX
 X coordinate of the generator point of the ECC_NISTP224 curve. More...
 
const ECC_NISTP224_Param ECC_NISTP224_generatorY
 Y coordinate of the generator point of the ECC_NISTP224 curve. More...
 
const ECC_NISTP224_Param ECC_NISTP224_prime
 Prime of the generator point of the ECC_NISTP224 curve. More...
 
const ECC_NISTP224_Param ECC_NISTP224_a
 'a' constant of the ECC_NISTP224 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b). More...
 
const ECC_NISTP224_Param ECC_NISTP224_b
 'b' constant of the ECC_NISTP224 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b). More...
 
const ECC_NISTP224_Param ECC_NISTP224_order
 Order of the generator point of the ECC_NISTP224 curve. More...
 
const ECC_NISTP224_Param ECC_NISTP224_k_mont
 'k' in Montgomery domain of the ECC_NISTP224 curve. More...
 
const ECC_NISTP224_Param ECC_NISTP224_a_mont
 'a' in Montgomery domain of the ECC_NISTP224 curve. More...
 
const ECC_NISTP224_Param ECC_NISTP224_b_mont
 'b' in Montgomery domain of the ECC_NISTP224 curve. More...
 
const ECC_Curve25519_Param ECC_Curve25519_generatorX
 X coordinate of the generator point of the ECC_Curve25519 curve. More...
 
const ECC_Curve25519_Param ECC_Curve25519_generatorY
 Y coordinate of the generator point of the ECC_Curve25519 curve. More...
 
const ECC_Curve25519_Param ECC_Curve25519_prime
 Prime of the generator point of the ECC_Curve25519 curve. More...
 
const ECC_Curve25519_Param ECC_Curve25519_a
 'a' constant of the ECC_Curve25519 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b). More...
 
const ECC_Curve25519_Param ECC_Curve25519_b
 'b' constant of the ECC_Curve25519 curve when expressed in short Weierstrass form (y^2 = x^3 + a*x + b). More...
 
const ECC_Curve25519_Param ECC_Curve25519_order
 Order of the generator point of the ECC_Curve25519 curve. More...
 

Macro Definition Documentation

§ ECCParams_STATUS_SUCCESS

#define ECCParams_STATUS_SUCCESS   (0)

Successful status code.

Function return ECCParams_STATUS_SUCCESS if the control code was executed successfully.

§ ECCParams_STATUS_ERROR

#define ECCParams_STATUS_ERROR   (-1)

Generic error status code.

Functions return ECCParams_STATUS_ERROR if the control code was not executed successfully.

§ ECCParams_CURVE_TYPE_NONE

#define ECCParams_CURVE_TYPE_NONE   0U

§ ECCParams_CURVE_TYPE_SHORT_WEIERSTRASS_AN3

#define ECCParams_CURVE_TYPE_SHORT_WEIERSTRASS_AN3   1U

§ ECCParams_CURVE_TYPE_SHORT_WEIERSTRASS_GEN

#define ECCParams_CURVE_TYPE_SHORT_WEIERSTRASS_GEN   2U

§ ECCParams_CURVE_TYPE_MONTGOMERY

#define ECCParams_CURVE_TYPE_MONTGOMERY   3U

§ ECCParams_CURVE_TYPE_EDWARDS

#define ECCParams_CURVE_TYPE_EDWARDS   4U

§ ECC_LENGTH_PREFIX_BYTES

#define ECC_LENGTH_PREFIX_BYTES   4

Number of bytes for the length word prepended before all parameters passed into the ECC SW library functions.

§ OCTET_STRING_OFFSET

#define OCTET_STRING_OFFSET   1

§ OCTET_STRING_PREFIX

#define OCTET_STRING_PREFIX   0x04

§ ECC_LENGTH_OFFSET_BYTES

#define ECC_LENGTH_OFFSET_BYTES   4

§ ECC_PARAM_LENGTH_WITH_OFFSET_BYTES

#define ECC_PARAM_LENGTH_WITH_OFFSET_BYTES   (ECCParams_NISTP256_LENGTH + ECC_LENGTH_OFFSET_BYTES)

§ ECCParams_CURVE25519_LENGTH

#define ECCParams_CURVE25519_LENGTH   32

Length of Curve25519 curve parameters in bytes.

§ ECCParams_FormatCurve25519PrivateKey

#define ECCParams_FormatCurve25519PrivateKey   ECCParams_formatCurve25519PrivateKey

Typedef Documentation

§ ECCParams_CurveType

typedef uint32_t ECCParams_CurveType

Enumeration of curve equations supported.

Elliptic curves can be expressed using multiple equations of polynomials over finite fields. All forms can be converted to one another using parameter substitution. Each curve has a default curve equations it was designed to use.

Some curve implementations have restrictions on which algorithms and schemes they work with. For example, Curve25519 was explicitely designed with ECDH in mind. It only uses and yields the X coordinate of a point on the elliptic curve in common implementations. Some implementations do provide X and Y affine coordinates but most do not. Therefore, ECDSA and ECJPAKE do not have compatible implementations for Curve25519 on some devices as the Y coordinate is required by them.

Check the header files of each device-specific implementation for information regarding curve-support for specific schemes on a device.

Name Equation
Short Weierstrass y^2 = x^3 + a*x + b mod p
Montgomery By^2 = x^3 + Ax^2 + x mod p
Edwards x^2 + y^2 = 1 + dx^2y^2 mod p

§ ECCParams_CurveParams

A structure containing the parameters of an elliptic curve.

Elliptical Curve Cryptography (ECC) prime curve parameters.

Enumeration Type Documentation

§ ECCParams_SecureCurve

Enumeration of ECC curve names supported by TF-M.

Enumerator
ECCParams_SecureCurve_NISTP224 
ECCParams_SecureCurve_NISTP256 
ECCParams_SecureCurve_NISTP384 
ECCParams_SecureCurve_NISTP521 
ECCParams_SecureCurve_BrainpoolP256R1 
ECCParams_SecureCurve_BrainpoolP384R1 
ECCParams_SecureCurve_BrainpoolP512R1 
ECCParams_SecureCurve_Curve25519 
ECCParams_SecureCurve_Ed25519 
ECCParams_SecureCurve_Wei25519 
ECCParams_SecureCurve_COUNT 

Function Documentation

§ ECCParams_formatCurve25519PrivateKey()

int_fast16_t ECCParams_formatCurve25519PrivateKey ( CryptoKey myPrivateKey)

Formats a CryptoKey to conform to Curve25519 private key requirements.

Curve25519 has specific private key requirements specified by the curve definition. Specifically, the bottom three and the top bit may not be set and the second to last bit must be set.

Parameters
myPrivateKeyAn initialized CryptoKey describing the entropy for a Curve25519 private key. Platform-specific restrictions for the location of the keying material apply. Some implementations do not support modifying keying material in flash for example.
Precondition
Initialize the CryptoKey with a 32-byte buffer in a compliant location.

§ ECCParams_getUncompressedGeneratorPoint()

int_fast16_t ECCParams_getUncompressedGeneratorPoint ( const ECCParams_CurveParams curveParams,
uint8_t *  buffer,
size_t  length 
)

Extracts the curve generator point from an ecliptic curve description.

The curve parameters ECCParams_CurveParams::generatorX and ECCParams_CurveParams::generatorY are extracted from curveParams and written as a concatenated octet string in big endian order to buffer. The format is defined in SEC 1: Elliptic Curve Cryptography section 2.3.3.

The curve point has the format 0x04 || X || Y and the length is 2 * size_of_x_or_y + 1 where 0x04 specifies octet string format. If the buffer length exceeds the curve point length, the remaining buffer space is zeroed.

Parameters
curveParamsPoints to the input curve parameters
bufferPoints to the destination where the generator point will be written to. Make sure that buffer is large enough to hold
lengthMaximum length of buffer in bytes.
Return values
ECCParams_STATUS_SUCCESSon success, ECCParams_STATUS_ERROR if the provided buffer length is insufficient to hold the curve point.

Variable Documentation

§ ECCParams_NISTP192

const ECCParams_CurveParams ECCParams_NISTP192

The NISTP192 curve in short Weierstrass form.

§ ECCParams_NISTP224

const ECCParams_CurveParams ECCParams_NISTP224

The NISTP224 curve in short Weierstrass form.

§ ECCParams_NISTP256

const ECCParams_CurveParams ECCParams_NISTP256

The NISTP256 curve in short Weierstrass form.

§ ECCParams_NISTP384

const ECCParams_CurveParams ECCParams_NISTP384

The NISTP384 curve in short Weierstrass form.

§ ECCParams_NISTP521

const ECCParams_CurveParams ECCParams_NISTP521

The NISTP521 curve in short Weierstrass form.

§ ECCParams_BrainpoolP256R1

const ECCParams_CurveParams ECCParams_BrainpoolP256R1

The BrainpoolP256R1 curve in short Weierstrass form.

§ ECCParams_BrainpoolP384R1

const ECCParams_CurveParams ECCParams_BrainpoolP384R1

The BrainpoolP384R1 curve in short Weierstrass form.

§ ECCParams_BrainpoolP512R1

const ECCParams_CurveParams ECCParams_BrainpoolP512R1

The BrainpoolP512R1 curve in short Weierstrass form.

§ ECCParams_Wei25519

const ECCParams_CurveParams ECCParams_Wei25519

A short Weierstrass equivalent representation of Ed25519.

§ ECCParams_Curve25519

const ECCParams_CurveParams ECCParams_Curve25519

The Curve25519 curve in Montgomery form.

§ ECCParams_Ed25519

const ECCParams_CurveParams ECCParams_Ed25519

The Ed25519 curve in Edwards form.

© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale