#include <crypto_struct.h>
§ id
| unsigned int psa_hash_operation_s::id |
Unique ID indicating which driver got assigned to do the operation. Since driver contexts are driver-specific, swapping drivers halfway through the operation is not supported. ID values are auto-generated in psa_driver_wrappers.h. ID value zero means the context is not valid or not assigned to any driver (i.e. the driver context is not active, in use).
§ alg
The documentation for this struct was generated from the following file: