Macros | Typedefs
Key derivation

Macros

#define PSA_KEY_DERIVATION_INPUT_SECRET   ((psa_key_derivation_step_t) 0x0101)
 
#define PSA_KEY_DERIVATION_INPUT_PASSWORD   ((psa_key_derivation_step_t) 0x0102)
 
#define PSA_KEY_DERIVATION_INPUT_OTHER_SECRET   ((psa_key_derivation_step_t) 0x0103)
 
#define PSA_KEY_DERIVATION_INPUT_LABEL   ((psa_key_derivation_step_t) 0x0201)
 
#define PSA_KEY_DERIVATION_INPUT_SALT   ((psa_key_derivation_step_t) 0x0202)
 
#define PSA_KEY_DERIVATION_INPUT_INFO   ((psa_key_derivation_step_t) 0x0203)
 
#define PSA_KEY_DERIVATION_INPUT_SEED   ((psa_key_derivation_step_t) 0x0204)
 
#define PSA_KEY_DERIVATION_INPUT_COST   ((psa_key_derivation_step_t) 0x0205)
 
#define PSA_KEY_DERIVATION_INPUT_CONTEXT   ((psa_key_derivation_step_t)0x0206U)
 

Typedefs

typedef uint16_t psa_key_derivation_step_t
 Encoding of the step of a key derivation. More...
 

Detailed Description

Macro Definition Documentation

§ PSA_KEY_DERIVATION_INPUT_SECRET

#define PSA_KEY_DERIVATION_INPUT_SECRET   ((psa_key_derivation_step_t) 0x0101)

A secret input for key derivation.

This should be a key of type PSA_KEY_TYPE_DERIVE (passed to psa_key_derivation_input_key()) or the shared secret resulting from a key agreement (obtained via psa_key_derivation_key_agreement()).

The secret can also be a direct input (passed to key_derivation_input_bytes()). In this case, the derivation operation may not be used to derive keys: the operation will only allow psa_key_derivation_output_bytes(), psa_key_derivation_verify_bytes(), or psa_key_derivation_verify_key(), but not psa_key_derivation_output_key().

§ PSA_KEY_DERIVATION_INPUT_PASSWORD

#define PSA_KEY_DERIVATION_INPUT_PASSWORD   ((psa_key_derivation_step_t) 0x0102)

A low-entropy secret input for password hashing / key stretching.

This is usually a key of type PSA_KEY_TYPE_PASSWORD (passed to psa_key_derivation_input_key()) or a direct input (passed to psa_key_derivation_input_bytes()) that is a password or passphrase. It can also be high-entropy secret such as a key of type PSA_KEY_TYPE_DERIVE or the shared secret resulting from a key agreement.

The secret can also be a direct input (passed to key_derivation_input_bytes()). In this case, the derivation operation may not be used to derive keys: the operation will only allow psa_key_derivation_output_bytes(), psa_key_derivation_verify_bytes(), or psa_key_derivation_verify_key(), but not psa_key_derivation_output_key().

§ PSA_KEY_DERIVATION_INPUT_OTHER_SECRET

#define PSA_KEY_DERIVATION_INPUT_OTHER_SECRET   ((psa_key_derivation_step_t) 0x0103)

A high-entropy additional secret input for key derivation.

This is typically the shared secret resulting from a key agreement obtained via psa_key_derivation_key_agreement(). It may alternatively be a key of type PSA_KEY_TYPE_DERIVE passed to psa_key_derivation_input_key(), or a direct input passed to psa_key_derivation_input_bytes().

§ PSA_KEY_DERIVATION_INPUT_LABEL

#define PSA_KEY_DERIVATION_INPUT_LABEL   ((psa_key_derivation_step_t) 0x0201)

A label for key derivation.

This should be a direct input. It can also be a key of type PSA_KEY_TYPE_RAW_DATA.

§ PSA_KEY_DERIVATION_INPUT_SALT

#define PSA_KEY_DERIVATION_INPUT_SALT   ((psa_key_derivation_step_t) 0x0202)

A salt for key derivation.

This should be a direct input. It can also be a key of type PSA_KEY_TYPE_RAW_DATA or PSA_KEY_TYPE_PEPPER.

§ PSA_KEY_DERIVATION_INPUT_INFO

#define PSA_KEY_DERIVATION_INPUT_INFO   ((psa_key_derivation_step_t) 0x0203)

An information string for key derivation.

This should be a direct input. It can also be a key of type PSA_KEY_TYPE_RAW_DATA.

§ PSA_KEY_DERIVATION_INPUT_SEED

#define PSA_KEY_DERIVATION_INPUT_SEED   ((psa_key_derivation_step_t) 0x0204)

A seed for key derivation.

This should be a direct input. It can also be a key of type PSA_KEY_TYPE_RAW_DATA.

§ PSA_KEY_DERIVATION_INPUT_COST

#define PSA_KEY_DERIVATION_INPUT_COST   ((psa_key_derivation_step_t) 0x0205)

A cost parameter for password hashing / key stretching.

This must be a direct input, passed to psa_key_derivation_input_integer().

§ PSA_KEY_DERIVATION_INPUT_CONTEXT

#define PSA_KEY_DERIVATION_INPUT_CONTEXT   ((psa_key_derivation_step_t)0x0206U)

A context for key derivation.

This is typically a direct input. It is currently unsupported to use it as a key of type PSA_KEY_TYPE_RAW_DATA.

Typedef Documentation

§ psa_key_derivation_step_t

typedef uint16_t psa_key_derivation_step_t

Encoding of the step of a key derivation.

Values of this type are generally constructed by macros called PSA_KEY_DERIVATION_INPUT_xxx.

© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale