Macros | Typedefs | Functions
Key attributes

Macros

#define PSA_KEY_ATTRIBUTES_INIT
 

Typedefs

typedef psa_key_attributes_t KeyStore_PSA_KeyAttributes
 
typedef psa_key_id_t KeyStore_PSA_keyID
 
typedef mbedtls_svc_key_id_t KeyStore_PSA_KeyFileId
 
typedef struct psa_key_attributes_s psa_key_attributes_t
 

Functions

static psa_key_attributes_t psa_key_attributes_init (void)
 
static void psa_set_key_id (psa_key_attributes_t *attributes, psa_key_id_t key)
 
static void mbedtls_set_key_owner_id (psa_key_attributes_t *attributes, mbedtls_key_owner_id_t owner)
 
static void psa_set_key_lifetime (psa_key_attributes_t *attributes, psa_key_lifetime_t lifetime)
 
static psa_key_id_t psa_get_key_id (const psa_key_attributes_t *attributes)
 
static psa_key_lifetime_t psa_get_key_lifetime (const psa_key_attributes_t *attributes)
 
static void psa_set_key_usage_flags (psa_key_attributes_t *attributes, psa_key_usage_t usage_flags)
 
static psa_key_usage_t psa_get_key_usage_flags (const psa_key_attributes_t *attributes)
 
static void psa_set_key_algorithm (psa_key_attributes_t *attributes, psa_algorithm_t alg)
 
static psa_algorithm_t psa_get_key_algorithm (const psa_key_attributes_t *attributes)
 
static void psa_set_key_type (psa_key_attributes_t *attributes, psa_key_type_t type)
 
static void psa_set_key_bits (psa_key_attributes_t *attributes, size_t bits)
 
static psa_key_type_t psa_get_key_type (const psa_key_attributes_t *attributes)
 
static size_t psa_get_key_bits (const psa_key_attributes_t *attributes)
 
psa_status_t psa_get_key_attributes (psa_key_id_t key, psa_key_attributes_t *attributes)
 
void psa_reset_key_attributes (psa_key_attributes_t *attributes)
 

Detailed Description

Macro Definition Documentation

§ PSA_KEY_ATTRIBUTES_INIT

#define PSA_KEY_ATTRIBUTES_INIT
Value:
{ \
0 \
}
struct psa_key_attributes_s psa_key_attributes_t
Definition: crypto_types.h:493

This macro returns a suitable initializer for a key attribute structure of type psa_key_attributes_t.

Referenced by psa_key_attributes_init().

Typedef Documentation

§ psa_key_attributes_t

The type of a structure containing key attributes.

This is an opaque structure that can represent the metadata of a key object. Metadata that can be stored in attributes includes:

  • The location of the key in storage, indicated by its key identifier and its lifetime.
  • The key's policy, comprising usage flags and a specification of the permitted algorithm(s).
  • Information about the key itself: the key type and its size.
  • Additional implementation-defined attributes.

The actual key material is not considered an attribute of a key. Key attributes do not contain information that is generally considered highly confidential.

An attribute structure works like a simple data structure where each function psa_set_key_xxx sets a field and the corresponding function psa_get_key_xxx retrieves the value of the corresponding field. However, a future version of the library may report values that are equivalent to the original one, but have a different encoding. Invalid values may be mapped to different, also invalid values.

An attribute structure may contain references to auxiliary resources, for example pointers to allocated memory or indirect references to pre-calculated values. In order to free such resources, the application must call psa_reset_key_attributes(). As an exception, calling psa_reset_key_attributes() on an attribute structure is optional if the structure has only been modified by the following functions since it was initialized or last reset with psa_reset_key_attributes():

Before calling any function on a key attribute structure, the application must initialize it by any of the following means:

A freshly initialized attribute structure contains the following values:

  • lifetime: PSA_KEY_LIFETIME_VOLATILE.
  • key identifier: 0 (which is not a valid key identifier).
  • type: 0 (meaning that the type is unspecified).
  • key size: 0 (meaning that the size is unspecified).
  • usage flags: 0 (which allows no usage except exporting a public key).
  • algorithm: 0 (which allows no cryptographic usage, but allows exporting).

A typical sequence to create a key is as follows:

  1. Create and initialize an attribute structure.
  2. If the key is persistent, call psa_set_key_id(). Also call psa_set_key_lifetime() to place the key in a non-default location.
  3. Set the key policy with psa_set_key_usage_flags() and psa_set_key_algorithm().
  4. Set the key type with psa_set_key_type(). Skip this step if copying an existing key with psa_copy_key().
  5. When generating a random key with psa_generate_key() or deriving a key with psa_key_derivation_output_key(), set the desired key size with psa_set_key_bits().
  6. Call a key creation function: psa_import_key(), psa_generate_key(), psa_key_derivation_output_key() or psa_copy_key(). This function reads the attribute structure, creates a key with these attributes, and outputs a key identifier to the newly created key.
  7. The attribute structure is now no longer necessary. You may call psa_reset_key_attributes(), although this is optional with the workflow presented here because the attributes currently defined in this specification do not require any additional resources beyond the structure itself.

A typical sequence to query a key's attributes is as follows:

  1. Call psa_get_key_attributes().
  2. Call psa_get_key_xxx functions to retrieve the attribute(s) that you are interested in.
  3. Call psa_reset_key_attributes() to free any resources that may be used by the attribute structure.

Once a key has been created, it is impossible to change its attributes.

Function Documentation

§ psa_key_attributes_init()

static psa_key_attributes_t psa_key_attributes_init ( void  )
static

Return an initial value for a key attributes structure.

§ psa_set_key_id()

static void psa_set_key_id ( psa_key_attributes_t attributes,
psa_key_id_t  key 
)
static

Declare a key as persistent and set its key identifier.

If the attribute structure currently declares the key as volatile (which is the default content of an attribute structure), this function sets the lifetime attribute to PSA_KEY_LIFETIME_PERSISTENT.

This function does not access storage, it merely stores the given value in the structure. The persistent key will be written to storage when the attribute structure is passed to a key creation function such as psa_import_key(), psa_generate_key(), psa_key_derivation_output_key() or psa_copy_key().

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate each of its arguments exactly once.

Parameters
[out]attributesThe attribute structure to write to.
keyThe persistent identifier for the key.

§ mbedtls_set_key_owner_id()

static void mbedtls_set_key_owner_id ( psa_key_attributes_t attributes,
mbedtls_key_owner_id_t  owner 
)
static

Set the owner identifier of a key.

When key identifiers encode key owner identifiers, psa_set_key_id() does not allow to define in key attributes the owner of volatile keys as psa_set_key_id() enforces the key to be persistent.

This function allows to set in key attributes the owner identifier of a key. It is intended to be used for volatile keys. For persistent keys, it is recommended to use the PSA Cryptography API psa_set_key_id() to define the owner of a key.

Parameters
[out]attributesThe attribute structure to write to.
ownerThe key owner identifier.

§ psa_set_key_lifetime()

static void psa_set_key_lifetime ( psa_key_attributes_t attributes,
psa_key_lifetime_t  lifetime 
)
static

Set the location of a persistent key.

To make a key persistent, you must give it a persistent key identifier with psa_set_key_id(). By default, a key that has a persistent identifier is stored in the default storage area identifier by PSA_KEY_LIFETIME_PERSISTENT. Call this function to choose a storage area, or to explicitly declare the key as volatile.

This function does not access storage, it merely stores the given value in the structure. The persistent key will be written to storage when the attribute structure is passed to a key creation function such as psa_import_key(), psa_generate_key(), psa_key_derivation_output_key() or psa_copy_key().

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate each of its arguments exactly once.

Parameters
[out]attributesThe attribute structure to write to.
lifetimeThe lifetime for the key. If this is PSA_KEY_LIFETIME_VOLATILE, the key will be volatile, and the key identifier attribute is reset to 0.

§ psa_get_key_id()

static psa_key_id_t psa_get_key_id ( const psa_key_attributes_t attributes)
static

Retrieve the key identifier from key attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate its argument exactly once.

Parameters
[in]attributesThe key attribute structure to query.
Returns
The persistent identifier stored in the attribute structure. This value is unspecified if the attribute structure declares the key as volatile.

§ psa_get_key_lifetime()

static psa_key_lifetime_t psa_get_key_lifetime ( const psa_key_attributes_t attributes)
static

Retrieve the lifetime from key attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate its argument exactly once.

Parameters
[in]attributesThe key attribute structure to query.
Returns
The lifetime value stored in the attribute structure.

§ psa_set_key_usage_flags()

static void psa_set_key_usage_flags ( psa_key_attributes_t attributes,
psa_key_usage_t  usage_flags 
)
static

Declare usage flags for a key.

Usage flags are part of a key's usage policy. They encode what kind of operations are permitted on the key. For more details, refer to the documentation of the type psa_key_usage_t.

This function overwrites any usage flags previously set in attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate each of its arguments exactly once.

Parameters
[out]attributesThe attribute structure to write to.
usage_flagsThe usage flags to write.

§ psa_get_key_usage_flags()

static psa_key_usage_t psa_get_key_usage_flags ( const psa_key_attributes_t attributes)
static

Retrieve the usage flags from key attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate its argument exactly once.

Parameters
[in]attributesThe key attribute structure to query.
Returns
The usage flags stored in the attribute structure.

§ psa_set_key_algorithm()

static void psa_set_key_algorithm ( psa_key_attributes_t attributes,
psa_algorithm_t  alg 
)
static

Declare the permitted algorithm policy for a key.

The permitted algorithm policy of a key encodes which algorithm or algorithms are permitted to be used with this key. The following algorithm policies are supported:

  • 0 does not allow any cryptographic operation with the key. The key may be used for non-cryptographic actions such as exporting (if permitted by the usage flags).
  • An algorithm value permits this particular algorithm.
  • An algorithm wildcard built from PSA_ALG_ANY_HASH allows the specified signature scheme with any hash algorithm.
  • An algorithm built from PSA_ALG_AT_LEAST_THIS_LENGTH_MAC allows any MAC algorithm from the same base class (e.g. CMAC) which generates/verifies a MAC length greater than or equal to the length encoded in the wildcard algorithm.
  • An algorithm built from PSA_ALG_AEAD_WITH_AT_LEAST_THIS_LENGTH_TAG allows any AEAD algorithm from the same base class (e.g. CCM) which generates/verifies a tag length greater than or equal to the length encoded in the wildcard algorithm.

This function overwrites any algorithm policy previously set in attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate each of its arguments exactly once.

Parameters
[out]attributesThe attribute structure to write to.
algThe permitted algorithm policy to write.

§ psa_get_key_algorithm()

static psa_algorithm_t psa_get_key_algorithm ( const psa_key_attributes_t attributes)
static

Retrieve the algorithm policy from key attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate its argument exactly once.

Parameters
[in]attributesThe key attribute structure to query.
Returns
The algorithm stored in the attribute structure.

§ psa_set_key_type()

static void psa_set_key_type ( psa_key_attributes_t attributes,
psa_key_type_t  type 
)
static

Declare the type of a key.

This function overwrites any key type previously set in attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate each of its arguments exactly once.

Parameters
[out]attributesThe attribute structure to write to.
typeThe key type to write. If this is 0, the key type in attributes becomes unspecified.

§ psa_set_key_bits()

static void psa_set_key_bits ( psa_key_attributes_t attributes,
size_t  bits 
)
static

Declare the size of a key.

This function overwrites any key size previously set in attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate each of its arguments exactly once.

Parameters
[out]attributesThe attribute structure to write to.
bitsThe key size in bits. If this is 0, the key size in attributes becomes unspecified. Keys of size 0 are not supported.

§ psa_get_key_type()

static psa_key_type_t psa_get_key_type ( const psa_key_attributes_t attributes)
static

Retrieve the key type from key attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate its argument exactly once.

Parameters
[in]attributesThe key attribute structure to query.
Returns
The key type stored in the attribute structure.

§ psa_get_key_bits()

static size_t psa_get_key_bits ( const psa_key_attributes_t attributes)
static

Retrieve the key size from key attributes.

This function may be declared as static (i.e. without external linkage). This function may be provided as a function-like macro, but in this case it must evaluate its argument exactly once.

Parameters
[in]attributesThe key attribute structure to query.
Returns
The key size stored in the attribute structure, in bits.

§ psa_get_key_attributes()

psa_status_t psa_get_key_attributes ( psa_key_id_t  key,
psa_key_attributes_t attributes 
)

Retrieve the attributes of a key.

This function first resets the attribute structure as with psa_reset_key_attributes(). It then copies the attributes of the given key into the given attribute structure.

Note
This function may allocate memory or other resources. Once you have called this function on an attribute structure, you must call psa_reset_key_attributes() to free these resources.
Parameters
[in]keyIdentifier of the key to query.
[in,out]attributesOn success, the attributes of the key. On failure, equivalent to a freshly-initialized structure.
Return values
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_DATA_CORRUPT
PSA_ERROR_DATA_INVALID
PSA_ERROR_BAD_STATEThe library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.

§ psa_reset_key_attributes()

void psa_reset_key_attributes ( psa_key_attributes_t attributes)

Reset a key attribute structure to a freshly initialized state.

You must initialize the attribute structure as described in the documentation of the type psa_key_attributes_t before calling this function. Once the structure has been initialized, you may call this function at any time.

This function frees any auxiliary resources that the structure may contain.

Parameters
[in,out]attributesThe attribute structure to reset.
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale