![]() |
![]() |
PSA cryptography module: type aliases.
This file contains portable definitions of integral types for properties of cryptographic keys, designations of cryptographic algorithms, and error codes returned by the library.
This header file does not declare any function.
#include <stdint.h>

Go to the source code of this file.
Data Structures | |
| struct | mbedtls_svc_key_id_t |
Macros | |
| #define | MBEDTLS_PSA_CRYPTO_KEY_ID_ENCODES_OWNER |
Typedefs | |
| typedef int32_t | psa_status_t |
| Function return status. More... | |
| typedef uint16_t | psa_key_type_t |
| Encoding of a key type. More... | |
| typedef uint8_t | psa_ecc_family_t |
| typedef uint8_t | psa_dh_family_t |
| typedef uint32_t | psa_algorithm_t |
| Encoding of a cryptographic algorithm. More... | |
| typedef uint32_t | psa_key_lifetime_t |
| typedef uint8_t | psa_key_persistence_t |
| typedef uint32_t | psa_key_location_t |
| typedef uint32_t | psa_key_id_t |
| typedef int32_t | mbedtls_key_owner_id_t |
| typedef uint32_t | psa_key_usage_t |
| Encoding of permitted usage on a key. More... | |
| typedef struct psa_key_attributes_s | psa_key_attributes_t |
| typedef uint16_t | psa_key_derivation_step_t |
| Encoding of the step of a key derivation. More... | |
Functions | |
| static int | mbedtls_key_owner_id_equal (mbedtls_key_owner_id_t id1, mbedtls_key_owner_id_t id2) |
| #define MBEDTLS_PSA_CRYPTO_KEY_ID_ENCODES_OWNER |