SimpleLinkGraphicsLibrary  5.00.00.05
Data Fields
Graphics_ImageButton Struct Reference

This structure defines the characteristics of a ImageButton. More...

#include <imageButton.h>

Collaboration diagram for Graphics_ImageButton:
Collaboration graph
[legend]

Data Fields

uint16_t xPosition
 
uint16_t yPosition
 
uint8_t borderWidth
 
bool selected
 
uint16_t imageHeight
 
uint16_t imageWidth
 
uint32_t borderColor
 
uint32_t selectedColor
 
Graphics_Imageimage
 

Detailed Description

This structure defines the characteristics of a ImageButton.

Field Documentation

§ xPosition

uint16_t Graphics_ImageButton::xPosition

§ yPosition

uint16_t Graphics_ImageButton::yPosition

§ borderWidth

uint8_t Graphics_ImageButton::borderWidth

§ selected

bool Graphics_ImageButton::selected

draws button with selected colors enabled

§ imageHeight

uint16_t Graphics_ImageButton::imageHeight

§ imageWidth

uint16_t Graphics_ImageButton::imageWidth

§ borderColor

uint32_t Graphics_ImageButton::borderColor

Border color, border is drawn if borderWidth >0

§ selectedColor

uint32_t Graphics_ImageButton::selectedColor

Background button color when selected

§ image

Graphics_Image* Graphics_ImageButton::image

Pointer to the image


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale