SimpleLinkGraphicsLibrary  5.00.00.05
Data Fields
Graphics_Display_Functions Struct Reference

This structure defines the implementation of a display driver. More...

#include <grlib.h>

Data Fields

void(*const pfnPixelDraw )(const Graphics_Display *pDisplay, int16_t lX, int16_t lY, uint16_t ulValue)
 A pointer to the function to draw a pixel on this display. More...
 
void(*const pfnPixelDrawMultiple )(const Graphics_Display *pDisplay, int16_t lX, int16_t lY, int16_t lX0, int16_t lCount, int16_t lBPP, const uint8_t *pucData, const uint32_t *pucPalette)
 A pointer to the function to draw multiple pixels on this display. More...
 
void(*const pfnLineDrawH )(const Graphics_Display *pDisplay, int16_t lX1, int16_t lX2, int16_t lY, uint16_t ulValue)
 A pointer to the function to draw a horizontal line on this display. More...
 
void(*const pfnLineDrawV )(const Graphics_Display *pDisplay, int16_t lX, int16_t lY1, int16_t lY2, uint16_t ulValue)
 A pointer to the function to draw a vertical line on this display. More...
 
void(*const pfnRectFill )(const Graphics_Display *pDisplay, const Graphics_Rectangle *pRect, uint16_t ulValue)
 A pointer to the function to draw a filled rectangle on this display. More...
 
uint32_t(*const pfnColorTranslate )(const Graphics_Display *pDisplay, uint32_t ulValue)
 
void(*const pfnFlush )(const Graphics_Display *pDisplay)
 
void(*const pfnClearDisplay )(const Graphics_Display *pDisplay, uint16_t ulValue)
 

Detailed Description

This structure defines the implementation of a display driver.

Field Documentation

§ pfnPixelDraw

void(*const Graphics_Display_Functions::pfnPixelDraw) (const Graphics_Display *pDisplay, int16_t lX, int16_t lY, uint16_t ulValue)

A pointer to the function to draw a pixel on this display.

Referenced by Graphics_drawPixelOnDisplay().

§ pfnPixelDrawMultiple

void(*const Graphics_Display_Functions::pfnPixelDrawMultiple) (const Graphics_Display *pDisplay, int16_t lX, int16_t lY, int16_t lX0, int16_t lCount, int16_t lBPP, const uint8_t *pucData, const uint32_t *pucPalette)

A pointer to the function to draw multiple pixels on this display.

Referenced by Graphics_drawMultiplePixelsOnDisplay().

§ pfnLineDrawH

void(*const Graphics_Display_Functions::pfnLineDrawH) (const Graphics_Display *pDisplay, int16_t lX1, int16_t lX2, int16_t lY, uint16_t ulValue)

A pointer to the function to draw a horizontal line on this display.

Referenced by Graphics_drawHorizontalLineOnDisplay().

§ pfnLineDrawV

void(*const Graphics_Display_Functions::pfnLineDrawV) (const Graphics_Display *pDisplay, int16_t lX, int16_t lY1, int16_t lY2, uint16_t ulValue)

A pointer to the function to draw a vertical line on this display.

Referenced by Graphics_drawVerticalLineOnDisplay().

§ pfnRectFill

void(*const Graphics_Display_Functions::pfnRectFill) (const Graphics_Display *pDisplay, const Graphics_Rectangle *pRect, uint16_t ulValue)

A pointer to the function to draw a filled rectangle on this display.

Referenced by Graphics_fillRectangleOnDisplay().

§ pfnColorTranslate

uint32_t(*const Graphics_Display_Functions::pfnColorTranslate) (const Graphics_Display *pDisplay, uint32_t ulValue)

A pointer to the function to translate 24-bit RGB colors to display-specific colors.

Referenced by Graphics_translateColorOnDisplay().

§ pfnFlush

void(*const Graphics_Display_Functions::pfnFlush) (const Graphics_Display *pDisplay)

A pointer to the function to flush any cached drawing operations on this display.

Referenced by Graphics_flushOnDisplay().

§ pfnClearDisplay

void(*const Graphics_Display_Functions::pfnClearDisplay) (const Graphics_Display *pDisplay, uint16_t ulValue)

A pointer to the function to clears Display. Contents of display buffer unmodified

Referenced by Graphics_clearDisplayOnDisplay().


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale