![]() |
![]() |
|
SimpleLinkGraphicsLibrary
5.00.00.05
|
Functions | |
| void | Graphics_drawRadioButton (const Graphics_Context *context, const Graphics_RadioButton *radioButton) |
| bool | Graphics_isRadioButtonSelected (const Graphics_RadioButton *radioButton, uint16_t x, uint16_t y) |
| void | Graphics_drawSelectedRadioButton (const Graphics_Context *context, const Graphics_RadioButton *radioButton) |
| void | Graphics_drawReleasedRadioButton (const Graphics_Context *context, const Graphics_RadioButton *radioButton) |
| void Graphics_drawRadioButton | ( | const Graphics_Context * | context, |
| const Graphics_RadioButton * | radioButton | ||
| ) |
Draws a RadioButton.
| context | is a pointer to the drawing context to use. |
| radioButton | is a pointer to the structure containing the extents of the RadioButton. |
This function draws a RadioButton . The RadioButton will contain the image passed in the RadioButton struct.
References AUTO_STRING_LENGTH, Graphics_RadioButton::font, Graphics_Context::font, Graphics_Context::foreground, g_sContext, Graphics_RadioButton::gap, Graphics_drawCircle(), Graphics_drawString(), Graphics_fillCircle(), Graphics_setFont(), Graphics_setForegroundColor(), Graphics_RadioButton::selected, Graphics_RadioButton::selectedColor, Graphics_RadioButton::text, Graphics_RadioButton::textColor, TRANSPARENT_TEXT, Graphics_RadioButton::xPosition, and Graphics_RadioButton::yPosition.
| bool Graphics_isRadioButtonSelected | ( | const Graphics_RadioButton * | radioButton, |
| uint16_t | x, | ||
| uint16_t | y | ||
| ) |
Determines if x and y coordinates are contained in RadioButton.
| radioButton | is a pointer to the structure containing the extents of the RadioButton. |
| x | x-coordinate to be determined if is inside RadioButton |
| y | y-coordinate to be determined if is inside RadioButton |
This function determines if x and y coordinates are contains inside RadioButton.
References Graphics_RadioButton::font, Graphics_RadioButton::gap, Graphics_RadioButton::numbOfChar, Graphics_RadioButton::xPosition, and Graphics_RadioButton::yPosition.
| void Graphics_drawSelectedRadioButton | ( | const Graphics_Context * | context, |
| const Graphics_RadioButton * | radioButton | ||
| ) |
Draws a selected RadioButton.
| context | is a pointer to the drawing context to use. |
| radioButton | is a pointer to the structure containing the extents of the RadioButton. |
This function draws a RadioButton using the selected parameters.
References Graphics_RadioButton::font, Graphics_Context::font, Graphics_Context::foreground, g_sContext, Graphics_fillCircle(), Graphics_setFont(), Graphics_setForegroundColor(), Graphics_RadioButton::selectedColor, Graphics_RadioButton::xPosition, and Graphics_RadioButton::yPosition.
| void Graphics_drawReleasedRadioButton | ( | const Graphics_Context * | context, |
| const Graphics_RadioButton * | radioButton | ||
| ) |
Draws a released RadioButton.
| context | is a pointer to the drawing context to use. |
| radioButton | is a pointer to the structure containing the extents of the RadioButton. |
This function draws a RadioButton using the released parameters.
References Graphics_RadioButton::font, Graphics_Context::foreground, g_sContext, Graphics_fillCircle(), Graphics_setForegroundColor(), Graphics_RadioButton::notSelectedColor, Graphics_RadioButton::xPosition, and Graphics_RadioButton::yPosition.