SimpleLinkGraphicsLibrary  5.00.00.05
Functions
ImageButton_api

Functions

void Graphics_drawImageButton (const Graphics_Context *context, const Graphics_ImageButton *imageButton)
 
bool Graphics_isImageButtonSelected (const Graphics_ImageButton *imageButton, uint16_t x, uint16_t y)
 
void Graphics_drawSelectedImageButton (const Graphics_Context *context, const Graphics_ImageButton *imageButton)
 
void Graphics_drawReleasedImageButton (const Graphics_Context *context, const Graphics_ImageButton *imageButton)
 

Detailed Description

Function Documentation

§ Graphics_drawImageButton()

void Graphics_drawImageButton ( const Graphics_Context context,
const Graphics_ImageButton imageButton 
)

Draws a ImageButton .

Parameters
contextis a pointer to the drawing context to use.
imageButtonis a pointer to the structure containing the extents of the ImageButton .

This function draws a ImageButton . The ImageButton will contain the image passed in the ImageButton struct.

Returns
None.

References Graphics_ImageButton::borderWidth, Graphics_Context::font, Graphics_Context::foreground, g_sContext, Graphics_drawImage(), Graphics_fillRectangle(), Graphics_setFont(), Graphics_setForegroundColor(), Graphics_ImageButton::imageHeight, Graphics_ImageButton::imageWidth, Graphics_ImageButton::xPosition, and Graphics_ImageButton::yPosition.

§ Graphics_isImageButtonSelected()

bool Graphics_isImageButtonSelected ( const Graphics_ImageButton imageButton,
uint16_t  x,
uint16_t  y 
)

Determines if x and y coordinates are contained in ImageButton .

Parameters
imageButtonis a pointer to the structure containing the extents of the ImageButton .
xx-coordinate to be determined if is inside ImageButton
yy-coordinate to be determined if is inside ImageButton

This function determines if x and y coordinates are contains inside ImageButton

Returns
true if x and y coordinates are inside ImageButton, false if not

References Graphics_ImageButton::borderWidth, Graphics_ImageButton::imageHeight, Graphics_ImageButton::imageWidth, Graphics_ImageButton::xPosition, and Graphics_ImageButton::yPosition.

§ Graphics_drawSelectedImageButton()

void Graphics_drawSelectedImageButton ( const Graphics_Context context,
const Graphics_ImageButton imageButton 
)

Draws a selected ImageButton .

Parameters
contextis a pointer to the drawing context to use.
imageButtonis a pointer to the structure containing the extents of the ImageButton .

This function draws a ImageButton using the selected parameters.

Returns
None.

References Graphics_ImageButton::borderWidth, Graphics_Context::font, Graphics_Context::foreground, g_sContext, Graphics_drawImage(), Graphics_fillRectangle(), Graphics_setFont(), Graphics_setForegroundColor(), Graphics_ImageButton::imageHeight, Graphics_ImageButton::imageWidth, Graphics_ImageButton::xPosition, and Graphics_ImageButton::yPosition.

§ Graphics_drawReleasedImageButton()

void Graphics_drawReleasedImageButton ( const Graphics_Context context,
const Graphics_ImageButton imageButton 
)

Draws a released ImageButton .

Parameters
contextis a pointer to the drawing context to use.
imageButtonis a pointer to the structure containing the extents of the ImageButton .

This function draws a ImageButton using the released parameters.

Returns
None.

References Graphics_ImageButton::borderWidth, Graphics_Context::font, Graphics_Context::foreground, g_sContext, Graphics_drawImage(), Graphics_fillRectangle(), Graphics_setFont(), Graphics_setForegroundColor(), Graphics_ImageButton::imageHeight, Graphics_ImageButton::imageWidth, Graphics_ImageButton::xPosition, and Graphics_ImageButton::yPosition.

© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale