Data Fields
XMEMWFF3_HWAttrs Struct Reference

Hardware attributes structure for the XMEMWFF3 driver. More...

#include <XMEMWFF3.h>

Collaboration diagram for XMEMWFF3_HWAttrs:
Collaboration graph
[legend]

Data Fields

FlashType flashType
 

Detailed Description

Hardware attributes structure for the XMEMWFF3 driver.

Contains hardware-specific configuration for the XMEMWFF3 driver that doesn't change during runtime.

Field Documentation

§ flashType

FlashType XMEMWFF3_HWAttrs::flashType

Configuration for the specific flash memory hardware


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale