Data Fields
TaskP_Params Struct Reference

#include <TaskP.h>

Data Fields

char * name
 
void * arg
 
int priority
 
size_t stackSize
 
void * stack
 Task stack pointer. NULL should be used when calling TaskP_create. A pointer to a current stack should be passed for TaskP_construct. Default: NULL. More...
 

Field Documentation

§ name

char* TaskP_Params::name

Task name. Default: NAME

§ arg

void* TaskP_Params::arg

Task function argument. Default: NULL

§ priority

int TaskP_Params::priority

Task priority. Higher values represent higher priorities. Default: 0

§ stackSize

size_t TaskP_Params::stackSize

Task stack size. Default: TaskP_DEFAULT_STACK_SIZE

§ stack

void* TaskP_Params::stack

Task stack pointer. NULL should be used when calling TaskP_create. A pointer to a current stack should be passed for TaskP_construct. Default: NULL.


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale