![]() |
![]() |
SDIOWFF3 driver object. More...
#include <SDIOWFF3.h>
Data Fields | |
| bool | isInit |
| bool | isOpen |
| bool | cardInitiated |
SDIOWFF3 driver object.
| bool SDIOWFF3_Object::isInit |
True if the driver is initiated
| bool SDIOWFF3_Object::isOpen |
True if the driver is opened
| bool SDIOWFF3_Object::cardInitiated |
True if the card is initiated