Data Fields
SDIO_Params Struct Reference

SDIO Parameters. More...

#include <SDIO.h>

Data Fields

void * custom
 

Detailed Description

SDIO Parameters.

SDIO Parameters are used to with the SDIO_open() call. Default values for these parameters are set using SDIO_Params_init().

See also
SDIO_Params_init()

Field Documentation

§ custom

void* SDIO_Params::custom

Custom argument used by driver implementation


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale