Data Fields
LogSinkUART_Config Struct Reference

LogSinkUART Global configuration. More...

#include <LogSinkUART.h>

Data Fields

void * object
 
void const * hwAttrs
 

Detailed Description

LogSinkUART Global configuration.

The LogSinkUART_Config structure contains a set of pointers used to characterize a LogSinkUART implementation.

Field Documentation

§ object

void* LogSinkUART_Config::object

Pointer to a driver specific data object

§ hwAttrs

void const* LogSinkUART_Config::hwAttrs

Pointer to a driver specific hardware attributes structure


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale