Data Fields
I2CWFF3_Object Struct Reference

I2CWFF3 Object. More...

#include <I2CWFF3.h>

Collaboration diagram for I2CWFF3_Object:
Collaboration graph
[legend]

Data Fields

I2C_BASE_OBJECT SwiP_Struct swi
 
I2C_BitRate bitRate
 
uint32_t addressMode
 
void * i2cPostFxn
 
Power_NotifyObj i2cPostObj
 

Detailed Description

I2CWFF3 Object.

The application must not access any member variables of this structure!

Field Documentation

§ swi

I2C_BASE_OBJECT SwiP_Struct I2CWFF3_Object::swi

§ bitRate

I2C_BitRate I2CWFF3_Object::bitRate

§ addressMode

uint32_t I2CWFF3_Object::addressMode

§ i2cPostFxn

void* I2CWFF3_Object::i2cPostFxn

§ i2cPostObj

Power_NotifyObj I2CWFF3_Object::i2cPostObj

The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale